1. Article purpose[edit source]
The purpose of this article is to:
- briefly introduce the Arm® Cortex®-A35 and its main features,
- indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
- list the software frameworks and drivers managing the peripheral,
- explain how to configure the peripheral.
2. Peripheral overview[edit source]
The Arm Cortex-A7 can be instantiated several times into a single cluster:
- The STM32MP25 main processor is a Cortex-A35 cluster embedding one or two core(s), depending on the selected line.
The Cortex-A35 processor is Arm's most power-efficient application processor capable of seamlessly supporting 32-bit and 64-bit code. It fully supports ARMv8-A architecture, with following features:
- AArch32 for full backward compatibility with Arm7
- AArch64 for 64-bit support
- Trustzone security
- Hardware virtualization support
- Neon Advanced SIMD and floating-point architecture support
- Memory management unit (MMU)
- Separate Level 1 (L1) data- and instruction-side memory systems
- Unified Level 2 (L2) memory system that provides Cortex-A35 subsystem memory coherency
The Cortex-A35 supports a non-secure and a secure modes that define two hardware execution contexts, named Cortex-A35 non-secure and Cortex-A35 secure.
Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.
3. Peripheral usage[edit source]
This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.
3.1. Boot time assignment[edit source]
As soon as the STM32MP2 is powered up, The Cortex-A35 starts to execute the ROM code, which is the first stage of the boot chain.
In Cortex-A35 main processor mode, it then executes the FSBL TF-A in secure mode before jumping to the SSBL U-Boot in non-secure mode.
3.1.1. On STM32MP2 series[edit source]
Click on to expand or collapse the legend...
- ☐ means that the peripheral can be assigned to the given boot time context.
- ☑ means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
- ⬚ means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (ROM code) |
Cortex-A35 secure (TF-A BL2) |
Cortex-A35 non-secure (U-Boot) | |||
Core/Processors | Arm® Cortex®-A35 | Arm® Cortex®-A35 | ✓ | ✓ | ✓ |
3.2. Runtime assignment[edit source]
At runtime, Cortex-A35 is executing OpenSTLinux BSP distribution. Cortex-A35 executes the secure monitor TF-A BL31 and secure OS OP-TEE in secure mode and Linux kernel in non-secure mode
3.2.1. On STM32MP25x lines
[edit source]
Click on to expand or collapse the legend...
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ☐ means that the peripheral can be assigned to the given runtime context.
- ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
- ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.
Domain | Peripheral | Runtime allocation | Comment ![]() | |||||
---|---|---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (OP-TEE / TF-A BL31) |
Cortex-A35 non-secure (Linux) |
Cortex-M33 secure (TF-M) |
Cortex-M33 non-secure (STM32Cube) |
Cortex-M0+![]() (STM32Cube) | |||
Arm® Cortex®-A35 | Arm® Cortex®-A35 | ✓OP-TEE ✓TF-A BL31 |
✓ |
4. Software frameworks and drivers[edit source]
Below are listed the software frameworks and drivers managing the Arm® Cortex®-A35 peripheral for the embedded software components listed in the above tables.
![]() |
Coming soon |
5. How to assign and configure the peripheral[edit source]
The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral by generating:
- partial device trees (pin control and clock tree) for the OpenSTLinux software components,
- HAL initialization code for the STM32CubeMPU Package.
The configuration is applied by the firmware running in the context in which the peripheral is assigned.
![]() |
Coming soon |
6. How to go further[edit source]
![]() |
Coming soon |
7. References[edit source]