VREFBUF internal peripheral - STM32MP15

Revision as of 17:49, 27 May 2021 by Registered User
Applicable for STM32MP15x lines

BackToNavigationTree button.png

1. Article purpose[edit source]

The purpose of this article is to

  • briefly introduce the VREFBUF peripheral and its main features
  • indicate the level of security supported by this hardware block
  • explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
  • explain, when needed, how to configure the VREFBUF peripheral.

2. Peripheral overview[edit source]

The VREFBUF peripheral is an internal voltage regulator.

2.1. Features[edit source]

The VREFBUF is supplied via the VDDA pin. When enabled, it can provide a reference voltage in the range of: 1,5V, 1,8V, 2,048V or 2,5V.

The VREFBUF can be used to provide an analog voltage reference for:

  • ADC internal peripheral[1]
  • DAC internal peripheral[2]
  • External components through the dedicated VREF+ pin.

The VREFBUF can be left unused. In this case, an external voltage regulator can provide reference voltage to VREF+ pin.

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to know which features are really implemented.

2.2. Security support[edit source]

The VREFBUF is a non-secure peripheral.

3. Peripheral usage and associated software[edit source]

3.1. Boot time[edit source]

The VREFBUF is usually not used at boot time. But it may be needed by the SSBL (see Boot chain overview), to supply the internal ADC[1] for example.

3.2. Runtime[edit source]

3.2.1. Overview[edit source]

The VREFBUF can be allocated to the Arm® Cortex®-A7 non-secure to be used under Linux® with regulator framework[3].

Info white.png Information
The VREFBUF is a system resource[4] which needs to be also controlled by the resource manager[4] in case its consumers (e.g. ADC[1], DAC[2] or an external device connected to VREF+ pin) are spread across:
  • the Arm® Cortex®-A7 non-secure context
  • the Arm® Cortex®-M4 context

For this reason, the direct control of VREFBUF from the Arm® Cortex®-M4 is not recommended in STM32Cube[5] by default.
It's recommended to implement it in STM32Cube only if all consumers and the VDDA supply pin are controlled in the Arm® Cortex®-M4 context.

The Peripheral assignment chapter describes which peripheral instance can be assigned to which context.

3.2.2. Software frameworks[edit source]

Internal peripherals software table template

| Analog
| VREFBUF
| 
| Linux regulator framework
|
|
|-
|}

3.2.3. Peripheral configuration[edit source]

The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration by itself can be performed via the STM32CubeMX tool for all internal peripherals. It can then be manually completed (especially for external peripherals) according to the information given in the corresponding software framework article.

3.2.4. Peripheral assignment[edit source]

Internal peripherals assignment table template

| rowspan="1" | Analog
| rowspan="1" | VREFBUF
| VREFBUF
| 
| 
|
| Assignment (single choice)
|-
|}

4. References[edit source]

BackToNavigationTree button.png