This article provides guidelines to setup environment for developing and debugging User Space application within STM32CubeIDE version 1.4 or 1.5.
1. Prerequisites[edit source]
Minimum hardware:
- STM32MP15x-based board
- Linux console
- Ethernet (or Ethernet over USB) for connection to Linux CA7
Minimum software:
- STM32CubeIDE 1.4.2 installed
- STM32MP15 project created
- Yocto SDk installed thanks to "Setup OpenSTLinux" CA7 contextual menu
2. Create User Space project[edit source]
Open new C Project wizard: File -> New -> Project... C Project.
In first window choose OpenSTLinux SDK
then Next and Advanced settings...
Purpose is to setup SDKPATH variable: Project Properties > C/C++ Build > Environment > Edit variable > Variables
Here SDK Installation is Embedded inside STM32CubeIDE, toolchain is located under <InstallDir>/plugins/com.st.openstlinux.sdk.openstlinux_5.4_dunfell_mp1_20_06_24_5.4.0.202007020712/tools/
In case SDK is installed on your disk, give its installation path.
Populate this project with main.c file: select project, right click: New -> File -> main.c Fill it with some C code:
void main() {
int i;
for (i=0;i<10;i++);
i++;
i++;
i++;
return 33;
}