This article explains the way STM32CubeIDE is managing Yocto SDK provided by OpenSTLinux.
1. Overview[edit source]
Two flavors are proposed for installing Yocto SDK:
- Yocto SDK is already installed on host workstation, typically after a download of the STM32MP1 OpenSTLinux Developer Package. In that case, only a setup is needed for STM32CubeIDE to use it.
- Yocto SDK is not present on host workstation, it can be installed via STM32CubeIDE.
The choice is proposed after the Setup OpenSTLinux menu, selecting Use existing.
Error creating thumbnail: Unable to save thumbnail to destination
Note that Setup OpenSTLinux phase also includes download and installation of OpenSTLinux Sources plugin.
2. Using already installed Yocto SDK[edit source]
You have then to give the Yocto SDK Install Root Path in the STM32Cube Preferences.
3. Installing Yocto SDK via STM32CubeIDE[edit source]
This corresponds to the Download choice where OpenSTLinux SDK plugin is installed. Note that missing of OpenSTLinux required packages will lead to unpredictable Yocto SDK usage...
A second choice allows to install Yocto SDK as:
- external, on host workstation disk, outside STM32CubeIDE scope; Yocto SDK removal is under final user responsibility
- embedded inside the STM32CubeIDE; Yocto SDK removal is managed by STM32CubeIDE
.