This page explains how to configure the U-Boot source for your board.
1. introduction[edit source]
Ressources [1] [2] already explain the porting U-Boot on a new board, this page is only a basic guideline.
To summarize, you need to configure U-Boot:
- add your board #device tree
- create your own board support #board subdirectory
- add TARGET_<board> in #Kconfig
- create your board #defconfig
- add your #config file
2. device tree[edit source]
See U-Boot_overview#Device_tree for details.
- copy the kernel device tree in arch/arm/dts directory: <board>.dts
- update arch/arm/dts/Makefile to compile your device tree, for example:
dtb-$(CONFIG_STM32MP15x) += \ <board>.dtb
- add a U-Boot device tree for your board n arch/arm/dts directory: <board>-u-boot.dtsi
This file with all the U-Boot update on kernel device tree is automatically inlcude during <board>.dts
This should include the <soc>-u-boot.dtsi file provided by STMicroelectronics and add all the properties needed by U-Boot (node /config, attibute u-boot,dm-pre-reloc / u-boot,dm-pre-proper)
At this point you can trying the generic ST defconfig with the ST board directory but any board specific feature are not correctly managed.
For example, on STM32MP15x lines :
make stm32mp15_trusted_defconfig
make DEVICE_TREE=<board> all
3. board subdirectory[edit source]
Create your own board support subdirectory = board/<vendor>/<board> and add a Makefile:
You can compile the ST files (in board/st/stm32mp1 or in board/st/common) or just copy as staring point and modify them.
For example in board/dhelectronics/dh_stm32mp1/Makefile:
ifdef CONFIG_SPL_BUILD
obj-y += ../../st/stm32mp1/spl.o
endif
obj-y += ../../st/stm32mp1/board.o board.o
You can add any files needed for your board.
4. Kconfig[edit source]
You need to support your board new TARGET_<board> in arch/arm/mach-stm32mp/Kconfig:
in arch/arm/mach-stm32mp/Kconfig: 1/ Add new TARGET_<board> 2/ Incluee your board Kconfig
choice prompt "STM32MP15x board select" optional [...] config TARGET_<BOARD> bool "<vendor> <board> board" select STM32MP15x help target the <vendor> <board> board with SOC STM32MP15x managed by board/<vendor>/<board> endchoice
[...] source "board/st/stm32mp1/Kconfig" source "board/dhelectronics/dh_stm32mp1/Kconfig" source "board/<vendor>/<board>/Kconfig" endif
3/ add board/<vendor>/<board>/Kconfig file:
The mininimal content is:
if TARGET_<VENDOR>_<BOARD> config SYS_BOARD default "<board>" config SYS_VENDOR default "<vendor>" config SYS_CONFIG_NAME default "<config>" endif
See for example board/dhelectronics/dh_stm32mp1/Kconfig
CONFIG_SYS_CONFIG_NAME = <config> is used in #config file