U-Boot overview

Revision as of 17:36, 3 April 2020 by Registered User (latest release on ST github)

1. Das U-Boot[edit source]

Das U-Boot ("the Universal Boot Loader" or U-Boot) is an open-source bootloader that can be used on ST boards to initialize the platform and load the Linux® kernel.

  git clone https://gitlab.denx.de/u-boot/u-boot.git

Read the README file before starting using U-Boot. It covers the following topics:

  • source file tree structure
  • description of CONFIG defines
  • instructions for building U-Boot
  • brief description of the Hush shell
  • list of common environment variables

2. U-Boot overview[edit source]

Zoom out to STM32MPU Embedded Software

The STM32 MPU boot chain uses Trusted Firmware-A (TF-A) as FSBL and U-Boot as SSBL.

For information, the same U-Boot source can also generate a alternate FSBL named SPL and the boot chain becomes: SPL as FSBL and U-Boot as SSBL.

Warning white.png Warning
This alternate boot chains with SPL cannot be used for product development.


2.1. SPL: alternate FSBL[edit source]

2.1.1. SPL description[edit source]

The U-Boot SPL or SPL can be a alternate first stage bootloader (FSBL).
It is a small binary (bootstrap utility) generated from the U-Boot source and stored in the internal limited-size embedded RAM. SPL main features are the following:

  • It is loaded by the ROM code.
  • It performs the initial CPU and board configuration (clocks and DDR memory).
  • It loads the SSBL (U-Boot) into the DDR memory.

2.1.2. SPL restrictions[edit source]

Warning white.png Warning
SPL cannot be used for product development.

SPL is provided only as an example of the simplest SSBL and to support upstream U-Boot development. However, several known limitations have been identified when SPL is used in conjunction with the minimal secure monitor provided within U-Boot for basic boot chain. They apply to:

  • no power managment
  • secure access to registers
  • limited features (STM32CubeProgrammer / boot from NAND Flash memory)
  • no SCMI support for clock, reset: not compatible with latest Linux kernel device tree

These limitations can't be removed.

2.1.3. SPL phases[edit source]

SPL executes the following main phases in SYSRAM:

  • board_init_f(): driver initialization including DDR initialization (mininimal stack and heap: CONFIG_SPL_STACK_R_MALLOC_SIMPLE_LEN)
  • configuration of heap in DDR memory (CONFIG_SPL_SYS_MALLOC_F_LEN)
  • board_init_r(): initialization of the other drivers activated in the SPL device tree
  • loading and execution of U-Boot (or Kernel in Falcon mode[1]: README.falcon ).

2.2. U-Boot: SSBL[edit source]

2.2.1. U-Boot description[edit source]

U-Boot is the second-stage bootloader (SSBL) of boot chains for STM32 MPU platforms.

SSBL main features are the following:

  • It is configurable and expendable.
  • It features a simple command line interface (CLI), allowing users to interact over a serial port console.
  • It provides scripting capabilities
  • It loads the kernel into RAM and gives control to the kernel
  • It manages several internal and external devices such as NAND and NOR Flash memories, Ethernet and USB.
  • It supports the following features and commands:
    • File systems: FAT, UBI/UBIFS, JFFS
    • IP stack: FTP
    • Display: LCD, HDMI, BMP for splashcreen
    • USB: host (mass storage) or device (DFU stack)

2.2.2. U-Boot phases[edit source]

U-Boot executes the following main phases in DDR memory:

  • Pre-relocation initialization (common/board_f.c): minimal initialization (such as CPU, clock, reset, DDR and console) running at the CONFIG_SYS_TEXT_BASE load address.
  • Relocation: copy of the code to the end of DDR memory.
  • Post-relocation initialization:(common/board_r.c): initialization of all the drivers.
  • Command execution through autoboot (CONFIG_AUTOBOOT) or console shell
    • Execution of the boot command (by default bootcmd=CONFIG_BOOTCOMMAND):
      for example, execution of the command bootm to:
      • load and check images (such as kernel, device tree and ramdisk)
      • fixup the kernel device tree
      • install the secure monitor (optional) or
      • pass the control to the Linux kernel (or to another target application)

3. U-Boot configuration[edit source]

The U-Boot binary configuration is based on

  • Kbuild infrastructure (as in Linux Kernel, you can use make menuconfig in U-Boot)
    The configurations are based on:
  • other compilation flags defined in include/configs/stm32mp*.h (these flags are progressively migrated to Kconfig)
    The file name is configured through CONFIG_SYS_CONFIG_NAME.
    For STM32MP15x lines More info.png, the include/configs/stm32mp1.h file is used.
  • DeviceTree: U-Boot binaries include a device tree blob that is parsed at runtime

All the configuration flags (prefixed by CONFIG_) are described in the source code, either in the README file or in the documentation directory .
For example, CONFIG_SPL activates the SPL compilation.
Hence to compile U-Boot, select the <target> and the device tree for the board in order to choose a predefined configuration.
Refer to #U-Boot_build for examples.

3.1. Kbuild[edit source]

Like the kernel, the U-Boot build system is based on configuration symbols (defined in Kconfig files). The selected values are stored in a .config file in the build directory, with the same makefile target. .
Proceed as follows:

  • Select a pre-defined configuration (defconfig file in configs directory ) and generate the first .config:
  make <config>_defconfig.
  • Change the U-Boot compile configuration (modify .config) by using one of the following five make commands:
  make menuconfig --> menu based program
  make config  --> line-oriented configuration
  make xconfig --> QT program[2]
  make gconfig --> GTK program
  make nconfig --> ncurse menu based program

You can then compile U-Boot with the updated .config.

Warning: the modification is performed locally in the build directory. It will be lost after a make distclean.

Save your configuration to be able to use it as a defconfig file:

   make savedefconfig

This target saves the current config as a defconfig file in the build directory. It can then be compared with the predefined configuration (configs/stm32mp*defconfig).

The other makefile targets are the following:

   make help
 ....
 Configuration targets:
   config	  - Update current config utilising a line-oriented program
   nconfig         - Update current config utilising a ncurses menu based
                     program
   menuconfig	  - Update current config utilising a menu based program
   xconfig	  - Update current config utilising a Qt based front-end
   gconfig	  - Update current config utilising a GTK+ based front-end
   oldconfig	  - Update current config utilising a provided .config as base
   localmodconfig  - Update current config disabling modules not loaded
   localyesconfig  - Update current config converting local mods to core
   defconfig	  - New config with default from ARCH supplied defconfig
   savedefconfig   - Save current config as ./defconfig (minimal config)
   allnoconfig	  - New config where all options are answered with no
   allyesconfig	  - New config where all options are accepted with yes
   allmodconfig	  - New config selecting modules when possible
   alldefconfig    - New config with all symbols set to default
   randconfig	  - New config with random answer to all options
   listnewconfig   - List new options
   olddefconfig	  - Same as oldconfig but sets new symbols to their
                    default value without prompting

3.2. Device tree[edit source]

Refer to doc/README.fdt-control for details.

The board device tree has the same binding as the kernel. It is integrated within the U-Boot binaries:

  • By default, it is appended at the end of the code (CONFIG_OF_SEPARATE).
  • It is embedded in the U-Boot binary (CONFIG_OF_EMBED). This is useful for debugging since it enables easy .elf file loading.

A default device tree is available in the defconfig file (by setting CONFIG_DEFAULT_DEVICE_TREE).

You can either select another supported device tree using the DEVICE_TREE make flag. For stm32mp boards, the corresponding file is: arch/arm/dts/stm32mp*.dts .

   make DEVICE_TREE=<dts-file-name>

or provide a precompiled device tree blob (using EXT_DTB option):

   make EXT_DTB=boot/<dts-file-name>.dtb

The SPL device tree is also generated from this device tree. However to reduce its size, the U-Boot makefile uses the fdtgrep tool to parse the full U-Boot DTB and identify all the drivers required by SPL.

To do this, U-Boot uses specific device-tree flags to define if the associated driver is initialized prior to U-Boot relocation and/or if the associated node is present in SPL :

  • u-boot,dm-pre-reloc => present in SPL, initialized before relocation in U-Boot
  • u-boot,dm-pre-proper => initialized before relocation in U-Boot
  • u-boot,dm-spl => present in SPL

In the device tree used by U-Boot, these flags need to be added in each node used in SPL or in U-Boot before relocation and for each used handle (clock, reset, pincontrol).

To have a file "<board>.dts" identical with Linux kernel, these U-Boot properties are only added for ST boards in the add-on file "<board>-u-boot.dtsi"; this file is automatically included in "<board>.dts" during compilation (it is a generic U-Boot Makefile behavior).

4. U-Boot command line interface (CLI)[edit source]

Refer to U-Boot Command Line Interface.

If CONFIG_AUTOBOOT is activated, you have CONFIG_BOOTDELAY seconds (2s by default, 1s for ST configuration) to enter the console by pressing any key, after the line below is displayed and bootcmd is executed (CONFIG_BOOTCOMMAND):

 Hit any key to stop autoboot:  2

4.1. Commands[edit source]

The commands are defined in cmd/*.c . They are activated through the corresponding CONFIG_CMD_* configuration flag.

Use the help command in the U-Boot shell to list the commands available on your device:

  help

Below the list of all commands extracted from U-Boot Manual (not-exhaustive):

  • Information Commands
    • bdinfo - prints Board Info structure
    • coninfo - prints console devices and information
    • flinfo - prints Flash memory information
    • iminfo - prints header information for application image
    • help - prints online help
  • Memory Commands
    • base - prints or sets the address offset
    • crc32 - checksum calculation
    • cmp - memory compare
    • cp - memory copy
    • md - memory display
    • mm - memory modify (auto-incrementing)
    • mtest - simple RAM test
    • mw - memory write (fill)
    • nm - memory modify (constant address)
    • loop - infinite loop on address range
  • Flash Memory Commands
    • cp - memory copy
    • flinfo - prints Flash memory information
    • erase - erases Flash memory
    • protect - enables or disables Flash memory write protection
    • mtdparts - defines a Linux compatible MTD partition scheme
  • Execution Control Commands
    • source - runs a script from memory
    • bootm - boots application image from memory
    • go - starts application at address 'addr'
  • Download Commands
    • bootp - boots image via network using BOOTP/TFTP protocol
    • dhcp - invokes DHCP client to obtain IP/boot params
    • loadb - loads binary file over serial line (kermit mode)
    • loads - loads S-Record file over serial line
    • rarpboot- boots image via network using RARP/TFTP protocol
    • tftpboot- boots image via network using TFTP protocol
  • Environment Variables Commands
    • printenv- prints environment variables
    • saveenv - saves environment variables to persistent storage
    • setenv - sets environment variables
    • run - runs commands in an environment variable
    • bootd - boots default, i.e., run 'bootcmd'
  • Flattened Device Tree support
    • fdt addr - selects the FDT to work on
    • fdt list - prints one level
    • fdt print - recursive printing
    • fdt mknode - creates new nodes
    • fdt set - sets node properties
    • fdt rm - removes nodes or properties
    • fdt move - moves FDT blob to new address
    • fdt chosen - fixup dynamic information
  • Special Commands
    • i2c - I2C sub-system
  • Storage devices
  • Miscellaneous Commands
    • echo - echoes args to console
    • reset - Performs a CPU reset
    • sleep - delays the execution for a predefined time
    • version - prints the monitor version

To add a new command, refer to doc/README.commands .

4.2. U-Boot environment variables[edit source]

The U-Boot behavior is configured through environment variables.

Refer to Manual and README / Environment Variables.

On the first boot, U-Boot uses a default environment embedded in the U-Boot binary. You can modify it by changing the content of CONFIG_EXTRA_ENV_SETTINGS in your configuration file (for example ./include/configs/stm32mp1.h) (see README / - Default Environment).

This environment can be modified and saved in the boot device. When it is present, it is loaded during U-Boot initialization:

  • for eMMC/SD card boot (CONFIG_ENV_IS_IN_MMC), at the end of the partition indicated by config field "u-boot,mmc-env-partition" in device-tree (partition named "ssbl" for ST boards).
  • for NAND boot (CONFIG_ENV_IS_IN_UBI), in the two UBI volumes "config" (CONFIG_ENV_UBI_VOLUME) and "config_r" (CONFIG_ENV_UBI_VOLUME_REDUND).
  • for NOR boot (CONFIG_ENV_IS_IN_SPI_FLASH), in the u-boot_env mtd parttion (at offset CONFIG_ENV_OFFSET).

4.2.1. env command[edit source]

The env command allows displaying, modifying and saving the environment in U-Boot console.

  help env
 env - environment handling commands
 
 Usage:
 env default [-f] -a - [forcibly] reset default environment
 env default [-f] var [...] - [forcibly] reset variable(s) to their default values
 env delete [-f] var [...] - [forcibly] delete variable(s)
 env edit name - edit environment variable
 env exists name - tests for existence of variable
 env print [-a | name ...] - print environment
 env print -e [name ...] - print UEFI environment
 env run var [...] - run commands in an environment variable
 env save - save environment
 env set -e name [arg ...] - set UEFI variable; unset if 'arg' not specified
 env set [-f] name [arg ...]

Example: proceed as follows to restore the default environment and save it. This is useful after a U-Boot upgrade:

  env default -a
  env save

4.2.2. bootcmd[edit source]

"bootcmd" variable is the autoboot command. It defines the command executed when U-Boot starts (CONFIG_BOOTCOMMAND).

For stm32mp, CONFIG_BOOTCOMMAND="run bootcmd_stm32mp":

  env print bootcmd    
  bootcmd=run bootcmd_stm32mp

"bootcmd_stm32mp" is a script that selects the command to be executed for each boot device (see ./include/configs/stm32mp1.h), based on generic distro scripts:

  • for serial/usb: execute the stm32prog command.
  • for mmc boot (eMMC, SD card), boot only on the same device (bootcmd_mmc...).
  • for nand boot, boot with on ubifs partition on nand (bootcmd_ubi0).
  • for nor boot, use the SD card (on SDMMC 0 on ST boards with bootcmd_mmc0)
  env print bootcmd_stm32mp

You can then change this configuration:

  • either permanently in your board file
    • default environment by CONFIG_EXTRA_ENV_SETTINGS (see ./include/configs/stm32mp1.h)
    • change CONFIG_BOOTCOMMAND value in your defconfig
 CONFIG_BOOTCOMMAND="run bootcmd_mmc0"
 CONFIG_BOOTCOMMAND="run distro_bootcmd"
  • or temporarily in the saved environment:
  env set bootcmd run bootcmd_mmc0 
  env save

Note: To reset the environment to its default value:

  env default bootcmd
  env save

4.3. Generic Distro configuration[edit source]

Refer to doc/README.distro for details.

This feature is activated by default on ST boards (CONFIG_DISTRO_DEFAULTS):

  • one boot command (bootmcd_xxx) exists for each bootable device.
  • U-Boot is independent of the Linux distribution used.
  • bootcmd is defined in ./include/config_distro_bootcmd.h

When DISTRO is enabled, the command that is executed by default is include/config_distro_bootcmd.h :

 bootcmd=run distro_bootcmd

This script tries any device found in the 'boot_targets' variable and executes the associated bootcmd.

Example for mmc0, mmc1, mmc2, pxe and ubifs devices:

 bootcmd_mmc0=setenv devnum 0; run mmc_boot
 bootcmd_mmc1=setenv devnum 1; run mmc_boot
 bootcmd_mmc2=setenv devnum 2; run mmc_boot
 bootcmd_pxe=run boot_net_usb_start; dhcp; if pxe get; then pxe boot; fi
 bootcmd_ubifs0=setenv devnum 0; run ubifs_boot

U-Boot searches for a extlinux.conf configuration file for each bootable device. This file defines the kernel configuration to be used:

  • bootargs
  • kernel + device tree + ramdisk files (optional)
  • FIT image

4.4. U-Boot scripting capabilities[edit source]

"Script files" are command sequences that are executed by the U-Boot command interpreter. This feature is particularly useful to configure U-Boot to use a real shell (hush) as command interpreter.

See U-Boot script manual for an example.

5. U-Boot build[edit source]

5.1. Prerequisites[edit source]

  • a PC with Linux and tools:
  • U-Boot source code
    • the latest STMicroelectronics U-Boot version
      • tar.xz file from Developer Package (for example STM32MP1) or from latest release on ST github [3]
      • from GITHUB[4], with git command
  git clone https://github.com/STMicroelectronics/u-boot
  • from the Mainline U-Boot in official GIT repository [5]
  git clone https://gitlab.denx.de/u-boot/u-boot.git

5.1.1. ARM cross compiler[edit source]

A cross compiler [6] must be installed on your Host (X86_64, i686, ...) for the ARM targeted Device architecture. In addition, the $PATH and $CROSS_COMPILE environment variables must be configured in your shell.

You can use gcc for ARM, available in:

For example, to use gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf.tar.xz from arm, extract the toolchain in $HOME and update your environment with:

  export PATH=$HOME/gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf/bin:$PATH
  export CROSS_COMPILE=arm-none-linux-gnueabihf-

For example, to use gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabi.tar.xz
from https://releases.linaro.org/components/toolchain/binaries/7.2-2017.11/arm-linux-gnueabi/
Unzip the toolchain in $HOME and update your environment with:

  export PATH=$HOME/gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabi/bin:$PATH
  export CROSS_COMPILE=arm-linux-gnueabi-

5.2. Compilation[edit source]

In the U-Boot source directory, select the defconfig for the <target> and the <device tree> for your board and then execute the make all command:

  make <target>_defconfig
  make DEVICE_TREE=<device tree> all

Use help to list other targets than all:

  make help
 

Optionally

  • KBUILD_OUTPUT can be used to change the output buil directory to compile several targets or not to compile in the source directory. For example:
  export KBUILD_OUTPUT=<path>
  • DEVICE_TREE can also be exported to your environment when only one board is supported. For example:
  export DEVICE_TREE=<device-tree>

The result is:

  export KBUILD_OUTPUT=<path>
  export DEVICE_TREE=<device tree>
  make <target>_defconfig
  make all

Examples from STM32MP15 U-Boot:

The boot chain for STM32MP15x lines More info.png use stm32mp15_trusted_defconfig:

  make stm32mp15_trusted_defconfig
  make DEVICE_TREE=stm32mp157f-dk2 all
  export KBUILD_OUTPUT=../build/stm32mp15_trusted
  export DEVICE_TREE=stm32mp157c-ev1
  make stm32mp15_trusted_defconfig
  make all

5.3. Output files[edit source]

The resulting U-Boot files are located in your build directory (U-Boot or KBUILD_OUTPUT).

The U-Boot generated files when TF-A is used as FSBL, with or without OP-TEE:

  • u-boot.stm32 : U-Boot binary with STM32 image header, loaded by TF-A

The files used to debug with gdb are

  • u-boot : elf file for U-Boot

6. References[edit source]