The STM32MPU distribution for Android™ runs on Arm® Cortex®-A processors. It is a subset of the STM32MPU Embedded Software distribution for Android.
It includes the following collection of software components:
- OpenSTLinux BSP that offers services for the application frameworks in the same context:
- boot chain based on TF-A and U-Boot.
- OP-TEE secure OS running on the Cortex-A core in Secure mode
- Linux® kernel running on the Arm® Cortex®-A core in Non-secure mode
- Application frameworks that rely on the services provided by the OpenSTLinux BSP, to provide specific functionalities (code libraries, APIs, tool sets...) to ease the development of software applications:
- OP-TEE application frameworks running in the secure OS user space (e.g. TEE Internal core API for the development of Trusted Applications (TA))
- Android application frameworks running in Linux OS user space (see AOSP[1] for more details)
The OpenSTLinux BSP for Android has some specificities:
- The Linux kernel source is based on the Common Kernel available in AOSP[2]
- The Linux kernel configuration is based on the reference configuration available in AOSP[3]
Android application frameworks are based on the AOSP platform manifest[4]. By default, one of the Google tags[5] is used as a reference.
The Google services (ex: Cast, Drive, Maps...) are neither embedded nor validated within this STM32MPU distribution for Android™.
1. How to get the software for this distribution?[edit source]
The STM32MPU distribution for Android™ is available through the three Packages (Starter, Developer, and Distribution) of the STM32MPU Embedded Software distribution for Android.
2. References[edit source]