Template:ArticleMainWriter Template:ArticleFirstDraftVersion Template:ReviewersList
1. Purpose[edit source]
This article explains how to compile a devicetree in a Windows® environment, and how to deploy the compiled devicetree.
2. Rationale[edit source]
STM32CubeMX can be used in both Linux®<> and Windows® environments. STM32MPU_Embedded_Software_distribution depends on a Linux® environment. Nevertheless, the generation of a devicetree from STM32CubeMX and its compilation can be managed in a Windows® environment for some components.
3. Pre-requisites[edit source]
- Install a cross-compiler
- A cross compiler is needed to parse/prepare the dts file.
- System Workbench for STM32 is a good candidate
- The zip file with the gcc could be find in C:\Ac6\SystemWorkbench\plugins\fr.ac6.mcu.externaltools.arm-none.win32_1.16.0.201807130628\tools
- mingw64 is also is good alternative
- System Workbench for STM32 is a good candidate
- A cross compiler is needed to parse/prepare the dts file.
- Install a devicetree compiler
- Install the dtc.exe and mkimage.exe from the zip file dt4win-0.2.0.zip
4. updating devicetree of TF-A[edit source]
5. updating devicetree of U-Boot[edit source]
6. updating devicetree of Kernel[edit source]
- Get the source code of Linux
- Apply patch on the source code of Linux
- Create a workdir directory
- mkdir workdir
- Copy from source code of Linux the dt-bindings and dt files
- cp <KernelSources>/include/dt-bindinds workdir
- cp <KernelSources>/arch/arm/boot/dts/* workdir/
- Copy your dts into workdir
- cp <Your/dts/file.dts> workdir/
- Prepare dts
- cd workdir
- arm-none-eabi-gcc.exe -E -nostdinc -I . -undef -D__DTS__ -x assembler-with-cpp -o <yourDTS.dts>.tmp <yourDTS.dts>
- compile dts.tmp with dtc.exe
- dtc.exe -I dts -O dtb -o <DTBresult.dtb> <yourDTS.dts>.tmp