This article aims to describe the content of the software release included in the STM32CubeMP2 Package, version v.0.3.0.
1. Delivery purpose and scope[edit source]
The STM32CubeMP2 Package is a software package running on Arm® Cortex®-M33 processor nd is a fundamental part of the STM32MPU Embedded Software distribution.
This release includes:
- The STM32Cube HAL: STM32 abstraction layer embedded software ensuring maximized portability across the STM32 portfolio. HAL APIs are available for all peripherals.
- Low-layer APIs (LL APIs) offering a fast lightweight expert-oriented layer that is closer to the hardware than the HAL.
LL APIs are only available for a limited set of peripherals. - A consistent set of middleware components such as AzureRTOS.
- All embedded software utilities delivered with a full set of examples.
It also includes:
- BSP for the STM32MP257F-EV1 Evaluation board (LED, button and COM ports)
- Projects: several projects (examples, applications) are implemented in IDE delivered by ST
2. Intended Audience[edit source]
The targeted audience is STM32 MPU customers and partners.
3. Licensing[edit source]
All licenses applicable to STM32CubeMP2 package are available here.
4. Supported devices[edit source]
The drivers provided within this package support all STM32MP25x lines .
5. Supported hardware[edit source]
The software examples and the drivers delivered in this package are applicable for the following boards:
- STM32MP257F-EV1 Evaluation board , for information about those boards, read the article STM32MP257x-EV1 hardware description.
6. Release content[edit source]
This release is the first release of the STM32CubeMP2 software package running on Arm® Cortex®-M33 core. The full content is available in STM32CubeMP2 Package content
6.1. Main changes[edit source]
This is the BETA release of STM32CubeMP2 package running on the Arm® Cortex®-m33 of STM32MP25x lines as a coprocessor. This STM32CubeMP2 package can be then used as any STM32Cube package running on STM32-MPU of STMicroelectronics.
6.1.1. HAL drivers[edit source]
- This is BETA release of STM32CubeMP2 package HAL drivers.
- All HAL drivers have been checked for MISRA 2012 compliance but some warnings are still to be completed.
- Check overview and all available HAL drivers in HAL drivers
6.1.2. LL drivers[edit source]
- This is BETA release of STM32CubeMP2 package LL drivers.
- All LL drivers have been checked for MISRA 2012 compliance but warnings are not fixed completely.
- Check overview and all available LL drivers here LL drivers
6.1.3. BSP[edit source]
- This is BETA release of STM32CubeMP2 package BSP drivers.
- Refer to BSP Drivers section here BSP drivers.
6.1.4. CMSIS[edit source]
- Bit and registers definition for STM32MP25x lines .
- Support for System, Startup and Linker files.
- For more details, refer to CMSIS
6.1.5. Middleware[edit source]
- OpenAMP [1]
- UCPD : STM32_USBPD_Library
- Check overview of middleware's in STM32CubeMP2 Package article
6.1.6. Projects[edit source]
- Check project section here Projects for details of projects implemented.
6.2. Released components[edit source]
6.2.1. Drivers[edit source]
Component | Version | Notes |
---|---|---|
Cortex-M CMSIS | V5.6.0 | - |
STM32MP2xx CMSIS | V0.3.0 | - |
STM32MP2xx HAL | V0.3.0 | - |
BSP STM32MP257F_EV1 | V0.3.0 | - |
Find here the list of available HAL , LL and BSP drivers.
6.2.2. Middleware[edit source]
Component | Version | Notes |
---|---|---|
AzureRTOSTM | v6.2.0.221223 | - |
OpenAMP | v2022.10_20230315 | - |
6.2.3. Utilities[edit source]
Component | Version | Notes |
---|---|---|
Resourcemanager | V0.3.0 | - |
6.3. Released projects[edit source]
The STM32CubeMP2 Package comes with a rich set of examples running on STMicroelectronics boards, organized by board and provided with preconfigured projects. The main supported development environment is STM32CubeIDE (works on Multiple OS's) and uses the GNU toolchain.
Find in this article STM3257-EV1 Projects, the exhaustive list of available projects for STM32MP257F-EV1 Evaluation board
The recommended supported toolchain for STM32MP2 is now STM32CubeIDE (All-in-one multi-OS development tool).
6.4. STM32MP25 Chip revA support[edit source]
- With this delivery, it is still possible to compile for STM32MP25 Chip revA. The STM32MP25XX_SI_CUT1_X macro must be defined as a preprocessor flag in the project definition for STM32MP25 Rev A support.
7. Main restrictions[edit source]
- Clock muxing RCC HAL API in CxM33 No secure context not yet supported by STM32CubeMP2 for DSI, LVDS, RTC, MCO1/2, DTS, USB
8. How to get started with STM32CubeMP2 Package[edit source]
Refer to How to get software and start with this release article.