RISAF internal peripheral

Revision as of 11:42, 26 October 2023 by Registered User
Applicable for STM32MP25x lines

Warning white.png Warning
Concerning the STM32MP25x lines More info.png, only the boot time assignment table and the runtime assignment table have been updated.
The other chapters have not been updated yet.


1. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the RISAF peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

2. Peripheral overview[edit source]

The RISAF peripheral is part of the RIF. It is used to protect external memory access.
Its main features are:

  • Configuration at fixed size memory blocks (512B) and pages (4kB)
  • Access filtering per:
    • secure level
    • CID filtering
    • privilege level per CID
    • read-only, write-only or read/write per CID
  • Possibility to delegate some sub-region configuration to a specified execution context defined by delegated configuration CID. Useful to manage memory region access right at SW component level instead of requiring changes to TDCID secure OS.

Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

3. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

On STM32MP25x lines More info.png, there are 4 RISAF instances. The following table shows RISAF - External memory interface mapping and provides information regarding RISAF programming owner and default HW configuration.
RISAF registers are accessible in read by all execution context to check memory can be accessed or not.

RISAF instance Protected interface Owner Nb regions Encryption Default configuration
RISAF1 BKPSRAM (lower 128kB) TDCID Secure 4 No Secure, unprivileged, any CID
RISAF2 256Mbyte of OCTOSPI1&2
memory mapped region
TDCID Secure 4 No Secure, unprivileged, any CID
RISAF4 DDR 4GB TDCID Secure 15 Yes Non-secure, unprivileged, any CID
RISAF5 PCIe TDCID Secure 2 No Secure, unprivileged, any CID


3.1. Boot time assignment[edit source]

In Cortex-A35 main processor mode, the FSBL TF-A is in charge of DDR controller initialization and of secure OS OP-TEE loading. This implies to configure RISAF4 secure and encrypted memory regions before doing secure code loading.

3.1.1. On STM32MP2 series[edit source]

Click on How to.png to expand or collapse the legend...

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Boot time allocation Comment How to.png
Instance Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
non-secure
(U-Boot)
Security RISAF RISAF1
RISAF2
RISAF4 "assigned peripheral" style="font-size:21px">☑ FSBL TF-A configures secure and encrypted memory regions
RISAF5

3.2. Runtime assignment[edit source]

In Cortex-A35 main processor mode, the access rights of the different memory regions are configured by OP-TEE before starting the execution of the firmware running on the other execution contexts.

3.2.1. On STM32MP25x lines More info.png[edit source]

Click on How to.png to expand or collapse the legend...

STM32MP25 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
non-secure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
non-secure
(STM32Cube)
Cortex-M0+
Warning.png
(STM32Cube)
Security RISAF RISAF1 OP-TEE
RISAF2 OP-TEE
RISAF4 OP-TEE
RISAF5 OP-TEE

4. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the RISAF peripheral for the embedded software components listed in the above tables.

Under construction.png Coming soon

5. How to assign and configure the peripheral[edit source]

The STM32CubeMX graphical tool proposes an interface to configure the different RISAF memory regions .
It is possible to select for each region:

  • the security level
  • the privilege level
  • if the region is encrypted or not (depends on RISAF capability)
  • the master CID

The STM32CubeMX will generate associated device tree configuration for the FSBL and secure OS running on the TDCID processor.

6. How to go further[edit source]

Under construction.png Coming soon

7. References[edit source]