How to change the CPU frequency

Revision as of 12:38, 17 December 2021 by Registered User (→‎OPP table)
Applicable for STM32MP13x lines, STM32MP15x lines

1. Purpose[edit source]

This article explains how to change the CPU operating point (also known as OPP). An operating point corresponds to the frequency of the processor and the voltage that needs to be supplied to sustain it.
It also shows how it is possible to define multiple operating points, allowing the system to jump among them at run time: this is the dynamic voltage and frequency scaling (DVFS). Some cautions are given at the end of the article, to help the user in its DVFS deployment.

2. Hardware side[edit source]

On STM32MP1 series products, the Cortex-A7 core:

  • can be clocked by PLL1 from the RCC internal peripheral: the PLL1P output frequency can be directly propagated to the core, or it can go through an intermediate MPUDIV divider
  • is supplied with
  • VDDCPU voltage on STM32MP13x lines More info.png
  • VDDCORE voltage on STM32MP15x lines More info.png

The part number tells the device maximum supported frequency, up to 900 MHz for the STM32MP13 or up to 800 MHz for the STM32MP15, with associated usage conditions. Otherwise, the frequency must be kept below 650 MHz.

3. Software side[edit source]

3.1. Boot time[edit source]

By default, in OpenSTLinux distribution, TF-A BL2 sets the CPU frequency to 650 MHz, that is the maximum frequency sustainable with the nominal voltage of 1.2 V.

3.1.1. On STM32MP13x lines More info.png[edit source]

TF-A recovers this configuration via the following properties read from the board device tree:

  • st,clksrc property, in rcc node, tells to use PLL1P as source clock for the MPU:
	&rcc {
		...
		st,clksrc = <
			CLK_MPU_PLL1P
		...
  • st,pll property, in pll1 node, tells which PLL1 configuration should be used at boot time:
	pll1:st,pll@0 {
		...
		st,pll = < &pll1_cfg1 >;
		...
  • Then, this said PLL1 configuration is declared in two steps:
  • A VCO configuration selection and post-dividers (pqr) configuration:
	pll1_cfg1: pll1_cfg1 {
		st,pll_vco = < &pll1_vco_1300Mhz >;
		st,pll_div_pqr = < 0 1 1 >;
	};
  • The VCO configuration:
	st,pll_vco {
		...
		pll1_vco_1300Mhz: pll1-vco-1300Mhz {
			src = < CLK_PLL12_HSE >;
			divmn = < 2 80 >;
			frac = < 0x800 >;
		};

3.1.2. On STM32MP15x lines More info.png[edit source]

To be completed - unclear for me

3.2. Runtime[edit source]

3.2.1. On STM32MP13x lines More info.png[edit source]

3.2.1.1. Overview[edit source]

By default, in OpenSTLinux distribution, the OP-TEE "soc extension" device tree file defines an OPP table that contains one or several frequency / voltage pair(s).

Info white.png Information
Whatever the implementation is, if your part number supports up to 900 MHz, ensure that the VDDCPU minimum voltage is increased from 1.2V to 1.35 V while running above 650 MHz
3.2.1.2. OPP table[edit source]

At runtime, Linux will automatically request to OP-TEE SCMI interface to switch between the available operating points according to the CPU load and thanks to Linux cpufreq framework, configured with "ondemand" governor policy (see Documentation/admin-guide/pm/cpufreq.rst ). This feature is called dynamic voltage and frequency scaling (DVFS).

For instance, in the example below, two operating points ([900 MHz ; 1.35 V]; [650 MHz ; 1.2 V]) are defined for a 900 MHz capable part number (opp-supported-hw = <0x2>), so TF-A will apply the [650 MHz ; 1.20 V] configuration at boot time and Linux will then dynamically jump between the two operating points ([900 MHz ; 1.35 V]; [650 MHz ; 1.2 V]) depending on the CPU load and thanks to OP-TEE SCMI interface.

&cpu0_opp_table {
		opp-900000000 {
			opp-hz = /bits/ 64 <900000000>;
			opp-microvolt = <1350000>;
			opp-supported-hw = <0x2>;
			st,opp-default;
		};

		opp-650000000 {
			opp-hz = /bits/ 64 <650000000>;
			opp-microvolt = <1200000>;
			opp-supported-hw = <0x2>;
		};
};

Notes:

  • The operating point(s) supported by devices able to run above 650 MHz (and up to 900 MHz) is/are identified by the opp-supported-hw property set to 0x2.
  • The OPP table above is present in OP-TEE device tree and TF-A can only define the opp-650000000 (since the opp-900000000 is useless at boot time)
  • The PLL1 configuration(s) needed to reach the above frequencies must be described via the 'st,clk_opp' property in 'rcc' device tree node, like this is visible in fdts/stm32mp135f-dk.dts , for instance
  • This description is valid for cold boot, but also when coming back from Standby low power mode.

3.2.2. On STM32MP15x lines More info.png[edit source]

3.2.2.1. Overview[edit source]

Two ways are offered to the user in order to set the CPU frequency:

  • By default, in OpenSTLinux distribution, the Linux kernel "soc extension" device tree file defines an OPP table that contains one or several frequency / voltage pair(s)
  • Nevertheless, it is possible to directly define the expected PLL1 static configuration in the FSBL device tree
Info white.png Information
Whatever the implementation is, if your part number supports up to 800 MHz, ensure that the VDDCORE minimum voltage is increased from 1.2V to 1.35 V while running above 650 MHz
3.2.2.2. OPP table[edit source]

At boot time, TF-A automatically selects the fastest operating point that is suitable for the current part number according to the OPP table (frequency and voltage couples) defined in the SOC extension device tree (fdts/stm32mp15xa.dtsi or fdts/stm32mp15xd.dtsi ).
At runtime, the Linux will automatically switch between the available operating points according to the CPU load and thanks to Linux cpufreq framework, configured with "ondemand" governor policy (see Documentation/admin-guide/pm/cpufreq.rst ). This feature is called dynamic voltage and frequency scaling (DVFS).

For instance, in the example below, two operating points ([800 MHz ; 1.35 V]; [400 MHz ; 1.2 V]) are defined for a 800 MHz capable part number (opp-supported-hw = <0x2>), so TF-A will apply the [800 MHz ; 1.35 V] configuration at boot time and Linux will then dynamically jump between the two operating points ([800 MHz ; 1.35 V]; [400 MHz ; 1.2 V]) depending on the CPU load.

&cpu0_opp_table {
		opp-800000000 {
			opp-hz = /bits/ 64 <800000000>;
			opp-microvolt = <1350000>;
			opp-supported-hw = <0x2>;
		};
		opp-400000000 {
			opp-hz = /bits/ 64 <400000000>;
			opp-microvolt = <1200000>;
			opp-supported-hw = <0x2>;
			opp-suspend;
		};
};

Notes:

  • The operating point(s) supported by devices able to run above 650 MHz (and up to 800 MHz) is/are identified by the opp-supported-hw property set to 0x2.
  • This same OPP table must be present in both the TF-A and Linux device tree
  • This description is valid for cold boot, but also when coming back from Standby low power mode.
  • During cold boot, TF-A computes and saves the PLL1 settings for all operating points available in the device tree in compliance with the hardware capabilities. These saved paramaters are used later to increase the performance of the system-state transitions.
3.2.2.3. PLL1 static configuration[edit source]

Should be reworked and moved to the boot time part ? Obsolete in DV4.0.0 ? The Cortex-A7 core frequency is selected at boot time, by the FSBL (TF-A), following the Clock device tree configuration - Bootloader specific syntax.

&rcc {
	...
	/* VCO = 1300.0 MHz => P = 650 (CPU) */
	pll1: st,pll@0 {
		cfg = < 2 80 0 0 0 PQR(1,0,0) >;
		frac = < 0x800 >;
	};
	...
};

The user can reduce this frequency by changing the above configuration, either manually or via the STM32CubeMX graphical user interface that allows generation of the corresponding device tree file.
Notes:

  • The VDDCORE voltage is specified in the regulators node of the board device tree, and it has to be kept consistent with the selected frequency, as explained in the overview above.
  • When the PLL1 static configuration is used, TF-A ignores the OPP table (see previous chapter) that may also be present in the device tree, so the secure monitor won't be able to answer to any upcoming frequency switch from Linux. It is therefore recommended to keep only one OPP in the table given to Linux, corresponding to the frequency setup by TF-A at boot time.

4. Dynamic voltage and frequency scaling (DVFS) caution[edit source]

  • As stated above, as soon as at least two operating points are defined in the OPP table, Linux kernel will automatically switch between them at runtime thanks to Linux cpufreq framework, configured with "ondemand" governor policy (see Documentation/admin-guide/pm/cpufreq.rst ). It is important to notice that cpufreq framework is only monitoring the CPU load to select the OPP because this can lead to some limitation during use cases where the CPU is not loaded a lot but high reactivity is needed to respect some real time constraints, like interrupt management. If you face some system issue where the CPU reactivity may be the root cause whereas DVFS is enabled, consider doing a trial with "performance" governor (see Documentation/admin-guide/pm/cpufreq.rst ).
  • Selecting OPP frequencies that can be reached with RCC MPUDIV dividor and without configuring again the PLL1 is recommended in order to get the fastest switch time between the OPP.