This article describes the content of OpenSTLinux distribution software release version openstlinux-6.1-yocto-mickledore-mpu-v24.06.26, which is part of the STM32 MPU ecosystem release note - v5.1.0.
1. Intended audience[edit source]
The targeted audience is STM32MP1 series and STM32MP25x lines customers or partners.
2. Delivery scope and purpose[edit source]
The OpenSTLinux distribution is a Linux® distribution based on the OpenEmbedded build Framework. It runs on the Arm® Cortex® processors, and is a fundamental part of the STM32MPU Embedded Software distribution. This delivery of OpenSTLinux distribution is part of STM32 MPU Ecosystem v5.1.0 (see the STM32 MPU ecosystem release note - v5.1.0).
3. Licensing[edit source]
This software package is licensed under a LIMITED LICENSE AGREEMENT FOR ST MATERIALS EVALUATION (LLA). Customers may not use this package except in compliance with the software license agreement (SLA).
All packages use the same source components. All components and their respective licenses are listed here.
4. Supported hardware[edit source]
This software delivery is compatible with the following boards:
STM32MP13 boards | |||
---|---|---|---|
Boards | PCBs list | Main features | Ordering |
STM32MP135F-DK Discovery kit |
|
|
STM32MP15 boards | |||
---|---|---|---|
Boards | PCBs list | Main features | Ordering |
STM32MP157D-DK1 Discovery kit |
|
|
|
STM32MP157F-DK2 Discovery kit |
|
|
|
STM32MP157D-EV1 Evaluation board |
|
|
|
STM32MP157F-EV1 Evaluation board |
|
|
|
STM32MP157A-DK1 Discovery kit |
|
|
Out of production |
STM32MP157C-DK2 Discovery kit |
|
|
Out of production |
STM32MP157A-EV1 Evaluation board |
|
|
Out of production |
STM32MP157C-EV1 Evaluation board |
|
|
Out of production |
STM32MP25 boards | |||||
---|---|---|---|---|---|
Boards | PCBs list | Main features | Ordering | ||
STM32MP257F-EV1 Evaluation board |
|
|
|||
STM32MP257F-DK Discovery kit |
|
|
|
5. Release content[edit source]
5.1. Main software components[edit source]
- Build process
- OpenEmbedded v4.2.4 (Mickledore) - Updated
- GCC version v12.3.0 - Updated
- Embedded software components
- Linux kernel v6.1-stm32mp-r2 (v6.1.82) - Updated
- TF-A v2.8-stm32mp-r2 - Updated
- U-Boot v2022.10-stm32mp-r2 - Updated
- OP-TEE 3.19.0-stm32mp-r2 - Updated
- External DT 5.0-stm32mp-r1 - New
- OpenOCD version v0.12.0 - Updated
- Applicative components
- Weston version v11.0.1 - Updated
- Wayland version 1.21.0 - Updated
- GStreamer version v1.22.6 - Updated
- GCnano version v6.4.15 - Updated
5.2. Changes[edit source]
5.2.1. OpenSTLinux layers[edit source]
Changes are:
- Rebase on Yocto Release 4.2.4 (Mickledore)
- Support of STM32MP25x lines
- Add external-dt support
- Extlinux
- Add support of FDTOVERLAYS via U-Boot
- FIP
- New frontend: now to generate FIP you need to call "bitbake fip-stm32mp" instead of asking "tf-a-stm32mp" to generate the FIP binaries via deploy command
- Add support of STM32 MPU
- Add FIP-DDR binaries generation
- Add support of encryption
- Support generation of FIP by configuration: OP-TEE : fastboot-sdcard, fastboot-emmc, optee-usb, ...
- CONF/MACHINE
- Add support of STM32MP25x lines and associated boards
- Add fastboot support for all STM32 MPUs
- Rename NAND storage
- Nand-4-256-1024 (FMC NAND )
- Nand-4-256-512 (SPI NAND )
- Nand-2-128-256 (SPI NAND )
- Add support of OP-TEE profiles
- system_services
- secure_and_system_services
- Put SDK information on specific include file: st-image-sdk-stm32mp.inc
- Components
- Add M33projects for STM32MP25x lines
- Add TF-M-stm32mp for STM32MP25x lines (To use only with external-dt OSLT)
- Add External dt mainly for STM32MP25x lines (used also for STM32MP unknown microprocessor device Xè-LINUX-RT Expansion Package)
- Add DDR firmware for STM32MP25x lines (DDR firmware use by bl2 - TF-A)
- OP-TEE: Add OP-TEE profiles
- TF-A-TOOLS: Add wrapper to manage generation of FIP binaries: create_st_fip.sh
- Minor fixes
5.2.2. Linux® kernel[edit source]
New component release tag v6.1-stm32mp-r2 is available, rebased on official Linux® kernel v6.1.82.
Changes are:
- Storage:
- STM32MP25: OSPI Add DTR support and legacy SPI
- Visual:
- STM32MP25 boards: ADV7535 CEC support
- STM32MP25: Improve DCMIPP support
- Pipes 1 & 2 - Flow Selection, Frame Control, Frame Counter & Stat removal
- Down sizing without pixel alignment constraints
- Add post-processing decimation support
- STM32MP25: H.264 Video Encoder
- STM32MP25: Improve Display support
- Pre-processing - Cropping & rotation
- Input RGB & YUV color formats
- STM32MP25: Add I3C controller (master) Linux driver
- STM32MP25: LPUART support
- Security
- STM23MP25: Add RISAF dump debug driver
- STM23MP25: Support crypt1 in TF-A, TF-M and cryp2 in TF-M, OP-TEE, U-Boot, and Linux
- Analog:
- STM23MP25: Add MDF IIO support
- Low power support
- STM23MP25: Add Linux system suspend based on PSCI OSI
- STM23MP25: Suspend/resume support for Audio, LVDS, DSI, CSI, DCMIPP, GPU, Ethernet, PCIe, USB2/3
- Core:
- STM23MP25: CoreSight support
- STM23MP25: DAM3 driver rework
- STM23MP25: Support IWDGX in all dedicated firmware
- STM23MP25: EXT-I: use interrupts-extended instead of interrupt-map
5.2.3. U-Boot[edit source]
New component release tag v2022.10-stm32mp-r2 is available, rebased on official U-Boot v2022.10.
Changes are:
- STM32MP25x lines support
- Support STM32MP257F-DK Discovery kit ) and STM32MP257x-EV1 Evaluation board
- STM32MP25: Hyperflash support
- STM32MP25: OSPI with Dual Transfer Rate support
- Firmware Update (FWU) support for metadata v2
- Complete UEFI support
- STM32MP25: power supply support for lvds / dsi /ltdc
- STM32MP25: Add support backup registers with NVM
- STM32MP25: RIF semaphore handling in gpio
- STM32MP25: IO synchronization parameters for pinctrl
- Update FASTBOOT support
- Makefile to build the external device tree
- Other minor fixes
5.2.4. TF-A[edit source]
New component release tag v2.8-stm32mp-r2 is available, rebased on official TF-A v2.8 (LTS tag lts-v2.8.15).
Changes are:
- Rebase on LTS-v2.8.15
- STM32MP25x lines support
- Firmware Update (FWU) support for metadata v2 (metadata v1 support removed)
- STM32MP25: Qdd NVMEM driver to manage TAMP backup registers
- STM32MP25: Add RIF, STPMIC2, OSPI and hyperflash support for STM32MP2
- STM32MP25: Several bug fixes in DDR, clocks, USB, OSPI, low-power, MMC, platform code and device tree
5.2.5. OP-TEE[edit source]
New component release tag v3.19.0-stm32mp-r2 is available, rebased on official OP_TEE OS 3.19.0.
Changes are:
- Add mailbox framework
- Add NVMEM driver to manage TAMP backup registers
- OP-TEE Profiles :
- system services : PSCI, SCMI
- secure and system services : PSCI, SCMI, TA and PTA support
- STM32MP25x lines support:
- Introduction of STM32MP25 platform
- New drivers for STM32MP25 (Clock, BSEC3, RIFSC, RISAB, RISAB, SERC, IAC, IPCC, FMC, OMM)
- RIF firewall configuration (peripheral and memory)
- Power management
- SCMI server from SCP firmware
- SCMI OPP/DVFS support
- SCMI regulator support (with PMIC and I2C secure)
- Secure UI
- Minor Fixes
5.2.6. External-DT[edit source]
NEW
New component release tag v5.0-stm32mp-r1 is available.
The external device tree component is used to host STM32 MPU embedded software device tree configurations in addition of the ones present in each software component (TF-A, OP-TEE, U-BOOT, LINUX, TF-M). It is Used for STM32MP25x lines , but not yet for STM32MP1 series.
6. Release change notification[edit source]
OpenSTLinux attention points to switch from ecosystem release v5.0.0 to ecosystem release v5.1.0 are documented in STM32 MPU OpenSTLinux release changes notification – v5.1.0 article.
7. Recommendations for use[edit source]
7.1. Safe use[edit source]
- Flash programming and boot from all supported flash devices: SDCard, eMMC, ONFI NAND and NOR flash memories.
- Develop Linux® applications, libraries, kernel modules based on OpenSTLinux delivery.
- Develop coprocessor Cube applications based on STM32CubeMP1 and STM32CubeMP2 deliveries.
- Develop boards based on STM32MP1 series and STM32MP25x lines .
- Prototype applications based on ST boards.
7.2. Non-recommended use[edit source]
- None
8. Restrictions[edit source]
- dcmipp-isp-ctrl tool will fail whenever DCMIPP auxiliary pipe only is used for camera capture (need to enable DCMIPP main pipe).
STM32MP1 series
- Camera resolution limited to 320*240 / 15 fps on STM32MP157F-EV1 Evaluation board : limitation when using DCMI configuration (correction under implementation and will be delivered soon),
- The partition layout always keeps the Firmware Update related partitions even if machine feature fw-update is disabled. To optimize the partition layout without Firmware Update feature, modifications are needed on flashlayout file generation and also on U-Boot source code in case of MTD partitions (storage mapping is hardcoded for MTD partitions, see How_to_configure_U-Boot_for_your_board#MTD_partitions)
- STM32MP15x lines : Issue to boot with SPI-Nand: patches to be upstreamed on GitHub
9. Minor release updates[edit source]
STMicroelectronics regularly delivers corrections through github® components which are U-Boot , OP-TEE , TF-A , Linux kernel .
The corrections can be incorporated into the STM32MP1 Developer Package or Distribution Package (see below).
Two possibilities exist to update a Distribution Package:
- Update your existing Distribution Package:
- Switch your Distribution Package to # github® mode .
- Use the devtool modify <recipe name> command to set up an environment. It fetches and unpacks the source code.
- In the extracted source code, use a git command such as git checkout -b WORK <github® TAG> to point to a new revision of the component.
- More rarely, STMicroelectronics also delivers fixes on layers through github®. These changes can be integrated (via git commands: git checkout -b WORK <github® commit SHA1>) into the local STM32MP1 Distribution Package environment. See below the github® links of the quoted layers :
- Get a new Distribution Package:
- Refer to Installing_the_OpenSTLinux_distribution page for installing instructions, and use the repo command given for the minor version below, if it exists.
10. How to get started with openstlinux-6.1-yocto-mickledore-mpu-v24.06.26[edit source]
Refer to How to download the software and start with this release?
11. Associated tools[edit source]
Refer to the Referenced tools release notes .
12. Yocto features enabled in the delivery[edit source]
OpenEmbedded[4] build framework engine is named OE-Core.
OpenSTLinux distribution is based on the build framework OpenEmbedded, and can be configured thanks to a mechanism named "features" (machine features, distribution features, ...).
Depending on the features enabled, the resulting distribution can have more capabilities or software embedded.
For example, if the Wifi is enabled then the Wifi software and drivers are present on the filesystem and the Wifi can be used.
12.1. Machine features[edit source]
The variable MACHINE_FEATURES specifies the list of hardware features the machine is capable of supporting.
These features (MACHINE_FEATURES) are defined inside the machine configuration .
12.2. Distribution features[edit source]
The variable DISTRO_FEATURES specifies the list of software features present in the distribution.
These features (DISTRO_FEATURES) are defined inside the distribution configuration .
Distribution feature | Purpose |
---|---|
alsa | Include ALSA support (OSS compatibility kernel modules installed if available). |
argp | |
autoresize | Add support of userfs auto resize feature in OpenSTLinux |
bluetooth | Include Bluetooth support |
bluez5 | Add Bluetooth stack |
efi | Add userland EFI tools |
ext2 | Add Second Extended File System support |
ext4 | Add Fourth Extended File System support |
gobject-introspection-data | Enable GObject Introspection, project for providing machine readable introspection data of the API of C libraries. |
gplv3 | Add gplv3 binaries in OpenSTLinux |
gstreamer | Add gstreamer tools in filesystem |
initrd | Add ramdisk |
ipv4 | Add ipv4 support |
ipv6 | Add ipv6 support |
kde | Add several tools (e.g. cups, fontconfig, ...) to the filesystem |
largefile | Enable large file support |
ldconfig | Include support for ldconfig and ld.so.conf on the target |
multiarch | Enable 64 bits BFD (Binary File Descriptor) |
nfs | Include NFS client support (for mounting NFS exports on device). |
opengl | Include the Open Graphics Library |
optee | Install tee service on the filesystem |
pam | Enable Pluggable Authentication Module |
pci | Add pci support |
pulseaudio | Network-capable sound server program |
splashscreen | Add U-Boot splashscreen |
systemd | Use systemd as init service |
usbgadget | USB Gadget Device support (for USB networking/serial/storage) |
usbhost | USB Host support (allows to connect external keyboard, mouse, storage, network etc) |
wayland | Add Wayland support |
wifi | WiFi support |
xattr | Add "Extended Attributes" support for filesystem |
zeroconf | Add zeroconf package to set up a ad-hoc network |
12.3. Bootscheme labels[edit source]
The variable BOOTSCHEME_LABELS defines which kind of boot is supported on the board.
These settings (BOOTSCHEME_LABELS) are defined inside the machine configuration .
Bootscheme label | Purpose |
---|---|
optee | Add OP-TEE in boot scheme |
12.4. Bootdevice labels[edit source]
The variable BOOTDEVICE_LABELS defines which kind of mass storage OpenSTLinux can program.
These settings (BOOTDEVICE_LABELS ) are defined inside the machine configuration .
Bootdevice label | Purpose |
---|---|
emmc | Add boot on eMMC device |
nand-4-256 | Add boot on NAND device |
nor-sdcard | Add boot stage on NOR device and the filesystem on SD card |
sdcard | Add boot on SD card |