1. STM32CubeMX 6.12.0 - MPU support[edit source]
1.1. New features supported in this releases[edit source]
- Support of STM32CubeMP2 package running on the Arm® Cortex®-A35 and Arm® Cortex®-M33 processors.
- Add a new feature called Resource Isolation Framework (RIF) which acts as a security guard for certain components of the microcontroller (peripherals) and its memory.
1.2. Features already supported in previous releases[edit source]
- Support of STM32CubeMP13 package running on the Arm® Cortex®-A7 processor.
- Support of STM32CubeMP15 package running on the Arm® Cortex®-A7 and Arm® Cortex®-M4 processors.
- Support for Azure RTOS ThreadX, FileX, LevelX, NETX and USBX, for STM32CubeMP13 package release
1.3. Main changes coming with new release[edit source]
- STM32MP135x A/C CPU max frequency was wrongly set to 900 MHZ instead of 650 MHZ.
- CLK_RTC_LSE not generated in TF-A DT (default configuration)
1.4. Known limitations[edit source]
1.4.1. With STM32CubeMP13 package[edit source]
- Only STM32CubeIDE is supported
- Only application context is supported
- Standard version of LevelX, USBX, NetX middlewares integrated without STM32MP13 platform specific patches.
- When using the STM32CubeMP13 package and activating Azure® RTOS ThreadX, the STM32CubeIDE linker file must contain the following section to avoid compilation issues:
.stack :
{
_stack_bottom = ABSOLUTE(.) ;
/* Allocate room for stack. This must be big enough for the
IRQ, FIQ, and SYS stack if nested interrupts are
enabled.*/
. = ALIGN(8) ;
. += 32768 ;
_sp = . - 16 ;
_stack_top = ABSOLUTE(.) ;
} >RAM
_end = .;
2. How to get STM32CubeMX[edit source]
STM32CubeMX for Linux®, Windows® and macOS ® | ||
---|---|---|
Download |
Version 6.11.0
| |
Installation guide |
| |
User manual |
| |
Detailed release note |
|
Minor releases may be available from the update site.