HPDMA device tree configuration

Revision as of 10:01, 21 May 2024 by Registered User
Applicable for STM32MP25x lines

1. Article purpose[edit source]

This article explains how to configure the HPDMA internal peripheral when it is assigned to the Linux® OS. In that case, it is controlled by the DMA Engine (Refer to Dmaengine overview).

The configuration is performed using the Device tree mechanism that provides a hardware description of the HPDMA internal peripheral, used by the STM32 DMA3 Linux driver and by the DMA framework.

Hardware description is a combination of:

  • STM32 HPDMA peripheral
  • STM32 HPDMA client

2. DT bindings documentation[edit source]

Complete device tree bindings can be found at this location: [1].

3. DT configuration[edit source]

This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.

STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.

3.1. DT configuration (STM32 level)[edit source]

The STM32MP2 HPDMA node is located

  • for STM32MP25x lines More info.png in stm32mp251.dtsi [2]


For example, at device level, the HPDMA is declared as follows:

hpdma: dma-controller@40400000 {
	compatible = "st,stm32-dma3";
	reg = <0x40400000 0x1000>;
	interrupts = <GIC_SPI 33 IRQ_TYPE_LEVEL_HIGH>,
		     <GIC_SPI 34 IRQ_TYPE_LEVEL_HIGH>,
		     <GIC_SPI 35 IRQ_TYPE_LEVEL_HIGH>,
		     <GIC_SPI 36 IRQ_TYPE_LEVEL_HIGH>,
		     <GIC_SPI 37 IRQ_TYPE_LEVEL_HIGH>,
		     <GIC_SPI 38 IRQ_TYPE_LEVEL_HIGH>,
		     <GIC_SPI 39 IRQ_TYPE_LEVEL_HIGH>,
		     <GIC_SPI 40 IRQ_TYPE_LEVEL_HIGH>,
		     <GIC_SPI 41 IRQ_TYPE_LEVEL_HIGH>,
		     <GIC_SPI 42 IRQ_TYPE_LEVEL_HIGH>,
		     <GIC_SPI 43 IRQ_TYPE_LEVEL_HIGH>,
		     <GIC_SPI 44 IRQ_TYPE_LEVEL_HIGH>,
		     <GIC_SPI 45 IRQ_TYPE_LEVEL_HIGH>,
		     <GIC_SPI 46 IRQ_TYPE_LEVEL_HIGH>,
		     <GIC_SPI 47 IRQ_TYPE_LEVEL_HIGH>,
		     <GIC_SPI 48 IRQ_TYPE_LEVEL_HIGH>;
	clocks = <&scmi_clk CK_SCMI_HPDMA1>;
	power-domains = <&RET_PD>;
	#dma-cells = <4>;
	st,axi-max-burst-len = <16>;
};
Warning white.png Warning
This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.

3.2. DT configuration (board level)[edit source]

reserved-memory {
	#address-cells = <2>;
	#size-cells = <2>;
	ranges;

	[...]
	hpdma1_lli: hpdma1-lli@a020000 {
		reg = <0x0 0xa020000 0x0 0xf0f0>;
		no-map;
	};
	[...]
};
&hpdma {
	memory-region = <&hpdma1_lli>;
};

Board device tree configuration can be used to specify memory-region property pointing on reserved memory used for HPDMA internal descriptors.

4. How to configure the DT using STM32CubeMX[edit source]

The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.

5. References[edit source]

Please refer to the following links for additional information: