This article introduces the structure and the content of the STM32CubeMP25 Package, the embedded software part of STM32Cube™, running on the Arm® Cortex®-M33 processor. It references also other interesting wiki articles to better understand and use the STM32CubeMP25 Package.
1. What is the STM32CubeMP25 Package[edit source]
STM32CubeMP25 Package, running on the Arm® Cortex®-M33 processor, consists of:
- The hardware abstraction layer (HAL), enabling portability between different STM32 devices via standardized API calls
- The low-layer API (LL), a light-weight, optimized, expert oriented set of APIs designed for runtime efficiency and so enhanced performance
- The board support package drivers (BSP), based on HAL drivers, an API set for the evaluation board and third-party components.
- A collection of middleware components (such as AzureRTOS)
- A collection of examples, running on an MPU board and allowing demonstration of a basic implementation of features from a set of IPs
2. Software architecture overview[edit source]
Software architecture overview is described in STM32CubeMP25 Package architecture.
3. STM32CubeMP25 Package structure[edit source]
This chapter describes the structure of the STM32CubeMP25 Package (drivers, middleware components...).
STM32CubeMP25 Package offers a highly portable Hardware Abstraction Layer (HAL), built around a generic and modular architecture.
This HAL allows the upper layers, middleware and application, to implement functions whenever STM32MP25 device is used. This improves the library code re-usability and guarantees easy portability from one device to another. STM32CubeMP25 Package also offers a highly portable Low Layer interface (LL), which allows a quick, simple and optimized API to access the STM32MP25 registers.
The STM32CubeMP25 Package is provided with the structure shown below.
4. STM32CubeMP25 Package content[edit source]
This chapter describes the content of the STM32CubeMP25 Package (drivers, middleware components...).
4.1. Drivers[edit source]
The Drivers folder contains all the STM32Cube Drivers, including BSP and HAL drivers.
4.1.1. HAL drivers[edit source]
STM32CubeMP25 HAL Driver items | Description |
---|---|
ADC |
* This driver provides firmware functions to manage the following * functionalities of the Analog to Digital Convertor (ADC) * peripheral: * + Initialization and de-initialization functions * ++ Initialization and Configuration of ADC * + Operation functions * ++ Start, stop, get result of conversions of regular * group, using 3 possible modes: polling, interruption or DMA. * + Control functions * ++ Channels configuration on regular group * ++ Analog Watchdog configuration * + State functions * ++ ADC state machine management * ++ Interrupts and flags management |
ADC_EX |
* This driver provides firmware functions to manage the following * extended functionalities of the Analog to Digital Convertor (ADC) * peripheral: * + Operation functions * ++ Start, stop, get result of conversions of ADC group injected, * using 2 possible modes: polling, interruption. * ++ Calibration * +++ ADC automatic self-calibration * +++ Calibration factors get or set * ++ Multimode feature when available * + Control functions * ++ Channels configuration on ADC group injected * + State functions * ++ ADC group injected contexts queue management |
BSEC |
* This driver provides firmware functions to manage the following * functionalities of the Boot and security and OTP control(BSEC) peripheral: * + Initialization and de-initialization functions * + Peripheral Control functions * + Peripheral State functions |
CRC |
* This driver provides firmware functions to manage the following
* functionalities of the Cyclic Redundancy Check (CRC) peripheral:
* + Initialization and de-initialization functions
* + Peripheral Control functions
* + Peripheral State functions
* + Extended features functions
|
CRYP |
* This driver provides firmware functions to manage the following * functionalities of the Cryptography (CRYP) peripheral: * + Initialization and de-initialization functions * + AES processing functions * + DES processing functions * + TDES processing functions * + DMA callback functions * + CRYP IRQ handler management * + Peripheral State functions |
CRYP_EX |
* This driver provides firmware functions to manage the following * functionalities of CRYP extension peripheral: * + Extended AES processing functions |
CSI |
* This file provides firmware functions to manage the following * functionalities of the Digital Camera Interface (CSI) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Error functions |
DCACHE |
* This file provides firmware functions to manage the following * functionalities of the DCACHE. * + Initialization and Configuration * + Cache coherency command * + Monitoring management |
DCMI |
* This file provides firmware functions to manage the following * functionalities of the Digital Camera Interface (DCMI) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Error functions |
DCMIPP |
* This driver provides firmware functions to manage the following * functionalities of the DCMIPP (Digital Camera Interface Pixel Pipeline) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Error functions |
DDR |
* This driver provides firmware functions to manage the following
* functionalities of the Double Data Rate Synchronous Dynamic Random
* Access Memory (DDR-SDRAM) Peripheral, through its controller
* (DDRCTRL) and its physical interface controller (DDRPHYC).
|
DMA |
* This driver provides firmware functions to manage the following * functionalities of the Direct Memory Access (DMA) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral State and errors functions |
DMA_EX |
* This driver provides firmware functions to manage the following
* functionalities of the DMA Extension peripheral:
* + Extended features functions
|
DSI |
* This file provides firmware functions to manage the following * functionalities of the DSI peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Errors functions |
ETH |
* This driver provides firmware functions to manage the following * functionalities of the Ethernet (ETH) peripheral: * + Initialization and deinitialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Errors functions |
EXTI |
* This driver provides firmware functions to manage the following * functionalities of the General Purpose Input/Output (EXTI) peripheral: * + Initialization and de-initialization functions * + IO operation functions |
FDCAN |
* This driver provides firmware functions to manage the following
* functionalities of the Flexible DataRate Controller Area Network
* (FDCAN) peripheral:
* + Initialization and de-initialization functions
* + IO operation functions
* + Peripheral Configuration and Control functions
* + Peripheral State and Error functions
|
GPIO |
* This driver provides firmware functions to manage the following * functionalities of the General Purpose Input/Output (GPIO) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Extended Peripheral Control functions |
HAL |
* This driver provides firmware functions to manage the following * functionalities of HAL, Tick, SYSCFG, DBGMCU: * + Initialization and de-initialization functions * + HAL Initialization and de-initialization functions * + Configure the source of the time base * + HAL Control functions * + Tick management (get/set/inc/priority/suspend/resume) * + Get HAL revision, the device revision identifier, the device identifier * + Enable/Disable DBG wake up on AIEC * + Enable/Disable the Debug Module during Domain1 SLEEP mode * + Enable/Disable the Debug Module during Domain1 STOP mode * + Enable/Disable the Debug Module during Domain1 STANDBY mode * + Configure the internal voltage reference buffer voltage scale * + Configure the internal voltage reference buffer high impedance mode * + Tune the Internal Voltage Reference buffer (VREFBUF) * + Enable/Disable the Internal Voltage Reference buffer (VREFBUF) * + Ethernet PHY Interface Selection either MII or RMII * + Analog Switch control for dual analog pads * + Enable/Disable the booster to reduce the total harmonic distortion of the analog * + Enable/Power-down the I/O Compensation Cell * + To Enable/Disable optimize the I/O speed when the product voltage is low * + Code selection for the I/O Compensation cell |
HASH |
* This driver provides firmware functions to manage the following * functionalities of the HASH peripheral: * + Initialization and de-initialization methods * + HASH or HMAC processing in polling mode * + HASH or HMAC processing in interrupt mode * + HASH or HMAC processing in DMA mode * + Peripheral State methods * + HASH or HMAC processing suspension/resumption |
HASH_EX |
* This driver provides firmware functions to manage the following * functionalities of the HASH peripheral for SHA-224 and SHA-256 * algorithms: * + HASH or HMAC processing in polling mode * + HASH or HMAC processing in interrupt mode * + HASH or HMAC processing in DMA mode * Additionally, this file provides functions to manage HMAC * multi-buffer DMA-based processing for MD-5, SHA-1, SHA-224 * and SHA-256. |
HSEM |
* This file provides firmware functions to manage the following * functionalities of the semaphore peripheral: * + Semaphore Take function (2-Step Procedure) , non blocking * + Semaphore FastTake function (1-Step Procedure) , non blocking * + Semaphore Status check * + Semaphore Clear Key Set and Get * + Release and release all functions * + Semaphore notification enabling and disabling and callback functions * + IRQ handler management |
ICACHE |
* This file provides firmware functions to manage the following * functionalities of the Instruction Cache (ICACHE). * + Initialization and Configuration * + Invalidate functions * + Monitoring management * + Memory address remap management |
IPCC |
* This file provides firmware functions to manage the following
* functionalities of the Inter-Processor communication controller
* peripherals (IPCC).
* + Initialization and de-initialization functions
* + Configuration, notification and interrupts handling
* + Peripheral State and Error functions
|
I2C |
* This driver provides firmware functions to manage the following * functionalities of the Inter Integrated Circuit (I2C) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral State and Errors functions |
I2C_EX |
* This driver provides firmware functions to manage the following
* functionalities of I2C Extended peripheral:
* + Filter Mode Functions
* + WakeUp Mode Functions
* + FastModePlus Functions
|
I2S |
* This file provides firmware functions to manage the following * functionalities of the Integrated Interchip Sound (I2S) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral State and Errors functions |
I3C |
* This file provides firmware functions to manage the following
* functionalities of the Improvement Inter Integrated Circuit (I3C) peripheral:
* + Initialization and de-initialization functions
* + IO operation functions
* + Peripheral State and Errors functions
|
IWDG |
* This file provides firmware functions to manage the following * functionalities of the Independent Watchdog (IWDG) peripheral: * + Initialization and Start functions * + IO operation functions |
LPTIM |
* This driver provides firmware functions to manage the following
* functionalities of the Low Power Timer (LPTIM) peripheral:
* + Initialization and de-initialization functions.
* + Start/Stop operation functions in polling mode.
* + Start/Stop operation functions in interrupt mode.
* + Reading operation functions.
* + Peripheral State functions.
|
LTDC |
* This file provides firmware functions to manage the following * functionalities of the LTDC peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Errors functions |
MCE |
* This driver provides firmware functions to manage the following * functionalities of the Memory Cipher Engine (MCE) Peripheral. |
MMC |
* This driver provides firmware functions to manage the following * functionalities of the Secure Digital (MMC) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + MMC card Control functions |
MMC_EX |
* This driver provides firmware functions to manage the following
* functionalities of the Secure Digital (MMC) peripheral:
* + Extended features functions
|
PCD |
* This driver provides firmware functions to manage the following
* functionalities of the USB Peripheral Controller:
* + Initialization and de-initialization functions
* + IO operation functions
* + Peripheral Control functions
* + Peripheral State functions
|
PCD_EX |
* This driver provides firmware functions to manage the following * functionalities of the USB Peripheral Controller: * + Extended features functions |
PKA |
* This driver provides firmware functions to manage the following * functionalities of public key accelerator(PKA): * + Initialization and de-initialization functions * + Start an operation * + Retrieve the operation result |
PSSI |
* This file provides firmware functions to manage the following
* functionalities of the Parallel Synchronous Slave Interface (PSSI) peripheral:
* + Initialization and de-initialization functions
* + IO operation functions
* + Peripheral State and Errors functions
|
PWR |
* This driver provides firmware functions to manage the following * functionalities of the Power Controller (PWR) peripheral: * + Initialization and de-initialization functions * + Peripheral Control functions * + Peripheral Extended features functions |
PWR_EX |
* This driver provides firmware functions to manage the following * functionalities of PWR extension peripheral: * + Peripheral Extended features functions |
XSPI |
* This driver provides firmware functions to manage the following * functionalities of the XSPI interface (XSPI). * + Initialization and de-initialization functions * + Indirect functional mode management * + Memory-mapped functional mode management * + Auto-polling functional mode management * + Interrupts and flags management * + MDMA channel configuration for indirect functional mode * + Errors management and abort functionality |
RAMCFG |
* This file provides firmware functions to manage the following * functionalities of the RAMs configuration controller peripheral: * + RAMCFG Initialization and De-initialization Functions. * + RAMCFG ECC Operation Functions. * + RAMCFG CRC Operation Functions. * + RAMCFG Configure Wait State Functions. * + RAMCFG Write Protection Functions. * + RAMCFG Erase Operation Functions. * + RAMCFG Handle Interrupt and Callbacks Functions. * + RAMCFG State and Error Functions. |
RCC |
* This driver provides firmware functions to manage the following
* functionalities of the Reset and Clock Control (RCC) peripheral:
* + Initialization and de-initialization functions
* + Peripheral Control functions
* + Extended Peripheral Control functions
|
RCC_EX |
* This driver provides firmware functions to manage the following
* functionalities RCC extension peripheral:
* + Extended Peripheral Control functions
|
RIF |
* This file provides firmware functions to manage the following * functionalities of RIF: * + RISC Initialization and Configuration functions * + IAC Initialization and Configuration functions |
RNG |
* This driver provides firmware functions to manage the following
* functionalities of the Random Number Generator (RNG) peripheral:
* + Initialization and configuration functions
* + Peripheral Control functions
* + Peripheral State functions
|
RNG_EX |
* This driver provides firmware functions to manage the following * functionalities of the Random Number Generator (RNG) peripheral: * + Lock configuration functions * + Reset the RNG |
RTC |
* This driver provides firmware functions to manage the following * functionalities of the Real-Time Clock (RTC) peripheral: * + Initialization/de-initialization functions * + Calendar (Time and Date) configuration * + Alarms (Alarm A and Alarm B) configuration * + WakeUp Timer configuration * + TimeStamp configuration * + Tampers configuration * + Backup Data Registers configuration * + RTC Tamper and TimeStamp Pins Selection * + Interrupts and flags management |
RTC_EX |
* This driver provides firmware functions to manage the following * functionalities of the Real Time Clock (RTC) Extended peripheral: * + RTC Time Stamp functions * + RTC Tamper functions * + RTC Wake-up functions * + Extended Control functions * + Extended RTC features functions |
SAI |
* This driver provides firmware functions to manage the following
* functionalities of the Serial Audio Interface (SAI) peripheral:
* + Initialization/de-initialization functions
* + I/O operation functions
* + Peripheral Control functions
* + Peripheral State functions
|
SAI_EX |
* This driver provides firmware functions to manage the following
* functionality of the SAI Peripheral Controller:
* + Modify PDM microphone delays.
|
SD |
* This driver provides firmware functions to manage the following * functionalities of the Secure Digital (SD) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State functions |
SD_EX |
* This driver provides firmware functions to manage the following
* functionalities of the Secure Digital (SD) peripheral:
* + Extended features functions
|
SMARTCARD |
* This driver provides firmware functions to manage the following
* functionalities of the Smartcard peripheral:
* + Initialization and de-initialization functions
* + IO operation functions
* + Peripheral Control functions
* + Peripheral State and Error functions
* + Extended features functions
|
SMARTCARD_EX |
* This driver provides extended firmware functions to manage the following * functionalities of the SmartCard. * + Initialization and de-initialization functions * + Peripheral Control functions |
SMBUS |
* This driver provides firmware functions to manage the following * functionalities of the System Management Bus (SMBus) peripheral, * based on I2C principles of operation : * + Initialization and de-initialization functions * + IO operation functions * + Peripheral State and Errors functions |
SPDIFRX |
* This driver provides firmware functions to manage the following
* functionalities of the SPDIFRX audio interface:
* + Initialization and Configuration
* + Data transfers functions
* + DMA transfers management
* + Interrupts and flags management
|
SPI |
* This driver provides firmware functions to manage the following * functionalities of the Serial Peripheral Interface (SPI) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State functions |
SPI_EX |
* This driver provides firmware functions to manage the following * SPI peripheral extended functionalities : * + IO operation functions * + Peripheral Control functions |
FMC_SRAM |
* This driver provides a generic firmware to drive SRAM memories * mounted as external device. |
FMC_NAND |
* This driver provides a generic firmware to drive NAND memories * mounted as external device. |
TIMER |
* This driver provides firmware functions to manage the following * functionalities of the Timer (TIM) peripheral: * + TIM Time Base Initialization * + TIM Time Base Start * + TIM Time Base Start Interruption * + TIM Time Base Start DMA * + TIM Output Compare/PWM Initialization * + TIM Output Compare/PWM Channel Configuration * + TIM Output Compare/PWM Start * + TIM Output Compare/PWM Start Interruption * + TIM Output Compare/PWM Start DMA * + TIM Input Capture Initialization * + TIM Input Capture Channel Configuration * + TIM Input Capture Start * + TIM Input Capture Start Interruption * + TIM Input Capture Start DMA * + TIM One Pulse Initialization * + TIM One Pulse Channel Configuration * + TIM One Pulse Start * + TIM Encoder Interface Initialization * + TIM Encoder Interface Start * + TIM Encoder Interface Start Interruption * + TIM Encoder Interface Start DMA * + Commutation Event configuration with Interruption and DMA * + TIM OCRef clear configuration * + TIM External Clock configuration |
TIMER_EX |
* This driver provides firmware functions to manage the following
* functionalities of the Timer Extended peripheral:
* + Time Hall Sensor Interface Initialization
* + Time Hall Sensor Interface Start
* + Time Complementary signal break and dead time configuration
* + Time Master and Slave synchronization configuration
* + Time Output Compare/PWM Channel Configuration (for channels 5 and 6)
* + Timer remapping capabilities configuration
|
UART |
* This driver provides firmware functions to manage the following * functionalities of the Universal Asynchronous Receiver Transmitter Peripheral (UART). * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions |
UART_EX |
* This driver provides firmware functions to manage the following extended
* functionalities of the Universal Synchronous Receiver Transmitter Peripheral (USART).
* + Peripheral Control functions
|
U(S)ART |
* This driver provides firmware functions to manage the following * functionalities of the Universal (Synchronous) Asynchronous Receiver Transmitter * Peripheral (U(S)ART). * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Error functions * + Peripheral Control functions |
4.1.2. LL drivers[edit source]
STM32CubeMP25 LL Driver items | Description |
---|---|
ADC |
* This driver provides firmware functions to manage the following * functionalities of the ADC peripheral: * + Initialization/de-initialization functions * + Configuration functions (ADC instance, group regular, group injected, * channels, analog watchdog, oversampling, multimode) * + IT/FLAGS management functions |
DELAYBLOCK |
* This file provides firmware functions to manage the following * functionalities of the DelayBlock peripheral: * + input clock frequency * + up to 12 oversampling phases |
DMA |
* This driver provides firmware functions to manage the following
* functionalities of the DMA peripheral:
* + Initialization/de-initialization functions
* + Configuration functions
* + IT/FLAGS management functions
|
EXTI |
* This driver provides firmware functions to manage the following
* functionalities of the EXTI peripheral:
* + Initialization/de-initialization functions
* + IT/FLAGS/Trigger management functions
* + Configuration functions
|
FMC |
* This driver provides firmware functions to manage the following * functionalities of the Flexible Memory Controller (FMC) peripheral memories: * + Initialization/de-initialization functions * + Peripheral Control functions * + Peripheral State functions |
GPIO |
* This driver provides firmware functions to manage the following
* functionalities of the GPIO peripheral:
* + Initialization/de-initialization functions
* + Data access functions
* + Port configuration functions
|
I2C |
* This driver provides firmware functions to manage the following * functionalities of the I2C peripheral: * + Initialization/de-initialization functions * + IT/FLAGS management functions * +Data management functions * + Configuration functions |
LPTIM |
* This driver provides firmware functions to manage the following * functionalities of the LPTIM peripheral: * + Initialization/de-initialization functions * + IT/FLAGS management functions * + Configuration (Trigger / Clock / Encoder / LPTIM) functions |
DMA |
* This driver provides firmware functions to manage the following * functionalities of the Direct Memory Access (DMA) peripheral: * + Channel Mangenment functions (Instance, Block, Buffer, Endianess etc) * + SRC/DES operation functions * + HW Trigger control |
PWR |
* This driver provides firmware functions to manage the following * functionalities of the PWR peripheral: * + De-initialization functions |
RCC |
* This driver provides firmware functions to manage the following * functionalities of the RCC peripheral: * + Clocks management functions (HSE/HSI/CSI/LSE/LSI/MCO/PLL) * + RTC/TIMERS functions * + IT/FLAGS management functions * + De-initialization functions * + Get system and peripherals clocks frequency functions |
RTC |
* This driver provides firmware functions to manage the following
* functionalities of the RTC peripheral:
* + Initialization/de-initialization functions
* + TIME/DATE/ALM functions
* + Configuration functions
|
SDMMC |
* This driver provides firmware functions to manage the following
* functionalities of the SDMMC peripheral:
* + Initialization/de-initialization functions
* + IT/FLAGS management functions
* + Data / DMA management functions
* + Configuration functions
|
SPI |
* This driver provides firmware functions to manage the following
* functionalities of the SPI peripheral:
* + Control and configuration functions
|
TIM |
* This driver provides firmware functions to manage the following * functionalities of the TIM peripheral: * + Initialization/de-initialization functions * + Configuration functions (Time base, Capture Compare, Output and Input Channel, * Timer Synchro, Break, DMA Burst Mode ) * + Counter clock selection functions * + Timer input remapping functions * + IT/FLAGS management functions * + DMA management functions * + Event management functions |
USART |
* This driver provides firmware functions to manage the following * functionalities of the USART peripheral: * + Initialization/de-initialization functions * + Configuration functions (Irda, Smartcard, Half duplex, * SPI Slave, LIN, Driver enable) * + Advanced configurations services functions * + IT/FLAGS management functions * + DMA management functions * + Data management functions * + Execution functions |
USB |
* This driver provides firmware functions to manage the following * functionalities of the USB Peripheral Controller: * + Initialization/de-initialization functions * + I/O operation functions * + Peripheral Control functions * + Peripheral State functions |
4.1.3. BSP drivers[edit source]
The BSP (Board Specific Package) drivers are parts of the STM32CubeMPU package based on the HAL drivers and provide a set of high level APIs relative to the hardware components and features in the STM32MP257x-EV1 Evaluation board . It provides API for LED, button and COM ports.
STM32CubeMP25 BSP Driver items |
---|
STM32MP257F-EV1 |
stm32mp257f_eval_bus.c stm32mp257f_eval_bus.h stm32mp257f_eval.c stm32mp257f_eval_camera.c stm32mp257f_eval_camera.h stm32mp257f_eval_conf_template.h stm32mp257f_eval_errno.h stm32mp257f_eval.h stm32mp257f_eval_pmic.c stm32mp257f_eval_pmic.h stm32mp257f_eval_usbpd_pwr.c stm32mp257f_eval_usbpd_pwr.h |
BSP Components are external components which can be attached to STM32MP257x-EV1 Evaluation board .
STM32CubeMP25 BSP Component Items | Description |
---|---|
Common |
This directory contains the BSP Common components drivers.
|
STPMIC2 |
This driver provides a set of functions offered needed to drive STPMIC2 PMU module.
|
TCPP0203 |
This driver provides a set of functions neede to drive TCPP02/03 Type-C port protection. |
4.2. Projects[edit source]
The "Projects" folder contains all STM32Cube examples that are classified in 3 ways as described below :
- Examples: It uses only the HAL drivers without any middleware component. They are available in directory Projects/<board_name>/Examples.
- Applications: It provides typical use cases of each middleware component. They are available in directory Projects/<board_name>/Applications.
- Demonstrations: This program demonstrates the USBPD stack. Directory Projects/<board_name>/Demonstrations.
List of Projects is available here. Unsupported domain!
4.2.1. Examples, applications and demonstrations for STM32MP257F-EV1 Evaluation board [edit source]
├── Application │ ├── FileX │ │ ├── Fx_NoR_Write_Read_File │ │ └── Fx_SRAM_File_Standalone │ ├── NetXDuo │ │ ├── Nx_Iperf │ │ ├── Nx_MQTT_Client │ │ ├── Nx_TCP_Echo_Client │ │ ├── Nx_TCP_Echo_Server │ │ ├── Nx_UDP_Echo_Client │ │ └── Nx_UDP_Echo_Server │ ├── OpenAMP │ │ └── OpenAMP_TTY_echo │ ├── TFM │ │ └── TFM_Protected_Storage │ ├── ThreadX │ │ ├── Tx_Thread_Creation │ │ ├── Tx_Thread_MsgQueue │ │ └── Tx_Thread_Sync │ └── USBPD │ └── USBPD_DRP_UCSI ├── Demonstrations │ └── USBPD_DRP_UCSI │ └── util └── Examples ├── CORTEX │ └── CORTEXM_ModePrivilege ├── CRC │ ├── CRC_Bytes_Stream_7bit_CRC │ └── CRC_UserDefinedPolynomial ├── CRYP │ ├── CRYP_AES_DMA │ └── CRYP_AESGCM ├── DMA │ ├── DMA_LinkedList │ └── DMA_RepeatedBlock ├── GPIO │ └── GPIO_EXTI ├── I2C │ ├── I2C_TwoBoards_ComDMA │ └── I2C_TwoBoards_ComPolling ├── I3C │ └── I3C_Controller_I2C_ComDMA ├── LPTIM │ └── LPTIM_PulseCounter ├── SPI │ └── SPI_FullDuplex_ComDMA └── TIM ├── TIM_DMABurst ├── TIM_OnePulse ├── TIM_PWMOutput └── TIM_TimeBase
4.2.2. Get started with STM32CubeMP25 Package[edit source]
To know how to get it, read STM32CubeMP25_Package_-_Getting_started article.