Some typical issues related to the PCIe feature are listed below. Solutions or debugging methods are proposed for these issues.
If your issue is not listed, try also looking in the articles in the Category:PCIe or troubleshooting grids categories.
Symptom | Resolution | |
---|---|---|
lspci doesn't show device. Device not enumerated | A possible issue is that the common reference clock is not started, check that the clkreq# sideband signal correctly toggles to low.
If it remains high, which indicates a non-conformant connection, force the GPIO to low in the device tree pcie_rc node: &pcie_rc { - pinctrl-names = "default", "init", "sleep"; - pinctrl-0 = <&pcie_pins_a>; - pinctrl-1 = <&pcie_init_pins_a>; - pinctrl-2 = <&pcie_sleep_pins_a>; + pinctrl-names = "default", "sleep"; + pinctrl-0 = <&pcie_init_pins_a>; + pinctrl-1 = <&pcie_sleep_pins_a>; note, by forcing the clkreq# to be always low, the host PCIe controller will not be able to enter in low power (ASPM) mode if enabled |
|
AER messages are flooding the console log | AER messages can be disabled with the pci=noaer command line option. However too many errors indicates either an issue with the device or the PCIe link. PCIe Electrical compliance characterization must be performed, and the reference clock Eye Diagram performed to check Jitter or power ranges characteristics
|