How to use the DCMIPP ISP

Applicable for STM32MP25x lines

1. Article purpose[edit source]

The purpose of this article is to provide guidance on managing the ISP block within the DCMIPP , utilizing the Video4Linux2 (V4L2) framework on the Linux® OS.

2. Overview of DCMIPP ISP Block Diagram[edit source]

2.1. Block diagram[edit source]

Block diagram of DCMIPP ISP Block (extracted from the STM32 MPU reference manuals)

The DCMIPP ISP, which is shared by both pipe1 and pipe2 and is instantiated only once, includes capabilities such as:

  • Statistic removal: Eliminates unnecessary metadata, like statistics, from the images received.
  • Bad-pixel removal: Automatically identifies and fixes bad pixels in the sensor array.
  • Decimation: Reduces the number of pixels to a maximum of 2688 by selecting one pixel out of every 1, 2, 4, or 8.
  • Black level correction: Adjusts the black level for each pixel in the red, green, and blue channels.
  • Exposure control: Increases the exposure from 0.0 up to 255.99 times.
  • Demosaicing: Transforms RawBayer format to RGB and supports NIR patterns of sizes 2x2 and 4x4.
  • Statistics extract: Computes average values for red, green, blue, and luminance, including dynamic bins.
  • Color conversion: Offers color conversion with flexible, fully programmable coefficients.
  • Contrast:Enhances contrast through luminance adjustment.

Refer to the STM32 MPU reference manuals for the complete list of features.


2.2. The software topology[edit source]

DCMIPP media-controller software topology

The diagram presented above illustrates the complete media-controller topology of the DCMIPP, including the ISP subdevice called dcmipp_main_isp.

Full control of the ISP is done by using both the v4l2-subdev pad API and dedicated video devices linked to the dcmipp_main_isp subdev.

All settings affecting the frame size or format are done via the dcmipp_main_isp pad (such as format, compose and crop settings), while others features are managed through two video device. The dcmipp_main_isp_params_output video output device allows to inject ISP block configuration while dcmipp_main_isp_stat_capture video capture device allows for control and capture of statistics data generated by the ISP.

3. DCMIPP ISP frame size & format control[edit source]

3.1. Mapping between HW features and v4l2-subdev pad api[edit source]

The table below outlines the association of features that can be accessed using the v4l2 sub-device pad API.

Feature / Block Integration with dcmipp_main_isp
Statistic removal crop selection on pad[0] (SINK), with only the top and height fields valid
Decimation compose selection on pad[0], with only width and height fields valid (SINK)
Demosaicing Automatically activated when ISP block input format on pad[0] (SINK) is a RAW format

3.1. Example (demosaicing / stat removal / decimation)[edit source]

Following media-ctl tool output illustrate a configuration of the dcmipp_main_isp subdev allowing:

  • demosaicing
  • removal of top 10 lines and bottom 2 lines of statistics
  • 2 time decimation of the frame
- entity 13: dcmipp_main_isp (4 pads, 5 links)
            type V4L2 subdev subtype Unknown flags 0
            device node name /dev/v4l-subdev2
	pad0: Sink
		[fmt:SRGGB10_1X10/2592x1940 field:none colorspace:rec709
		 crop.bounds:(0,0)/2592x1940
		 crop:(0,10)/2592x1928
		 compose:(0,0)/1296x964]
		<- "dcmipp_input":2 [ENABLED,IMMUTABLE]
	pad1: Source
		[fmt:RGB888_1X24/1296x964 field:none colorspace:rec709]
		-> "dcmipp_main_postproc":0 [ENABLED,IMMUTABLE]
		-> "dcmipp_aux_postproc":0 []
	pad2: Sink
		[fmt:RGB888_1X24/1296x964 field:none colorspace:rec709]
		<- "dcmipp_main_isp_params_output":0 [ENABLED,IMMUTABLE]
	pad3: Source
		[fmt:RGB888_1X24/1296x964 field:none colorspace:rec709]
		-> "dcmipp_main_isp_stat_capture":0 [ENABLED,IMMUTABLE]
  • On pad0, crop:(0,10)/2592x1928 indicates that the original frame should be cropped to a size of 2592x1928 starting at line 10. Since original frame size is 2592x1940, this leads to cut of first 10 lines and bottom 2 lines. Above example can be set using the following command:
media-ctl -d /dev/media1 --set-v4l2 "'dcmipp_main_isp':0[crop:(0,10)/2592x1928]"
  • On same pad0, compose:(0,0)/1296x964 indicates to resize the frame (after the crop) to a size of 1296x964. On the dcmipp_main_isp subdev, this is done by decimation of the frame. Above example can be set using the following command:
media-ctl -d /dev/media1 --set-v4l2 "'dcmipp_main_isp':0[compose:(0,0)/1296x964]"
  • pad0 format SRGGB10_1X10 is a RawBayer format, leading to automatic activation of the demosaicing block, which will thus generate a RGB888_1X24 on the output pad (pad1) of the subdev. Frame size is also automatically set to the size of the compose.

4. DCMIPP ISP block parameter video output device dcmipp_main_isp_params_output[edit source]

The dcmipp_main_isp_params_output video output device allows for configuration of other features of the DCMIPP ISP not already configurated via the v4l2_subdev pad api. That is:

  • bad pixel removal
  • black level correction
  • exposure control
  • demosaicing filters control
  • color conversion
  • contrast enhancement

Parameters are injected into the DCMIPP ISP via V4L2 buffer of type V4L2_META_FMT_ST_DCMIPP_ISP_PARAMS negociated with the dcmipp_main_isp_params_output video device.

#define V4L2_META_FMT_ST_DCMIPP_ISP_PARAMS      v4l2_fourcc('S', 'T', 'I', 'P') /* STM32 DCMIPP ISP Parameters */

Once the application have allocated buffers via the driver V4L2_REQBUFS ioctl, it needs to fill in those buffers with struct stm32_dcmipp_params_cfg structures. Requesting setting application is done by using the V4L2_QBUF ioctl, using a traditionnal V4L2 buffer handling mechanism.

4.1. parameter structure (struct stm32_dcmipp_params_cfg) description[edit source]

The main structure is made a bitfield module_cfg_update indicating which parameter is valid within the structure, allowing to apply one or more parameters at once. The other element of the structure is struct stm32_dcmipp_isp_ctrls_cfg which contains structures for each configurable feature.

/**
 * struct stm32_dcmipp_params_cfg - STM32 DCMIPP ISP Input Parameters Meta Data
 *
 * @module_cfg_update: mask the config bits of which module should be updated
 * @ctrls: configuration of other ISP blocks
 */
struct stm32_dcmipp_params_cfg {
       __u32 module_cfg_update;
       struct stm32_dcmipp_isp_ctrls_cfg ctrls;
};

/**
 * struct stm32_dcmipp_isp_ctrls_cfg - STM32 DCMIPP ISP Controls
 *
 * @bpr_cfg: configuration of the bad pixel removal block
 * @blc_cfg: configuration of the black level correction block
 * @ex_cfg: configuration of the exposure block
 * @dm_cfg: configuration of the demosaicing filters block
 * @cc_cfg: configuration of the color conversion block
 * @ce_cfg: configuration of the contrast enhancement block
 */
struct stm32_dcmipp_isp_ctrls_cfg {
       struct stm32_dcmipp_isp_bpr_cfg bpr_cfg;
       struct stm32_dcmipp_isp_blc_cfg blc_cfg;
       struct stm32_dcmipp_isp_ex_cfg ex_cfg;
       struct stm32_dcmipp_isp_dm_cfg dm_cfg;
       struct stm32_dcmipp_isp_cc_cfg cc_cfg;
       struct stm32_dcmipp_isp_ce_cfg ce_cfg;
};

Further details about each element of this structure can be found within the stm32-dcmipp-config.h [1] file.

4.2. example[edit source]

5. DCMIPP ISP statistics control & capture video device dcmipp_main_isp_stat_capture[edit source]

5.1. The available controls[edit source]

Further controls are available and applicable on the dcmipp_main_isp subdev:

  • demosaicing_peak / demosaicing_horizontal_line / demosaicing_vertical_line / demosaicing_edge: control of the strength of the demosaicing algorithms. Please refer to the refman in order to get more detail about the implemented demosaicing algorithms.
  • blacklevel_rgb: unique value to be applied for all R/G/B components for blacklevel compensation
  • bad_pixel_control: control of the strength of the bad pixels detection algorithm
  • bad_pixel_count: returns the amount of bad pixels detected within the last frame handled by the ISP block

Exposure / contrast and color conversion blocks requires more informations so controls below must provided using specific structures

  • isp_exposure_block_control: this control is used to apply settings into the exposure block via the struct v4l2_ctrl_isp_exposure below matching the parameters required by the HW block and described within the RefMan.
/**
 * struct v4l2_ctrl_isp_exposure - Exposure Block control within an ISP
 *
 * @enable: boolean indicating if the exposure compensation should be enabled or not
 * @shift_R: shift for RED component
 * @mult_R: multiply for RED component
 * @shift_G: shift for GREEN component
 * @mult_G: multiply for GREEN component
 * @shift_B: shift for BLUE component
 * @mult_B: multiply for BLUE component
 */
struct v4l2_ctrl_isp_exposure {
        bool enable;
        __u8 shift_R;
        __u8 mult_R;
        __u8 shift_G;
        __u8 mult_G;
        __u8 shift_B;
        __u8 mult_B;
};
  • isp_contrast_block_control: this control is used to apply settings into the contrast block via the struct v4l2_ctrl_isp_contrast below matching the parameters required by the HW block and described within the RefMan.
/**
 * struct v4l2_ctrl_isp_contrast - Contrast Block control within an ISP
 *
 * @enable: boolean indicating if the contrast compensation should be enabled or not
 * @lum: luminance increase value table (9 * 8 bits)
 */
struct v4l2_ctrl_isp_contrast {
        bool enable;
        __u8 lum[9];
};
  • isp_color_conversion_block_cont: this control is used to apply settings into the color conversion block via the struct v4l2_ctrl_isp_color_conv below matching the parameters required by the HW block and described within the RefMan. If used, it will override the color conversion settings done automatically by the subdev based on sink & source formats.
/**
 * struct v4l2_ctrl_isp_color_conv - Color Conversion parameters within an ISP
 *
 * @enable: boolean indicating if the color conversion should be enabled or not
 * @clamping: boolean indicating if the converted color shall be clamped or not
 * @clamping_as_rgb: boolean indicating if the clamping applies to RGB color space (YUV otherwise)
 * @coeff: color conversion coefficients of the matrix (RGB 3x3 + 1 offset column)
 */
struct v4l2_ctrl_isp_color_conv {
        bool enable;
        bool clamping;
        bool clamping_as_rgb;
        __u16 coeff[3][4];
};

5.2. The statistic extraction[edit source]

5.2.1. Statistics buffer format[edit source]

Statistics generated by the DCMIPP are available via the dcmipp_main_isp_stat_capture V4L2 device. The DCMIPP generated two types of statistics AVERAGE and BINS which are made available via the struct stm32_dcmipp_stat_buf described below.

struct stm32_dcmipp_stat_buf {
        __u32 average_RGB[3];
        __u32 bins[12];
} __packed;
  • average_RGB: contains the average value of each component in the statistic area of the frame
  • bins: 12 dynamic bins of based on luminance in order to perform later on contrast enhancement

Each buffer extract of the V4L2 device (of type V4L2_BUF_TYPE_META_CAPTURE) will contain one struct stm32_dcmipp_stat_buf, using a dedicated dataformat V4L2_META_FMT_ST_ISP_STAT.

5.2.2. Statistics controls[edit source]

The dcmipp_main_isp_stat_capture V4L2 device also exposes controls in order to tune the statistics extraction:

  • ISP stat region control (V4L2_CID_ISP_STAT_REGION): control the statistics extraction area. Allows to define the area of the frame from which statistics are processed. The following struct v4l2_ctrl_isp_stat_region is used to set the control. For the time being there must be only a unique region hence nb_regions should be set to 1.
/**
 * struct v4l2_ctrl_isp_stat_region - Region where ISP statistics are collected
 *
 * @nb_regions: number of regions
 * @top: top coordinate of a region
 * @left: left coordinate of a region
 * @width: width of a region
 * @height: height of a region
 */
struct v4l2_ctrl_isp_stat_region {
        __u8 nb_regions;
        __u32 top[25];
        __u32 left[25];
        __u32 width[25];
        __u32 height[25];
};
  • ISP stat location control (V4L2_CID_ISP_STAT_LOCATION): control the statistic extraction position within the DCMIPP pipeline.
    • 0: statistics are extracted prior to frame processing (aka beginning of the pipeline)
    • 1: statistics are extracted after demosaicing block
  • ISP stat average filter control (V4L2_CID_ISP_STAT_AVG_FILTER): control the filtering of pixels in the statistics AVERAGE processing
    • 0: no filtering performed, all pixels used for average calculation
    • 1: pixels with value < 16 or >= 240 are discarded from average calculation
    • 2: pixels with value < 32 or >= 224 are discarded from average calculation
    • 3: pixels with value < 64 or >= 192 are discarded from average calculation
  • ISP stat bin component control (V4L2_CID_ISP_STAT_BIN_COMP): control which component is used for BINS processing (R/G/B or Luminance)
    • 0: R component used
    • 1: G component used
    • 2: B component used
    • 3: luminance used

6. Use case examples[edit source]

Under construction.png Coming soon

7. Debug[edit source]

Under construction.png Coming soon