STM32 MPU ecosystem release note - v5.0.2.BETA

Revision as of 18:23, 12 December 2023 by Registered User (→‎STM32MP25 chip revA support)
Applicable for STM32MP25x lines

This article describes the content of STM32MP25-Ecosystem-v5.0.2.BETA release of STM32MPU Embedded Software distribution and its associated ecosystem.
This delivery is an update from previous STM32MP25 Ecosystem ALPHA release delivered in April 2023.

1. Delivery purpose[edit source]

The STM32MP25 Ecosystem-v5.0.2.BETA release is dedicated to the STM32MP25x lines More info.png[1]. It is a major release, based on new community components version, listed in the embedded software chapter below.

This STM32MP25 Ecosystem-v5.0.2.BETA release aims at:

  • providing a full ecosystem for the STM32MP25x lines More info.png[1]
  • working efficiently with STM32 MPU boards, using one of the packages (Starter Package, Developer Package or Distribution Package) provided by STMicroelectronics: refer to Which Package better suits your needs for more information.

The STM32MP25 Ecosystem V5.0.2.BETA Delivery main contents are :

  • STM32MP25 Rev B final with DDR4/LPDDR4 4GB, Full System performances, ETH GMAC controller with 4 Tx queues (instead 2) + RMON counters increased
  • OpenSTLinux V5.0.2 based
  • STM32MP257EV1 boards revC with STM32MP25 Rev B and STPMIC25 Rev A silicon revisions
  • STM32CubeMX code generation (Device trees for OpenSTLinux and TF-M, STM32Cube Software code for 'Arm® Cortex®-M33 non secure co-procrocessor. firmware)
  • 1st STM32MP25 Wiki documentation
  • Emb. SW by default supporting STM32MP25 Rev B but still compliant STM32MP25 Rev A with specific STM32MP257EV1 board device tree and specific compilation switches (This STM32MP25 Rev A compliance will be removed for STM32MP25 Ecosystem Mass Market Delivery) - refer to #STM32MP25 chip revA support

2. Delivery scope[edit source]

This ecosystem release consists of:

  • STM32MP257F-EV1 boards
  • STM32 MPU Embedded Software distribution
  • STM32DDRFW-UTIL
  • STM32PRGFW-UTIL
  • STM32 referenced tools (more details are provided in the Referenced tools release notes chapter below):
  • STM32CubeIDE
  • STM32CubeMX
  • STM32CubeProgrammer
  • Keygen tool
  • Signing tool
  • X-LINUX-AI expansion package
  • hosted at the non-browsable URL http://packages.openstlinux.st.com
  • enabled by default in the Starter Package
  • providing regularly updated or additional packages
  • Documentation
  • the present user guide in Wiki format
  • the documentation package (for more details refer to Reference documents chapter below)
  • STM32MP25 boards support
  • STM32MP25 Evaluation boards
More details are provided in the supported hardware chapter below.

3. Intended audience[edit source]

The targeted audience is STM32MP25 ALPHA customers and partners.

4. Licensing[edit source]

This software package is licensed under a SOFTWARE LICENSE AGREEMENT FOR ST MATERIALS (SLA). Customers should only use this package in compliance with the software license agreement (SLA).


5. Supported hardware[edit source]

This software delivery is compatible with the following boards:


STM32MP25 boards
Boards PCBs list Main features Ordering
STM32MP257F-EV1.jpg
STM32MP257F-EV1 Evaluation board
  • Finished good VA32MP257F1$MR1
  • MB1936 (main board)
  • STM32MP257FAI3[2] Rev.Y
    • Arm®-based dual Cortex®-A35 1500 MHz
    • Secure boot and cryptography
    • 2 x 16-Gbit DDR4, 32 bits, 1200 MHz
  • PMIC STPMIC25 Cut1.1
  • Optional expansion boards
    • LVDS WSVGA display B-LVDS7-WSVGA board (finished good BLVDS7SVGA$PZ1)
    • 5-megapixel image sensor raw Bayer B-CAMS-IMX board (finished good BCAMSIMX$MZ1)
    • DSI to HDMI adapter Full HD 30fps B-LCDAD-HDMI1 board

Evaluation board with STM32MP257F MPU

STM32MP257F-DK.png
STM32MP257F-DK Discovery kit
  • Finished good DK32MP257F$AR1
  • MB1605 (main board)
  • STM32MP257FAI3[2] Rev.Y
    • Arm®-based dual Cortex®-A35 1500 MHz
    • Secure boot and cryptography
    • 32-Gbit LPDDR4, 32 bits, 1200 MHz
  • PMIC STPMIC25 Cut1.1
  • Optional expansion boards
    • LVDS WSVGA display B-LVDS7-WSVGA board (finished good BLVDS7SVGA$PZ1)
    • 5-megapixel image sensor raw Bayer B-CAMS-IMX board (finished good BCAMSIMX$MZ1)
Under construction.png Coming soon
Info white.png Information
The STLINK, embedded on the boards, requires upgraded USB PC drivers: see ST-LINK article

6. Release content[edit source]

6.1. Embedded software[edit source]

Embedded software STM32MP25x lines More info.png
OpenSTLinux (Arm® Cortex®-A35) Yes
STM32CubeMP2 (Arm® Cortex®-M33) Yes
TF-M (Arm® Cortex®-M33) Yes
STM32DDRFW-UTIL (Arm® Cortex®-A35) Yes
STM32PRGFW-UTIL (Arm® Cortex®-A35) Yes

6.1.1. OpenSTLinux (Arm® Cortex®-A35)[edit source]

unknown revision is the new version delivered with the STM32MP1-ecosystem-v5.0.0 release. This software set consists of the following components: STM32 MPU OpenSTLinux release note - v5.0.2.BETA

6.1.1.1. Main changes[edit source]

Linux® kernel STM32 MPU OpenSTLinux release note - v5.0.2.BETA dt-stm32mp (New) STM32 MPU OpenSTLinux release note - v5.0.2.BETA U-Boot STM32 MPU OpenSTLinux release note - v5.0.2.BETA TF-A STM32 MPU OpenSTLinux release note - v5.0.2.BETA OP-TEE STM32 MPU OpenSTLinux release note - v5.0.2.BETA SCP firmware (New) STM32 MPU OpenSTLinux release note - v5.0.2.BETA OpenSTLinux layers STM32 MPU OpenSTLinux release note - v5.0.2.BETA

Warning DB.png Important
More information about the changes are available through the detailed release note
6.1.1.2. Restrictions[edit source]

STM32 MPU OpenSTLinux release note - v5.0.2.BETA

6.1.2. STM32CubeMP2 (Arm® Cortex®-M33)[edit source]

unknown revision version

6.1.2.1. Main changes[edit source]
  • BETA release of STM32CubeMP2 package HAL drivers.
  • All HAL drivers have been checked for MISRA 2012 compliance but warnings are not fixed completely.
  • BETA release of STM32CubeMP2 package LL drivers.
  • All LL drivers have been checked for MISRA 2012 compliance but warnings are not fixed completely.
  • AzureRTOS (ThreadX, LevelX, FileX, NetXDuo) middlewares
  • OpenAMP v2021.10.0 middleware
  • UCPD middleware
6.1.2.2. Main restrictions[edit source]
  • Clock muxing RCC HAL API in CxM33 No secure context not yet supported by STM32CubeMP2 for DSI, LVDS, RTC, MCO1/2, DTS, USB

6.1.3. TF-M (Arm® Cortex®-M33)[edit source]

unknown revision version

6.1.3.1. Main changes[edit source]
  • CxM33 firmware in secure context
  • TF-M device tree introduced in TF-M build process
  • TFM_Protected_Storage_CM33_trusted-firmware-m example project in STM32CubeMP2
  • Tests with TF-m-tests
6.1.3.2. Main information[edit source]
  • To install in local STM32CubeMP2/Middlewares/Third_party/trusted-firmware-m directory for usage – refer to STM32CubeIDE user guide (How to build and debug secure project on STM32MP25 co-processor in STM32CubeIDE user guide)
6.1.3.3. Main restrictions[edit source]

6.1.4. STM32DDRFW-UTIL (Arm® Cortex®-A35)[edit source]

STM32DDRFW-UTIL-v0.3.0 version.

STM32DDRFW-UTIL provides DDR settings configuration and tests services.

6.1.4.1. Main changes[edit source]
  • DDR settings and tests (DDR4 4GB 1200 MHz, LPDDR4 4GB 1200 MHz, DDR3 1GB 930 MHz)
  • Support of STM32MP257F-EV1 (MB1936) board / DDR4 settings
  • Improve board customization capability for LPDDR4 and DDR3
  • Utility fwm to be compiled and debugged in Cortex®-A35 Aarch64 bits using STM32CubeIDE to access to 4GB addressing range
  • To use with STM32CubeMX or in standalone
6.1.4.2. Main restrictions[edit source]
  • None

6.1.5. STM32PRGFW-UTIL (Arm® Cortex®-A35)[edit source]

STM32PRGFW-UTIL-v1.1.0.rc4 version.

STM32PRGFW-UTIL provides multiple applications to manage the one-time programmable (OTP) memories.

6.1.5.1. Main changes[edit source]
  • Fuses settings
  • PMIC command to read/write STPMIC25 NVM content
  • Utility fwm to be compiled and debugged in Cortex®-A35 Aarch32 bits with STM32CubeIDE
  • To use with STM32CubeProgrammer or in standalone
6.1.5.2. Main restrictions[edit source]
  • None

6.2. Tools[edit source]

6.2.1. STM32CubeProgrammer, Signing tool, Keygen[edit source]

STM32CubeProgrammer v0.0.0.MP25-BETA02 version - Updated .

6.2.1.1. Main changes[edit source]
  • Flash programming with STM32MP25 on supported flashes by OpenSTLinux with STM32CubeProgrammer tool
  • Hash of (RoT Public Keys + Algo) hashes (256 bits, ROTPK) generation with KeyGen tool
  • TF-A BL2 binary signature with stm32header V2.2 with Signing tool for STM32MP25 Rev B
  • FSBL encryption with Signing tool
  • Signing services with PKCS#11
  • OTP programming via CLI/GUI
6.2.1.2. Supported operating systems and architectures[edit source]

• Windows® 7, 8, 10, and 11: 32 bits (x86) and 64 bits (x64) • Linux® 64 bits (tested on Ubuntu® 64 bits) • macOS® (minimum version OS X® Yosemite)

6.2.1.3. Information[edit source]
  • v0.0.0.MP25-BETA02 based on v2.14 version + STM32MP25 revB support
  • Flashload over UART OK for Utilities fmws but not available with OpenSTLinux bootloaders
  • FSBL (TF-A) header handled by BOOTROM has been upgraded for STM32MP25 Rev B (Header V2.2 version) versus STM32MP25 Rev A (Header V2.0 version). If the FSBL is signed with and header v2.0 version, the target will not boot with a STM32MP25 Rev B.
    • In case of non secure boot, the header is generated by Yocto build process
    • In case of secure boot, the header is generated by Signing tool in CubeProgrammer delivery
  • Note Still possible to ensure TF-A BL2 binary signature with stm32header V2.0 with Signing tool for STM32MP25 Rev A with CubeProg ALPHA version (V2.13)
6.2.1.4. Restrictions[edit source]
  • None

6.2.2. STM32CubeMX[edit source]

STM32CubeMX-6.99.27-B3 version - Updated .

6.2.2.1. Main changes[edit source]
  • Pinout/list Peripherals - some IOC file examples in Teamspace with:
    • MP25_EV1 - RIF Open - BETA DV IOC file
    • MP25_EV1 - RIF Ecosystem - BETA DV IOC file
    • MP25_EV1 - RIF Ecosystem - M33 examples - BETA DV IOC file
  • Clocks tree UI
  • DDR Settings
    • DDR4 using STM32-DDR-FWUTIL embedded SW binary with EVAL board
    • LPDDR4 and DDR3 tests using STM32-DDR-FWUTIL embedded SW binary
  • Code generation
    • Device trees with GPIO, IP Assignment, Clocks, RIF parts for TF-A, OP-TEE, U-BOOT, KERNEL SW components on Cortex A35 and SW TF-M components on Cortex M33
    • STM32CubeMP2 on Cortex M33 non secure context
6.2.2.2. Supported operating systems and architectures[edit source]
  • Windows® 10 and 11, 64 bits (x64)(b)
  • Linux®: Ubuntu® LTS 20.04 and LTS 22.04, and Fedora® 36(c) (d) (e)
  • macOS® 12 (Monterey), macOS® 13 (Ventura)(f)
6.2.2.3. Supported toolchains[edit source]

STM32CubeMX generates project files for the following toolchains:

  • STM32CubeIDE by STMicroelectronics
6.2.2.4. Main restrictions[edit source]
  • RIF Aware IPs not all available in terms of UI - Available PWR, FMC, GPIO, RCC - Not yet available DMA, TAMP, RTC, IPCC, HSEM
  • RIF Aware IPs not all available in terms of device tree - Available PWR, FMC - Not yet available GPIO, RCC, DMA, TAMP, RTC, IPCC, HSEM
  • RIFSC configuration for DSIHOST IP w DSI_RD, DSI_TRIG, DSI COMMON parts not available in UI
  • RIFSC configuration for ETHACM IP w ETHSW_ACM,  ETHSW_ACM_MSG, ETHSW_DEIP parts not available in UI
  • RIFSC configuration for LTDC IP w LTDC_L3, LTDC_L1L2, LTDC_ROT, LTDC_Common parts not available in UI
  • LVDS IP should be managed as a single IP with LVDS1 and LVDS2 pins and single or dual datalanes modes - In current version, managed as 2 LVDS instances LVDS1 and LVDS2 and RIFSC configuration with LVDS not functional

6.2.3. STM32CubeIDE[edit source]

STM32CubeIDE-v1.13.0.23_MP2-D4 version - Updated .

6.2.3.1. Main changes[edit source]
  • STM32CubeMP2, TF-M firmwares on Cortex-M33 production mode
  • STM32-PRG-FWUTIL firmware support on Cortex-A35 dev mode Aarch32 bits
  • STM32-DDR-FWUTIL firmware support on Cortex-A35 dev mode Aarch64 bits to address DDR 4GB
  • OpenSTLinux developer package plug-in to install thru STM32CubeIDE
  • Console semi-hosting support (logs thu SWD)
  • cmake management update – Information in user guide How to build and debug secure project on STM32MP25 co-processor in STM32CubeIDE user guide - Available in TeamSpace [1]
  • STM32CubeMX stand-alone project
6.2.3.2. Main restrictions[edit source]
  • None

6.3. STM32MP25 chip revA support[edit source]

6.4. Miscellaneous[edit source]

Detailed features are available in the release notes of the different components that constitute this delivery:

Moreover, the software workarounds implemented to provide solutions to the STM32MPU device errata are listed in STM32MP15 ecosystem errata sheet and STM32MP13 ecosystem errata sheet.

7. Minor release updates[edit source]

Some minor release of STM32MP1 OpenSTLinux distribution is available. More details can be found in STM32_MPU_OpenSTLinux_release_note_-_v5.0.0#Minor_release_updates.

8. Reference documents[edit source]

8.1. STM32MP25 resources[edit source]


All the resources for the STM32MP2 series are located in the STM32MP2 series web page.

Info white.png Information
The different STM32MP25 microprocessor part numbers available (with their corresponding internal peripherals, security options and packages) are described in the STM32MP25 microprocessor part numbers.


Reference Name Link
Application notes
AN5489 AN5489 - Getting started with STM32MP25xx lines hardware development AN5489.pdf
AN5723 AN5723 - Guidelines for DDR memory configuration on STM32MP2 MPUs AN5723.pdf
AN5724 AN5724 - Guidelines for DDR memory routing on STM32MP2 MPUs AN5724.pdf
AN5718 AN5718 - Migrating from STM32MP15x lines to STM32MP25x lines MPUs AN5718.pdf
AN5726 AN5726 - Guidelines for using low-power modes on STM32MP2 MPUs AN5726.pdf
AN5827 AN5827 - Guidelines for entering RMA state on MPU series Under preparation
AN5727 AN5727 - How to use STPMIC25 for a wall adapter powered application on STM32MP25x lines MPUs Under preparation
AN5730 AN5730 - Guidelines for measuring system power consumption on STM32MP2 MPUs Under preparation
AN6115 AN6115 - How to connect STPMIC25 unused pins AN6115.pdf
AN6116 AN6116 - STPMIC25 BOM details AN6116.pdf
AN6128 AN6128 - STPMIC25 PCB layout guidelines AN6128.pdf
Datasheets[3]
DS14284 STM32MP25xC/F Datasheet DS14284.pdf
DS14285 STM32MP25xA/D Datasheet DS14285.pdf
DS14278 STPMIC25 datasheet
DS14278.pdf
Errata sheets
ES0598 STM32MP25x ErrataSheet ES0598.pdf
Reference manuals[3]
RM0457 STM32MP25 reference manual
(STM32MP25xx advanced Arm®-based 32/64-bit MPUs)
RM0457.pdf
Programming manuals
PM0264 STM32 Cortex®-M33 MCUs and MPUs programming manual PM0264.pdf
Boards schematics
STM32MP257F-EV1 board (MB1936) schematics STM32MP257F-EV1 board revD schematics with STM32MP25F RevB 18x18 package MB1936-D01.pdf
B-CAMS-IMX schematics Camera module bundle schematics MB1854-B01.pdf
B-LVDS7-WSVGA schematics LVDS TFT LCD module schematics b-lvds7-wsvga.html
STM32MP25F-DK schematics STM32MP257F-DK board schematics example with STM32MP25F RevY 14x14 package Under preparation
DDR routing examples schematics Additional DDR memory routing examples DDR routing examples
User manuals
UM3359 STM32MP2357F-EV1 User Manual UM3359.pdf
UM3354 B-CAMS-IMX Camera module bundle User Manual UM3354.pdf

9. How to download the software and start with this release?[edit source]

The list of embedded software packages available for download depends on the selected packages.

The table below provides the available board part numbers as well as information in order to:

  • get started with one of the three available Packages (Starter, Developer or Distribution Package)
  • get started with the board
  • find the associated embedded software distributions
  • download source code
  • build a piece of embedded software.
Supported board Jump to
STM32MP257x-EV1 Evaluation board More info green.png STM32MP25 Evaluation boards - getting started, including software download

10. STM32MPU Embedded Software distribution detailed release notes[edit source]

The table below lists the software packages available in the STM32MPU Embedded Software distributions, and provides the corresponding release notes.
The release notes give more information and details about the features and content of the packages.
They do not explain how to download the software. Refer to How to download the software and start with this release.

Firmware Release note Version
OpenSTLinux Distribution STM32 MPU OpenSTLinux release note - v5.0.2.BETA unknown revision
STM32Cube MPU Package STM32CubeMP2 Package release note - v0.3.0 unknown revision
TF-M Trusted Firmware-M release note - v0.3.0 unknown revision

11. Referenced tools release notes[edit source]

The table below lists the available tools, and provides links to the corresponding release notes.

Each release note gives information on how to install and use the corresponding tool.

The set of tools that can be downloaded depends on the package that is used (double check Which Package better suits your needs article for more information on each package).

Tools Release notes Host PC Which Package may need the tool ?
Linux® version Windows version Starter Package Developer Package Distribution Package
STM32CubeIDE STM32CubeIDE_release_note 1.13.0.23_MP2-D4 1.13.0.23_MP2-D4
STM32CubeMX STM32CubeMX release note 6.99.27-B3 6.99.27-B3
STM32CubeProg STM32CubeProgrammer release note 0.0.0-MP25-B02 0.0.0-MP25-B02
Keygen KeyGen release note v0.0.0-MP25-B02 v0.0.0-MP25-B02
Signing tool Signing tool release note v0.0.0-MP25-B02 v0.0.0-MP25-B02
STM32DDRFW-UTIL STM32DDRFW-UTIL release note 0.3.0 0.3.0
STM32PRGFW-UTIL STM32PRGFW-UTIL release note 1.1.0.rc4 1.1.0.rc4

12. References[edit source]

  1. 1.0 1.1 The STM32MP25x lines More info.png includes the STM32MP25x lines More info.png and the STM32MP25x lines More info.png
  2. 2.0 2.1 STM32MP25 microprocessor part numbers
  3. 3.0 3.1 The part numbers are specified in STM32MP25 microprocessor part numbers