This article introduces the structure and the content of the STM32CubeMP25 Package, the embedded software part of STM32Cube™, running on the Arm® Cortex®-M33 coprocessor. It references also other interesting wiki articles to better understand and use the STM32CubeMP25 Package.
1. What is the STM32CubeMP25 Package[edit source]
STM32CubeMP25 Package, running on the Arm® Cortex®-M33 processor, consists of:
- The hardware abstraction layer (HAL), enabling portability between different STM32 devices via standardized API calls
- The low-layer API (LL), a light-weight, optimized, expert oriented set of APIs designed for runtime efficiency and so enhanced performance
- The board support package drivers (BSP), based on HAL drivers, an API set for the evaluation board and third-party components.
- A collection of middleware components (such as AzureRTOS)
- A collection of examples, running on an MPU board and allowing demonstration of a basic implementation of features from a set of IPs
2. Software architecture overview[edit source]
Software architecture overview is described in STM32CubeMP2 Package architecture.
3. STM32CubeMP25 Package structure[edit source]
This chapter describes the structure of the STM32CubeMP25 Package (drivers, middleware components...).
STM32CubeMP25 Package offers a highly portable Hardware Abstraction Layer (HAL), built around a generic and modular architecture.
This HAL allows the upper layers, middleware and application, to implement functions whenever STM32MP25 device is used. This improves the library code re-usability and guarantees easy portability from one device to another. STM32CubeMP25 Package also offers a highly portable Low Layer interface (LL), which allows a quick, simple and optimized API to access the STM32MP25 registers.
The STM32CubeMP25 Package is provided with the structure shown below.
4. STM32CubeMP2 Package content[edit source]
This chapter describes the content of the STM32CubeMP2 Package (drivers, middleware components...).
4.1. Drivers[edit source]
The Drivers folder contains all the STM32Cube Drivers, including BSP and HAL drivers.
4.1.1. HAL drivers[edit source]
STM32CubeMP2 HAL Driver items | Description |
---|---|
ADC |
* This driver provides firmware functions to manage the following * functionalities of the Analog to Digital Convertor (ADC) * peripheral: * + Initialization and de-initialization functions * ++ Initialization and Configuration of ADC * + Operation functions * ++ Start, stop, get result of conversions of regular * group, using 3 possible modes: polling, interruption or DMA. * + Control functions * ++ Channels configuration on regular group * ++ Analog Watchdog configuration * + State functions * ++ ADC state machine management * ++ Interrupts and flags management |
ADC_EX |
* This driver provides firmware functions to manage the following * extended functionalities of the Analog to Digital Convertor (ADC) * peripheral: * + Operation functions * ++ Start, stop, get result of conversions of ADC group injected, * using 2 possible modes: polling, interruption. * ++ Calibration * +++ ADC automatic self-calibration * +++ Calibration factors get or set * ++ Multimode feature when available * + Control functions * ++ Channels configuration on ADC group injected * + State functions * ++ ADC group injected contexts queue management |
BSEC |
* This driver provides firmware functions to manage the following * functionalities of the Boot and security and OTP control(BSEC) peripheral: * + Initialization and de-initialization functions * + Peripheral Control functions * + Peripheral State functions |
CRC |
* This driver provides firmware functions to manage the following
* functionalities of the Cyclic Redundancy Check (CRC) peripheral:
* + Initialization and de-initialization functions
* + Peripheral Control functions
* + Peripheral State functions
* + Extended features functions
|
CRYP |
* This driver provides firmware functions to manage the following * functionalities of the Cryptography (CRYP) peripheral: * + Initialization and de-initialization functions * + AES processing functions * + DES processing functions * + TDES processing functions * + DMA callback functions * + CRYP IRQ handler management * + Peripheral State functions |
CRYP_EX |
* This driver provides firmware functions to manage the following * functionalities of CRYP extension peripheral: * + Extended AES processing functions |
CSI |
* This file provides firmware functions to manage the following * functionalities of the Digital Camera Interface (CSI) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Error functions |
DCACHE |
* This file provides firmware functions to manage the following * functionalities of the DCACHE. * + Initialization and Configuration * + Cache coherency command * + Monitoring management |
DCMI |
* This file provides firmware functions to manage the following * functionalities of the Digital Camera Interface (DCMI) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Error functions |
DCMIPP |
* This driver provides firmware functions to manage the following * functionalities of the DCMIPP (Digital Camera Interface Pixel Pipeline) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Error functions |
DDR |
* This driver provides firmware functions to manage the following
* functionalities of the Double Data Rate Synchronous Dynamic Random
* Access Memory (DDR-SDRAM) Peripheral, through its controller
* (DDRCTRL) and its physical interface controller (DDRPHYC).
|
DMA |
* This driver provides firmware functions to manage the following * functionalities of the Direct Memory Access (DMA) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral State and errors functions |
DMA_EX |
* This driver provides firmware functions to manage the following
* functionalities of the DMA Extension peripheral:
* + Extended features functions
|
DSI |
* This file provides firmware functions to manage the following * functionalities of the DSI peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Errors functions |
ETH |
* This driver provides firmware functions to manage the following * functionalities of the Ethernet (ETH) peripheral: * + Initialization and deinitialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Errors functions |
EXTI |
* This driver provides firmware functions to manage the following * functionalities of the General Purpose Input/Output (EXTI) peripheral: * + Initialization and de-initialization functions * + IO operation functions |
FDCAN |
* This driver provides firmware functions to manage the following
* functionalities of the Flexible DataRate Controller Area Network
* (FDCAN) peripheral:
* + Initialization and de-initialization functions
* + IO operation functions
* + Peripheral Configuration and Control functions
* + Peripheral State and Error functions
|
GPIO |
* This driver provides firmware functions to manage the following * functionalities of the General Purpose Input/Output (GPIO) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Extended Peripheral Control functions |
HAL |
* This driver provides firmware functions to manage the following * functionalities of HAL, Tick, SYSCFG, DBGMCU: * + Initialization and de-initialization functions * + HAL Initialization and de-initialization functions * + Configure the source of the time base * + HAL Control functions * + Tick management (get/set/inc/priority/suspend/resume) * + Get HAL revision, the device revision identifier, the device identifier * + Enable/Disable DBG wake up on AIEC * + Enable/Disable the Debug Module during Domain1 SLEEP mode * + Enable/Disable the Debug Module during Domain1 STOP mode * + Enable/Disable the Debug Module during Domain1 STANDBY mode * + Configure the internal voltage reference buffer voltage scale * + Configure the internal voltage reference buffer high impedance mode * + Tune the Internal Voltage Reference buffer (VREFBUF) * + Enable/Disable the Internal Voltage Reference buffer (VREFBUF) * + Ethernet PHY Interface Selection either MII or RMII * + Analog Switch control for dual analog pads * + Enable/Disable the booster to reduce the total harmonic distortion of the analog * + Enable/Power-down the I/O Compensation Cell * + To Enable/Disable optimize the I/O speed when the product voltage is low * + Code selection for the I/O Compensation cell |
HASH |
* This driver provides firmware functions to manage the following * functionalities of the HASH peripheral: * + Initialization and de-initialization methods * + HASH or HMAC processing in polling mode * + HASH or HMAC processing in interrupt mode * + HASH or HMAC processing in DMA mode * + Peripheral State methods * + HASH or HMAC processing suspension/resumption |
HASH_EX |
* This driver provides firmware functions to manage the following * functionalities of the HASH peripheral for SHA-224 and SHA-256 * algorithms: * + HASH or HMAC processing in polling mode * + HASH or HMAC processing in interrupt mode * + HASH or HMAC processing in DMA mode * Additionally, this file provides functions to manage HMAC * multi-buffer DMA-based processing for MD-5, SHA-1, SHA-224 * and SHA-256. |
HSEM |
* This file provides firmware functions to manage the following * functionalities of the semaphore peripheral: * + Semaphore Take function (2-Step Procedure) , non blocking * + Semaphore FastTake function (1-Step Procedure) , non blocking * + Semaphore Status check * + Semaphore Clear Key Set and Get * + Release and release all functions * + Semaphore notification enabling and disabling and callback functions * + IRQ handler management |
ICACHE |
* This file provides firmware functions to manage the following * functionalities of the Instruction Cache (ICACHE). * + Initialization and Configuration * + Invalidate functions * + Monitoring management * + Memory address remap management |
IPCC |
* This file provides firmware functions to manage the following
* functionalities of the Inter-Processor communication controller
* peripherals (IPCC).
* + Initialization and de-initialization functions
* + Configuration, notification and interrupts handling
* + Peripheral State and Error functions
|
I2C |
* This driver provides firmware functions to manage the following * functionalities of the Inter Integrated Circuit (I2C) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral State and Errors functions |
I2C_EX |
* This driver provides firmware functions to manage the following
* functionalities of I2C Extended peripheral:
* + Filter Mode Functions
* + WakeUp Mode Functions
* + FastModePlus Functions
|
I2S |
* This file provides firmware functions to manage the following * functionalities of the Integrated Interchip Sound (I2S) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral State and Errors functions |
I3C |
* This file provides firmware functions to manage the following
* functionalities of the Improvement Inter Integrated Circuit (I3C) peripheral:
* + Initialization and de-initialization functions
* + IO operation functions
* + Peripheral State and Errors functions
|
IWDG |
* This file provides firmware functions to manage the following * functionalities of the Independent Watchdog (IWDG) peripheral: * + Initialization and Start functions * + IO operation functions |
LPTIM |
* This driver provides firmware functions to manage the following
* functionalities of the Low Power Timer (LPTIM) peripheral:
* + Initialization and de-initialization functions.
* + Start/Stop operation functions in polling mode.
* + Start/Stop operation functions in interrupt mode.
* + Reading operation functions.
* + Peripheral State functions.
|
LTDC |
* This file provides firmware functions to manage the following * functionalities of the LTDC peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Errors functions |
MMC |
* This driver provides firmware functions to manage the following * functionalities of the Secure Digital (MMC) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + MMC card Control functions |
MMC_EX |
* This driver provides firmware functions to manage the following
* functionalities of the Secure Digital (MMC) peripheral:
* + Extended features functions
|
PKA |
* This driver provides firmware functions to manage the following * functionalities of public key accelerator(PKA): * + Initialization and de-initialization functions * + Start an operation * + Retrieve the operation result |
PSSI |
* This file provides firmware functions to manage the following
* functionalities of the Parallel Synchronous Slave Interface (PSSI) peripheral:
* + Initialization and de-initialization functions
* + IO operation functions
* + Peripheral State and Errors functions
|
PWR |
* This driver provides firmware functions to manage the following * functionalities of the Power Controller (PWR) peripheral: * + Initialization and de-initialization functions * + Peripheral Control functions * + Peripheral Extended features functions |
PWR_EX |
* This driver provides firmware functions to manage the following * functionalities of PWR extension peripheral: * + Peripheral Extended features functions |
OSPI |
* This driver provides firmware functions to manage the following * functionalities of the OSPI interface (OSPI). * + Initialization and de-initialization functions * + Indirect functional mode management * + Memory-mapped functional mode management * + Auto-polling functional mode management * + Interrupts and flags management * + HPDMA channel configuration for indirect functional mode * + Errors management and abort functionality |
RAMCFG |
* This file provides firmware functions to manage the following * functionalities of the RAMs configuration controller peripheral: * + RAMCFG Initialization and De-initialization Functions. * + RAMCFG ECC Operation Functions. * + RAMCFG CRC Operation Functions. * + RAMCFG Configure Wait State Functions. * + RAMCFG Write Protection Functions. * + RAMCFG Erase Operation Functions. * + RAMCFG Handle Interrupt and Callbacks Functions. * + RAMCFG State and Error Functions. |
RCC |
* This driver provides firmware functions to manage the following
* functionalities of the Reset and Clock Control (RCC) peripheral:
* + Initialization and de-initialization functions
* + Peripheral Control functions
* + Extended Peripheral Control functions
|
RCC_EX |
* This driver provides firmware functions to manage the following
* functionalities RCC extension peripheral:
* + Extended Peripheral Control functions
|
RIF |
* This file provides firmware functions to manage the following * functionalities of RIF: * + RISC Initialization and Configuration functions * + IAC Initialization and Configuration functions |
RNG |
* This driver provides firmware functions to manage the following
* functionalities of the Random Number Generator (RNG) peripheral:
* + Initialization and configuration functions
* + Peripheral Control functions
* + Peripheral State functions
|
RNG_EX |
* This driver provides firmware functions to manage the following * functionalities of the Random Number Generator (RNG) peripheral: * + Lock configuration functions * + Reset the RNG |
RTC |
* This driver provides firmware functions to manage the following * functionalities of the Real-Time Clock (RTC) peripheral: * + Initialization/de-initialization functions * + Calendar (Time and Date) configuration * + Alarms (Alarm A and Alarm B) configuration * + WakeUp Timer configuration * + TimeStamp configuration * + Tampers configuration * + Backup Data Registers configuration * + RTC Tamper and TimeStamp Pins Selection * + Interrupts and flags management |
RTC_EX |
* This driver provides firmware functions to manage the following * functionalities of the Real Time Clock (RTC) Extended peripheral: * + RTC Time Stamp functions * + RTC Tamper functions * + RTC Wake-up functions * + Extended Control functions * + Extended RTC features functions |
SAI |
* This driver provides firmware functions to manage the following
* functionalities of the Serial Audio Interface (SAI) peripheral:
* + Initialization/de-initialization functions
* + I/O operation functions
* + Peripheral Control functions
* + Peripheral State functions
|
SAI_EX |
* This driver provides firmware functions to manage the following
* functionality of the SAI Peripheral Controller:
* + Modify PDM microphone delays.
|
SD |
* This driver provides firmware functions to manage the following * functionalities of the Secure Digital (SD) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State functions |
SD_EX |
* This driver provides firmware functions to manage the following
* functionalities of the Secure Digital (SD) peripheral:
* + Extended features functions
|
SMARTCARD |
* This driver provides firmware functions to manage the following
* functionalities of the Smartcard peripheral:
* + Initialization and de-initialization functions
* + IO operation functions
* + Peripheral Control functions
* + Peripheral State and Error functions
* + Extended features functions
|
SMARTCARD_EX |
* This driver provides extended firmware functions to manage the following * functionalities of the SmartCard. * + Initialization and de-initialization functions * + Peripheral Control functions |
SMBUS |
* This driver provides firmware functions to manage the following * functionalities of the System Management Bus (SMBus) peripheral, * based on I2C principles of operation : * + Initialization and de-initialization functions * + IO operation functions * + Peripheral State and Errors functions |
SPDIFRX |
* This driver provides firmware functions to manage the following
* functionalities of the SPDIFRX audio interface:
* + Initialization and Configuration
* + Data transfers functions
* + DMA transfers management
* + Interrupts and flags management
|
SPI |
* This driver provides firmware functions to manage the following * functionalities of the Serial Peripheral Interface (SPI) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State functions |
SPI_EX |
* This driver provides firmware functions to manage the following * SPI peripheral extended functionalities : * + IO operation functions * + Peripheral Control functions |
FMC_SRAM |
* This driver provides a generic firmware to drive SRAM memories * mounted as external device. |
FMC_NAND |
* This driver provides a generic firmware to drive NAND memories * mounted as external device. |
TIMER |
* This driver provides firmware functions to manage the following * functionalities of the Timer (TIM) peripheral: * + TIM Time Base Initialization * + TIM Time Base Start * + TIM Time Base Start Interruption * + TIM Time Base Start DMA * + TIM Output Compare/PWM Initialization * + TIM Output Compare/PWM Channel Configuration * + TIM Output Compare/PWM Start * + TIM Output Compare/PWM Start Interruption * + TIM Output Compare/PWM Start DMA * + TIM Input Capture Initialization * + TIM Input Capture Channel Configuration * + TIM Input Capture Start * + TIM Input Capture Start Interruption * + TIM Input Capture Start DMA * + TIM One Pulse Initialization * + TIM One Pulse Channel Configuration * + TIM One Pulse Start * + TIM Encoder Interface Initialization * + TIM Encoder Interface Start * + TIM Encoder Interface Start Interruption * + TIM Encoder Interface Start DMA * + Commutation Event configuration with Interruption and DMA * + TIM OCRef clear configuration * + TIM External Clock configuration |
TIMER_EX |
* This driver provides firmware functions to manage the following
* functionalities of the Timer Extended peripheral:
* + Time Hall Sensor Interface Initialization
* + Time Hall Sensor Interface Start
* + Time Complementary signal break and dead time configuration
* + Time Master and Slave synchronization configuration
* + Time Output Compare/PWM Channel Configuration (for channels 5 and 6)
* + Timer remapping capabilities configuration
|
UART |
* This driver provides firmware functions to manage the following * functionalities of the Universal Asynchronous Receiver Transmitter Peripheral (UART). * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions |
UART_EX |
* This driver provides firmware functions to manage the following extended
* functionalities of the Universal Synchronous Receiver Transmitter Peripheral (USART).
* + Peripheral Control functions
|
U(S)ART |
* This driver provides firmware functions to manage the following * functionalities of the Universal (Synchronous) Asynchronous Receiver Transmitter * Peripheral (U(S)ART). * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Error functions * + Peripheral Control functions |
4.1.2. LL drivers[edit source]
STM32CubeMP2 LL Driver items | Description |
---|---|
ADC |
* This driver provides firmware functions to manage the following * functionalities of the ADC peripheral: * + Initialization/de-initialization functions * + Configuration functions (ADC instance, group regular, group injected, * channels, analog watchdog, oversampling, multimode) * + IT/FLAGS management functions |
DELAYBLOCK |
* This file provides firmware functions to manage the following * functionalities of the DelayBlock peripheral: * + input clock frequency * + up to 12 oversampling phases |
DMA |
* This driver provides firmware functions to manage the following
* functionalities of the DMA peripheral:
* + Initialization/de-initialization functions
* + Configuration functions
* + IT/FLAGS management functions
|
EXTI |
* This driver provides firmware functions to manage the following
* functionalities of the EXTI peripheral:
* + Initialization/de-initialization functions
* + IT/FLAGS/Trigger management functions
* + Configuration functions
|
FMC |
* This driver provides firmware functions to manage the following * functionalities of the Flexible Memory Controller (FMC) peripheral memories: * + Initialization/de-initialization functions * + Peripheral Control functions * + Peripheral State functions |
GPIO |
* This driver provides firmware functions to manage the following
* functionalities of the GPIO peripheral:
* + Initialization/de-initialization functions
* + Data access functions
* + Port configuration functions
|
I2C |
* This driver provides firmware functions to manage the following * functionalities of the I2C peripheral: * + Initialization/de-initialization functions * + IT/FLAGS management functions * +Data management functions * + Configuration functions |
LPTIM |
* This driver provides firmware functions to manage the following * functionalities of the LPTIM peripheral: * + Initialization/de-initialization functions * + IT/FLAGS management functions * + Configuration (Trigger / Clock / Encoder / LPTIM) functions |
DMA |
* This driver provides firmware functions to manage the following * functionalities of the Direct Memory Access (DMA) peripheral: * + Channel Mangenment functions (Instance, Block, Buffer, Endianess etc) * + SRC/DES operation functions * + HW Trigger control |
PWR |
* This driver provides firmware functions to manage the following * functionalities of the PWR peripheral: * + De-initialization functions |
RCC |
* This driver provides firmware functions to manage the following * functionalities of the RCC peripheral: * + Clocks management functions (HSE/HSI/CSI/LSE/LSI/MCO/PLL) * + RTC/TIMERS functions * + IT/FLAGS management functions * + De-initialization functions * + Get system and peripherals clocks frequency functions |
RTC |
* This driver provides firmware functions to manage the following
* functionalities of the RTC peripheral:
* + Initialization/de-initialization functions
* + TIME/DATE/ALM functions
* + Configuration functions
|
SDMMC |
* This driver provides firmware functions to manage the following
* functionalities of the SDMMC peripheral:
* + Initialization/de-initialization functions
* + IT/FLAGS management functions
* + Data / DMA management functions
* + Configuration functions
|
SPI |
* This driver provides firmware functions to manage the following
* functionalities of the SPI peripheral:
* + Control and configuration functions
|
TIM |
* This driver provides firmware functions to manage the following * functionalities of the TIM peripheral: * + Initialization/de-initialization functions * + Configuration functions (Time base, Capture Compare, Output and Input Channel, * Timer Synchro, Break, DMA Burst Mode ) * + Counter clock selection functions * + Timer input remapping functions * + IT/FLAGS management functions * + DMA management functions * + Event management functions |
USART |
* This driver provides firmware functions to manage the following * functionalities of the USART peripheral: * + Initialization/de-initialization functions * + Configuration functions (Irda, Smartcard, Half duplex, * SPI Slave, LIN, Driver enable) * + Advanced configurations services functions * + IT/FLAGS management functions * + DMA management functions * + Data management functions * + Execution functions |
4.1.3. BSP drivers[edit source]
The BSP (Board Specific Package) drivers are parts of the STM32CubeMPU package based on the HAL drivers and provide a set of high level APIs relative to the hardware components and features in the STM32MP257x-EV1 Evaluation board .
It provides API for LED, button and COM ports.
STM32CubeMP2 BSP Driver items |
---|
STM32MP257F-EV1 |
stm32mp257f_eval_bus.c |
BSP Components are external components which can be attached to STM32MP257x-EV1 Evaluation board .
STM32CubeMP2 BSP Component Items | Description |
---|---|
Common |
This directory contains the BSP common components drivers. |
STPMIC2 |
This driver provides a set of functions needed to drive STPMIC2 PMU module. |
TCPP0203 |
This driver provides a set of functions needed to drive TCPP02/03 Type-C port protection. |
4.2. Projects[edit source]
The "Projects" folder contains all STM32Cube examples that are classified in 3 ways as described below :
- Examples: It uses only the HAL drivers without any middleware component. They are available in directory Projects/<board_name>/Examples.
- Applications: It provides typical use cases of each middleware component. They are available in directory Projects/<board_name>/Applications.
- Demonstrations: This program demonstrates the USBPD stack. Directory Projects/<board_name>/Demonstrations.
List of Projects is available here. Projects/STM32CubeProjectsList.html
4.2.1. Examples, applications and demonstrations for STM32MP257F-EV1 Evaluation board
[edit source]
4.2.1.1. List of all applications[edit source]
├── Application │ ├── FileX │ │ ├── Fx_NoR_Write_Read_File │ │ └── Fx_SRAM_File_Standalone │ ├── NetXDuo │ │ ├── Nx_Iperf │ │ ├── Nx_MQTT_Client │ │ ├── Nx_TCP_Echo_Client │ │ ├── Nx_TCP_Echo_Server │ │ ├── Nx_UDP_Echo_Client │ │ └── Nx_UDP_Echo_Server │ ├── OpenAMP │ │ └── OpenAMP_TTY_echo │ ├── TFM │ │ └── TFM_Protected_Storage │ ├── ThreadX │ │ ├── Tx_Thread_Creation │ │ ├── Tx_Thread_MsgQueue │ │ └── Tx_Thread_Sync │ └── USBPD │ └── USBPD_DRP_UCSI ├── Demonstrations │ └── USBPD_DRP_UCSI │ └── util └── Examples ├── CORTEX │ └── CORTEXM_ModePrivilege ├── CRC │ ├── CRC_Bytes_Stream_7bit_CRC │ └── CRC_UserDefinedPolynomial ├── CRYP │ ├── CRYP_AES_DMA │ └── CRYP_AESGCM ├── DMA │ ├── DMA_LinkedList │ └── DMA_RepeatedBlock ├── GPIO │ └── GPIO_EXTI ├── I2C │ ├── I2C_TwoBoards_ComDMA │ └── I2C_TwoBoards_ComPolling ├── I3C │ └── I3C_Controller_I2C_ComDMA ├── LPTIM │ └── LPTIM_PulseCounter ├── SPI │ └── SPI_FullDuplex_ComDMA └── TIM ├── TIM_DMABurst ├── TIM_OnePulse ├── TIM_PWMOutput └── TIM_TimeBase
4.2.1.2. ThreadX applications[edit source]
4.2.1.3. USBX Device applications[edit source]
4.2.1.4. NetX Duo applications[edit source]
4.2.1.5. FileX applications[edit source]
STM32CubeMP2 package provides the following set of applications :
Application | Short description |
---|---|
Fx_NoR_Write_Read_File | Demonstrates how to create a Fat File system on the NOR flash using FileX alongside LevelX. The application is designed to execute file operations on the MX25L51245G NOR flash device, the code provides all required software code for properly managing it. For more information, refer to the application Projects/STM32MP257F-EV1/Applications/FileX/Fx_NoR_Write_Read_File/README.md file. |
Fx_SRAM_File_Edit_Standalone | This application provides an example of FileX stack usage in Standalone mode (without ThreadX). It demonstrates how to create a FAT File system in internal SRAM using FileX API. For more information, refer to the application Projects/STM32MP257F-EV1/Applications/FileX/Fx_SRAM_File_Edit_Standalone/README.md file. |
4.2.1.6. LevelX applications[edit source]
5. Get started with STM32CubeMP25 Package[edit source]
To know how to get it, read STM32CubeMP2 Package - Getting Started article.