This article aims to give general information about the x-linux-ai tool. presenting its core features, potential applications, and benefits to users seeking to leverage its capabilities within STM32MPU.
1. Description[edit source]
1.1. What is X-LINUX-AI Tool ?[edit source]
The X-LINUX-AI tool is a software designed to verify the current version of X-Linux-AI and to display a comprehensive list of all the available features and applications. The feature set provided is specifically designed for the development of artificial intelligence applications, offering a comprehensive suite of tools and frameworks. This includes TensorFlow™ Lite with the XNNPACK delegate for optimized performance, native support for the Coral Edge TPU™ accelerator, and ONNX Runtime™ with XNNPACK for executing ONNX models. OpenCV 4.7.x enhances image processing capabilities. Support for the Sony™ IMX335 5Mpx
sensor and access to the AI package repository of OpenSTLinux round out this robust offering, allowing for easy
integration and management of AI components.
The X-LINUX-AI Tool is designed to simplify the management and utilization of AI (Artificial Intelligence) capabilities on devices running OpenSTLinux. It offers the essential tools for effective management of AI packages, which is invaluable for a wide range of applications from industrial to educational purposes.
The X-LINUX-AI version is synchronized with the OpenSTLinux version, evolving based on the alterations made throughout the development cycle. Major changes prompt an update to the middle digit in the version number, following the pattern 5.x.0, where 'x' is indicative of the sequence of significant updates. For minor improvements , the last digit is increased, according to the 5.0.x format. The initial '5' denotes the current version of OpenSTLinux.
1.2. Key Features[edit source]
- Simplified AI package management: The X-LINUX-AI Tool provides a user-friendly interface that allows users to navigate through various options for managing AI-related software packages.
- Compatibility checks: It ensures that the AI packages we are using are compatible with our specific hardware setup, which is crucial for optimal performance and stability.
2. X-LINUX-AI Tool installation[edit source]
After having configured the AI OpenSTLinux package you can install the X-LINUX-AI components.
apt-get install x-linux-ai-tool
3. How to use X-LINUX-AI Tool:[edit source]
Usage: x-linux-ai -[option] -v --version : Show X-LINUX-AI current version if it is installed -f --supported-features : Print all supported frameworks in this X-LINUX-AI version -l --list : Print installed and ready-to-install packages -i --install <pkg> : Install X-LINUX-AI package -r --remove <pkg> : Remove X-LINUX-AI package -h --help : Show this help
3.1. Usage Example[edit source]
The following command can be used to show the version of x-linux-ai:
x-linux-ai -v
X-LINUX-AI version: v5.0.0
For displaying the features of x-linux-ai, refer to the command provided below:
x-linux-ai -f
root@stm32mp1:# x-linux-ai -f Features: * TensorFlow™ Lite 2.11.0 with XNNPACK delegate activated * Coral Edge TPU™ accelerator native support * libedgetpu 2.0.0 (Grouper) aligned with TensorFlow™ Lite 2.11.0 * libcoral 2.0.0 (Grouper) aligned with TensorFlow™ Lite 2.11.0 * PyCoral 2.0.0 (Grouper) aligned with TensorFlow™ Lite 2.11.0 * ONNX Runtime™ 1.14.0 with XNNPACK execution engine activated * OpenCV 4.7.x * Python™ 3.11.x * Support of Sony™ IMX335 5Mpx sensor with use of DCMIPP and internal ISP * Support for the OpenSTLinux AI package repository allowing the installation of a prebuilt package using apt-* utilities * Application : * Image Classification : * C++ / Python™ example using TensorFlow™ Lite based on the MobileNet v3 quantized model * C++ / Python™ example using Coral Edge TPU™ based on the MobileNet v1 quantized model and compiled for the Edge TPU™ * Python™ example using ONNX Runtime based on the MobileNet v3 quantized model * C++ example using Network Binary Graph based on MobileNet v3 quantized model * Object Detection : * C++ example using TensorFlow™ Lite based on the COCO SSD MobileNet v1 quantized model * Python™ example using TensorFlow™ Lite based on the YoloV4-tiny quantized model * C++ / Python™ example using Coral Edge TPU™ based on the COCO SSD MobileNet v1 quantized model and compiled for the Edge TPU™ * C++ / Python™ example using ONNX Runtime based on the COCO SSD MobileNet v1 quantized model * Face Recognition : * C++ example using proprietary model capable of recognizing the face of a known (enrolled) user. Contact the local STMicroelectronics support for more information about this application or send a request to edge.ai@st.com * Human Pose Estimation * Python™ example using TensorFlow™ Lite based on Movenet SinglePose Lightning quantized model * Semantic Segmentation * Python™ example using TensorFlow™ Lite based on DeepLabV3 quantized model * Application support for the 1080p, 720p, 480p, and 272p display configurations * X-LINUX-AI SDK add-on extending the OpenSTLinux SDK with AI functionality to develop and build an AI application easily. The X-LINUX-AI SDK add-on provides support for all the above frameworks. It is available from the [X-LINUX-AI] STM32MP25-beta repository ## Further information on how to install and how to use X-LINUX-AI Starter package <https://wiki.st.com/stm32mp25-beta-v5/wiki/X-LINUX-AI_Starter_package> ## Further information on how to install and how to use X-LINUX-AI Developer package <https://wiki.st.com/stm32mp25-beta-v5/wiki/X-LINUX-AI_Developer_package> ## Further information on how to install and how to use X-LINUX-AI Distribution package <https://wiki.st.com/stm32mp25-beta-v5/wiki/X-LINUX-AI_Distribution_package> ## Application samples Find more information on the wiki page: https://wiki.st.com/stm32mpu/wiki/X-LINUX-AI_OpenSTLinux_Expansion_Package
x-linux-ai -l
root@stm32mp1:# x-linux-ai -l [installed] coral-edgetpu-benchmark [installed] libedgetpu2 [installed] libtensorflow-lite2 [installed] tflite-vx-delegate [installed] tim-vx [installed] x-linux-ai-benchmark [not installed] coral-image-classification-cpp [not installed] coral-image-classification-python [not installed] coral-models-coco-ssd-mobilenetv1 [not installed] coral-models-mobilenetv1 [not installed] coral-object-detection-cpp [not installed] coral-object-detection-python [not installed] libcoral2 [not installed] libtensorflow-lite-tools [not installed] onnx-image-classification-python [not installed] onnx-models-coco-ssd-mobilenetv1 [not installed] onnx-models-mobilenetv1 [not installed] onnx-models-mobilenetv3 [not installed] onnx-object-detection-cpp [not installed] onnx-object-detection-python [not installed] onnxruntime [not installed] onnxruntime-tools [not installed] onnxruntime-unit-tests [not installed] packagegroup-x-linux-ai [not installed] packagegroup-x-linux-ai-coral [not installed] packagegroup-x-linux-ai-npu [not installed] packagegroup-x-linux-ai-onnxruntime [not installed] packagegroup-x-linux-ai-tflite [not installed] python3-libtensorflow-lite [not installed] python3-onnxruntime [not installed] python3-pycoral [not installed] tflite-face-recognition-cpp [not installed] tflite-image-classification-cpp [not installed] tflite-image-classification-python [not installed] tflite-models-coco-ssd-mobilenetv1 [not installed] tflite-models-deeplabv3 [not installed] tflite-models-mobilenetv1 [not installed] tflite-models-mobilenetv3 [not installed] tflite-models-movenet-singlepose-lightning [not installed] tflite-models-yolov4-tiny [not installed] tflite-object-detection-cpp [not installed] tflite-object-detection-python [not installed] tflite-pose-estimation-python [not installed] tflite-semantic-segmentation-python [not installed] tim-vx-tools
x-linux-ai -i <package>
root@stm32mp25-revab:~# x-linux-ai -i onnxruntime Reading package lists... Done Building dependency tree... Done Reading state information... Done The following NEW packages will be installed: onnxruntime 0 upgraded, 1 newly installed, 0 to remove and 16 not upgraded. Need to get 0 B/6089 kB of archives. After this operation, 0 B of additional disk space will be used. The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found at https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses. Selecting previously unselected package onnxruntime. (Reading database ... 18419 files and directories currently installed.) Preparing to unpack .../onnxruntime_1.14.0+git0+6ccaeddefa-r0_arm64.deb ... Unpacking onnxruntime (1.14.0+git0+6ccaeddefa-r0) ... Setting up onnxruntime (1.14.0+git0+6ccaeddefa-r0) ... N: Ignoring file 'packages.openstlinux.st.com.list.tmp' in directory '/etc/apt/sources.list.d/' as it has an invalid filename extension onnxruntime has been installed successfully.
x-linux-ai -r <package>
root@stm32mp25-revab:~# x-linux-ai -r onnxruntime Reading package lists... Done Building dependency tree... Done Reading state information... Done The following packages will be REMOVED: onnxruntime 0 upgraded, 0 newly installed, 1 to remove and 16 not upgraded. After this operation, 0 B of additional disk space will be used. The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found at https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses. (Reading database ... 18423 files and directories currently installed.) Removing onnxruntime (1.14.0+git0+6ccaeddefa-r0) ... N: Ignoring file 'packages.openstlinux.st.com.list.tmp' in directory '/etc/apt/sources.list.d/' as it has an invalid filename extension onnxruntime has been removed successfully.