X-LINUX-AI Tool

Revision as of 14:26, 11 April 2024 by Registered User

This article aims to give general information about the x-linux-ai tool. (il faut developper encore un petit peu)

1. Description[edit source]

1.1. What is X-LINUX-AI Tool ?[edit source]

The X-LINUX-AI tool is a software designed to verify the current version of X-Linux-AI and to display a comprehensive list of all the available features and applications. The feature set provided is specifically designed for the development of artificial intelligence applications, offering a comprehensive suite of tools and frameworks. This includes TensorFlow™ Lite with the XNNPACK delegate for optimized performance, native support for the Coral Edge TPU™ accelerator, and ONNX Runtime™ with XNNPACK for executing ONNX models. OpenCV 4.7.x enhances image processing capabilities. Support for the Sony™ IMX335 5Mpx sensor and access to the AI package repository of OpenSTLinux round out this robust offering, allowing for easy integration and management of AI components.

The X-Linux-AI version is synchronized with the OpenSTLinux version, evolving based on the alterations made throughout the development cycle. Major changes prompt an update to the middle digit in the version number, following the pattern 5.x.0, where 'x' is indicative of the sequence of significant updates. For minor improvements , the last digit is increased, according to the 5.0.x format. The initial '5' denotes the current version of OpenSTLinux.

2. X-LINUX-AI Tool installation[edit source]

Warning white.png Warning
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.

After having configured the AI OpenSTLinux package you can install the X-LINUX-AI components.

    apt-get install x-linux-ai-tool

3. How to use X-LINUX-AI Tool:[edit source]

Usage:x-linux-ai

-v --version :  Show X-LINUX-AI current version if it is installed
-f --supported-features : Print all supported frameworks in this X-LINUX-AI version
-a --supported-appli :    Print all delivered applications in this X-LINUX-AI version
-h --help :     Show this help


3.1. Usage Example[edit source]

    x-linux-ai -v
X-LINUX-AI version: v5.0.0
    x-linux-ai -f
Features:
 * TensorFlow™ Lite 2.11.0 with XNNPACK delegate activated 
 * ONNX Runtime 1.14.0 with XNNPACK execution engine activated 
 * OpenCV 4.7.x 
 * Python™ 3.10.x (enabling Pillow module) 
 * Coral Edge TPU™ accelerator native support 
   * libedgetpu 2.0.0 (Gouper) aligned with TensorFlow™ Lite 2.11.0 
   * libcoral 2.0.0 (Gouper) aligned with TensorFlow™ Lite 2.11.0 
   * PyCoral 2.0.0 (Gouper) aligned with TensorFlow™ Lite 2.11.0 
 * Support for the OpenSTLinux AI package repository allowing the installation of a prebuilt package using apt-* utilities
Find more informations on the wiki page: https://wiki.st.com/stm32mpu/wiki/X-LINUX-AI_OpenSTLinux_Expansion_Package
   x-linux-ai -a 
Applications:
 * C++ / Python™ image classification example using TensorFlow™ Lite based on the MobileNet v1 quantized model 
 * C++ / Python™ object detection example using TensorFlow™ Lite based on the COCO SSD MobileNet v1 quantized model 
 * C++ / Python™ image classification example using Coral Edge TPU™ based on the MobileNet v1 quantized model and compiled for the Edge TPU™ 
 * C++ / Python™ object detection example using Coral Edge TPU™ based on the COCO SSD MobileNet v1 quantized model and compiled for the Edge TPU™ 
 * C++ face recognition application using proprietary model capable of recognizing the face of a known (enrolled) user. Contact the local STMicroelectronics support for more information about this application or send a request to edge.ai@st.com 
 * Python™ image classification example using ONNX Runtime based on the MobileNet v1 quantized model 
 * C++ / Python™ object detection example using ONNX Runtime based on the COCO SSD MobileNet v1 quantized model