- Last edited 2 weeks ago ago
How to play audio
Contents
1 Article purpose[edit]
This article explains how to play audio through the ALSA audio framework in Linux® OS context. The examples below, show how to play audio on the different audio hardware interfaces of the STM32MPU boards.
2 Audio playback overview[edit]
The ALSA framework exposes audio devices associated to the board audio hardware interfaces.
The application audio streams are routed by default through the PulseAudio sound server. PulseAudio exposes audio profiles which are mapped on the ALSA sound card audio devices. The PulseAudio server provides a command line interface which allows to list audio profiles and to select a profile, to play on a specific audio interface.
The audio playback examples in following sections are given for ALSA utilities. However, the audio playbacks can be launched by other applications, such as gstreamer multimedia framework.
3 Examples[edit]
3.1 Audio playback on headset output[edit]
3.1.1 Playback on ALSA device[edit]
Run audio playback on 'playback_codec' ALSA device:
![]() |
'playback_codec' is an alias defined in /etc/asound.conf, for headset output device. |
Board $> aplay -D playback_codec /usr/share/sounds/alsa/Front_Left.wav
3.1.2 Playback via PulseAudio[edit]
- Configure Pulseaudio
Change the Pulseaudio active profile of the sound card, to 'analog-stereo' profile:
![]() |
The Pulseaudio analog-stereo profile is the default profile. So next command is not required after boot. |
![]() |
Example below is given for sound card index 0. Check sound cards index with "pactl list cards short" command. |
Board $> pacmd set-card-profile 0 output:analog-stereo+input:analog-stereo
- Run audio playback:
Board $> aplay /usr/share/sounds/alsa/Front_Left.wav
3.2 Audio playback on HDMI output[edit]
![]() |
The support of HDMI output is board dependent. Please, check available outputs with "aplay -l" command. |
3.2.1 Playback on ALSA device[edit]
Run audio playback on 'playback_hdmi' ALSA device:
![]() |
'playback_hdmi' is an alias defined in /etc/asound.conf, for hdmi output device. |
Board $> aplay -D playback_hdmi /usr/share/sounds/alsa/Front_Left.wav
3.2.2 Playback via PulseAudio[edit]
- Configure Pulseaudio
Change the Pulseaudio active profile of the sound card, to 'hdmi-stereo' profile:
![]() |
Example below is given for sound card index 0. Check sound card index with "pactl list cards short" command. |
Board $> pacmd set-card-profile 0 output:hdmi-stereo
- Run audio playback:
Board $> aplay /usr/share/sounds/alsa/Front_Left.wav
3.3 Audio playback on S/PDIF output[edit]
![]() |
The support of S/PDIF output is board dependent. Please, check available outputs with "aplay -l" command. |
3.3.1 Set IEC958 status bits[edit]
Example: set IEC958 mode bit.
Board $> iecset -c STM32MP1EV -n device=0 pro on
3.3.2 Playback on ALSA device[edit]
Run audio playback on 'playback_spdif' ALSA device:
![]() |
'playback_spdif' is an alias defined in /etc/asound.conf, for S/PDIF output device. |
Board $> speaker-test -D playback_spdif -c 2 -F S32_LE -f 440 -t sine -l 1
3.3.3 Playback via PulseAudio[edit]
- Configure Pulseaudio
Change the sound card active profile, to S/PDIF 'iec958-stereo' profile.
![]() |
Example below is given for sound card index 0. Check sound card index with "pactl list cards short" command. |
Board $> pacmd set-card-profile 0 output:iec958-stereo
- Run audio playback:
Board $> speaker-test -c 2 -F S32_LE -f 440 -t sine -l 1