- Last edited 8 months ago ago
SDMMC device tree configuration
Contents
1 Article purpose[edit]
This article explains how to configure the SDMMC internal peripheral when it is assigned to the Linux® OS. In that case, it is controlled by the MMC framework.
The configuration is performed using the device tree mechanism that provides a hardware description of the SDMMC peripheral, used by the STM32 SDMMC Linux driver and by the MMC framework.
If the peripheral is assigned to another execution context, refer to How to assign an internal peripheral to a runtime context article for guidelines on peripheral assignment and configuration.
2 DT bindings documentation[edit]
The SDMMC device tree bindings are composed of:
- generic MMC device tree bindings [1].
- SDMMC MMC/SD/SDIO interface bindings [2].
3 DT configuration[edit]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.
STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1 DT configuration (STM32 level)[edit]
The SDMMC peripheral node is located in stm32mp151.dtsi[3] file.
sdmmc1: sdmmc@58005000 { Comments compatible = "arm,pl18x", "arm,primecell"; arm,primecell-periphid = <0x00253180>; reg = <0x58005000 0x1000>, --> The controller register location <0x58006000 0x1000>; --> The delay block register location interrupts = <GIC_SPI 49 IRQ_TYPE_LEVEL_HIGH>; --> The interrupt number used interrupt-names = "cmd_irq"; clocks = <&rcc SDMMC1_K>; clock-names = apb_pclk resets = <&rcc SDMMC1_R>; status = "disabled"; };
![]() |
This device tree part is related to STM32 microprocessors. It should be kept as is, without being modified by the end-user. |
3.2 DT configuration (board level)[edit]
The SDMMC peripheral may connect to one SD card, one e•MMC™ device or one SDIO card.
&sdmmc1{ Comments pinctrl-names = "default", "opendrain", "sleep"; --> For pinctrl configuration, please refer to Pinctrl device tree configuration pinctrl-0 = <&sdmmc1_b4_pins_a &sdmmc1_dir_pins_a>; pinctrl-1 = <&sdmmc1_b4_od_pins_a &sdmmc1_dir_pins_a>; pinctrl-2 = <&sdmmc1_b4_sleep_pins_a &sdmmc1_dir_sleep_pins_a>; st,neg-edge; --> Generate data and command on sdmmc clock falling edge st,sig-dir; --> Allow to select direction polarity of an external transceiver st,use-ckin; --> Use sdmmc_ckin pin from an external transceiver to sample the receive data bus-width = <4>; --> Number of data lines, can be 1, 4 or 8 vmmc-supply = <&vdd_sd>; --> Supply node for card's power vqmmc-supply = <&sd_switch>; --> Supply node for IO line power status = "okay"; --> Enable the node };
Below optional properties have to be used when an external transceiver is connected:
- st,sig-dir: This property allows to select external transceiver direction signals polarity. When this property is set, the voltage transceiver IOs are driven as output when the direction signals are high. Without setting this property, the voltage transceiver IOs are driven as output when the direction signals are low.
- st,use-ckin: By setting this property, the sdmmc_ckin pin from an external transceiver is used to sample the receive data.
3.3 DT configuration examples[edit]
Below example shows how to configure the SDMMC when an e•MMC™ is connected with 8 data lines [4].
&sdmmc2{ Comments pinctrl-names = "default", "opendrain", "sleep"; pinctrl-0 = <&sdmmc2_b4_pins_a &sdmmc2_dir_pins_a>; pinctrl-1 = <&sdmmc2_b4_od_pins_a &sdmmc2_dir_pins_a>; pinctrl-2 = <&sdmmc2_b4_sleep_pins_a &sdmmc2_dir_sleep_pins_a>; non-removable; --> Non-removable slot, assume always present no-sd; --> Avoid to send SD command during initialization no-sdio; --> Avoid to send SDIO command during initialization st,neg-edge; bus-width = <8>; vmmc-supply = <&v3v3>; vqmmc-supply = <&vdd>; mmc-ddr-3_3v; --> Host supports e•MMC™ DDR 3.3V status = "okay"; };
Below example shows how to configure the SDMMC to SD card (4 data lines) with an external transceiver [4].
&sdmmc1{ Comments pinctrl-names = "default", "opendrain", "sleep"; pinctrl-0 = <&sdmmc1_b4_pins_a &sdmmc1_dir_pins_a>; pinctrl-1 = <&sdmmc1_b4_od_pins_a &sdmmc1_dir_pins_a>; pinctrl-2 = <&sdmmc1_b4_sleep_pins_a &sdmmc1_dir_sleep_pins_a>; broken-cd; --> use polling mode for card detection st,neg-edge; st,sig-dir; st,use-ckin; bus-width = <4>; sd-uhs-sdr12; --> sd modes supported [1] sd-uhs-sdr25; sd-uhs-sdr50; sd-uhs-ddr50; sd-uhs-sdr104; vmmc-supply = <&vdd_sd>; vqmmc-supply = <&sd_switch>; status = "okay"; };
4 How to configure the DT using STM32CubeMX[edit]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.
5 References[edit]
Please refer to the following links for additional information: