This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1 STM32CubeMX 6.9.0 - MPU support[edit source]
Main updates
- The bundled JRE™ is Adoptium® Temurin™ 17.0.6 and JavaFX-17.0.2
Main fixes
- 155060 - [STM32CubeMX] [RCC] PLL2R initialization not generated in device tree.
- 141444 - Keep ST boards compatibility in DT when selecting a project from Board selector
- 136275 - [DTGen] SocAllIPs IOCs do not compile due to missing driver in OSTL
- Download the all-in-one Windows installer from st.com
- Windows Installer - STM32CubeIDE-Mac
STM32CubeMX for Linux®, Windows® and macOS ® | ||
---|---|---|
Download |
Version 6.9.0
| |
Installation guide | ||
User manual | ||
Detailed release note |
|
Minor releases may be available from the update site.