This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.PRG-TOOLBOX-FB is an open-source tool provided by STMicroelectronics. This tool is designed to take advantage of Fastboot high transfer bandwidth, to write into external flash memory (like eMMC, SDMMC…).
Fastboot (FB) is a protocol that was originally created for Android™ and is primarily used to modify the flash filesystem via a USB connection from a host computer.
The tool is a wrapper for Fastboot. It is specifically designed for STM32 MPU products.
More information can be found in the detailed release notes referenced later in this article.
1 PRG-TOOLBOX-FB - Version v1.0.0[edit source]
PRG-TOOLBOX-FB for STM32 Arm® Cortex® MPUs . | ||
---|---|---|
Download |
Version v1.0.0
| |
Compile |
| |
Contents |
|