This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article is only applicable for STMP32 Microprocessor with more than one CPU.
1 How to see the number of active CPU[edit source]
root@st:~# cat /proc/cpuinfo processor : 0 model name : ARMv7 Processor rev 0 (v7l) BogoMIPS : 2387.14 Features : swp half thumb fastmult vfp edsp neon vfpv3 tls CPU implementer : 0x41 CPU architecture: 7 CPU variant : 0x3 CPU part : 0xc09 CPU revision : 0 processor : 1 model name : ARMv7 Processor rev 0 (v7l) BogoMIPS : 2393.70 Features : swp half thumb fastmult vfp edsp neon vfpv3 tls CPU implementer : 0x41 CPU architecture: 7 CPU variant : 0x3 CPU part : 0xc09 CPU revision : 0 Hardware : STi SoC with Flattened Device Tree Revision : 0000 Serial : 0000000000000000
2 How to disable a CPU[edit source]
On this example we disable CPU1
root@st:~# echo 0 > /sys/devices/system/cpu/cpu1/online CPU1: shutdown root@st:~# cat /proc/cpuinfo processor : 0 model name : ARMv7 Processor rev 0 (v7l) BogoMIPS : 2387.14 Features : swp half thumb fastmult vfp edsp neon vfpv3 tls CPU implementer : 0x41 CPU architecture: 7 CPU variant : 0x3 CPU part : 0xc09 CPU revision : 0 Hardware : STi SoC with Flattened Device Tree Revision : 0000 Serial : 0000000000000000
3 How to enable a disabled CPU[edit source]
On this example we enable CPU1
root@st:~# echo 1 > /sys/devices/system/cpu/cpu1/online CPU1: shutdown