- Last edited 9 months ago ago
Gst-play
Contents
1 Overview[edit]
gst-play (gst-play-1.0) is a GStreamer command line utility available with GStreamer-1.X.
This utility plays multimedia content using the Playbin element as a basic player. It takes as an input either individual files, URLs or a whole directories (in this case it will recurse into sub-directories as well).
2 Usage[edit]
gst-play accepts the following options:
Board $> gst-play-1.0 --help
Usage: gst-play-1.0 [OPTION?] FILE1|URI1 [FILE2|URI2] [FILE3|URI3] ... Help Options: -h, --help Show help options --help-all Show all help options --help-gst Show GStreamer Options Application Options: -v, --verbose Output status information and property notifications --flags Control playback behaviour setting playbin 'flags' property --version Print version information and exit --videosink Video sink to use (default is autovideosink) --audiosink Audio sink to use (default is autoaudiosink) --gapless Enable gapless playback --shuffle Shuffle playlist --no-interactive Disable interactive control via the keyboard --volume Volume --playlist Playlist file containing input media files -q, --quiet Do not print any output (apart from errors)
The user can control the playback through the host terminal keyboard. Press k to list the available keyboard shortcuts once the content is playing:
<space> Pause/Resume playback <up/down arrows> Volume up/down <left/right arrows> Seek back/forward +/- Increase/decrease playback rate d Reverse playback direction t Cycle through trick modes a Switch audio track s Switch subtitle track v Switch video track > Skip to next item in playlist < Go back to previous item in playlist q, ESC Quit
Information provided by gst-play Ubuntu manual
3 Examples[edit]
![]() |
Don't have /usr/local/demo/media/ST2297_visionv3.webm ? Follow instructions in this article. |
![]() |
To hear audio track, depending on the considered board, an audio headset must be plugged on |
3.1 Basic audio/video playback[edit]
Board $> gst-play-1.0 /usr/local/demo/media/ST2297_visionv3.webm
3.2 Video only playback[edit]
Board $> gst-play-1.0 /usr/local/demo/media/ST2297_visionv3.webm --audiosink=fakesink
Audio rendering is disabled, but audio decoding continues.
3.3 Playlist playback[edit]
Board $> gst-play-1.0 /usr/local/demo/media/ST2297_visionv3.webm /usr/local/demo/media/ST2297_visionv3.webm /usr/local/demo/media/ST2297_visionv3.webm /usr/local/demo/media/ST2297_visionv3.webm
Press ">" key to play the next file, "<" key to play the previous one.
3.4 Loop or repeat the same video[edit]
This option is not currently available within gst-play but here are some alternatives:
- Playlist with the same video over and over. In the example below, the same video file is played 3 times. The video file can be added as many times as needed:
Board $> gst-play-1.0 /usr/local/demo/media/ST2297_visionv3.webm /usr/local/demo/media/ST2297_visionv3.webm /usr/local/demo/media/ST2297_visionv3.webm
- For loop (here 1000 times):
Board $> for i in `seq 1 1000`;do gst-play-1.0 /usr/local/demo/media/ST2297_visionv3.webm; done
3.5 Seek while playing[edit]
Board $> gst-play-1.0 /usr/local/demo/media/ST2297_visionv3.webm /usr/local/demo/media/ST2297_visionv3.webm /usr/local/demo/media/ST2297_visionv3.webm /usr/local/demo/media/ST2297_visionv3.webm
Press "right arrow key" to seek forward, "left arrow key" to seek backward.
3.6 Change playback speed[edit]
Board $> gst-play-1.0 /usr/local/demo/media/ST2297_visionv3.webm
Press "+" key to increase rate and "-" key to decreased it.
3.7 HTTP streaming[edit]
![]() |
An internet connection is required, for example by plugging an Ethernet cable on |
Board $> gst-play-1.0 https://github.com/STMicroelectronics/meta-st-openstlinux/blob/thud/recipes-samples/demo/demo-launcher/media/ST2297_visionv3.webm?raw=true
3.8 Audio/video playback on HDMI TV[edit]
![]() |
Plug first HDMI TV cable as described in How to display on HDMI article |
Switch audio output on HDMI:
Board $> pacmd set-card-profile 0 output:hdmi-stereo
Than play the video:
Board $> gst-play-1.0 /usr/local/demo/media/ST2297_visionv3.webm
3.9 Audio/video playback in background[edit]
Option --no-interactive must be set in order to be able to play in background:
Board $> gst-play-1.0 /usr/local/demo/media/ST2297_visionv3.webm --no-interactive &
[1] 14998
root@stm32mp1:~# Now playing /av_h264_main_640x480_30fps_1000kbps_aac-lc_192kbps.mp4
Then to stop playback:
Board $> killall gst-play-1.0
or
Board $> fg <CTRL+C>