Template:ArticleMainWriter Template:ArticleApprovedVersion
1 Introduction[edit source]
Configfs[1] is a RAM-based filesystem that provides the converse of sysfs functionality.
While sysfs provides a filesystem-based view of kernel objects, configfs is a filesystem-based manager of kernel objects or config_items (every object in configfs is a config_item). This means that kernel objects can be created, managed and destroyed from the user space.
2 Installing configs on your target board[edit source]
Configfs can be enabled and ready to be used in all STM32MPU Embedded Software distribution, via the Linux® kernel configuration CONFIG_CONFIGFS_FS (set to yes by default):
Symbol: CONFIGFS_FS Location: File systems ---> Pseudo filesystems --> -*- Userspace-driven configuration filesystem
Please refer to Menuconfig or how to configure kernel article for instructions for modifying the configuration and recompiling the Linux kernel image in the Distribution Package context.
3 Getting started[edit source]
3.1 How to mount configfs[edit source]
Use the following command to mount Configfs at /sys/kernel/config:
mount -t configfs none /sys/kernel/config
3.2 How to set and manage configfs from Linux kernel drivers and user space[edit source]
Refer to the Linux documentation[1] for detailed information.
Configfs is used by the USB framwework. Refer to USB API description for an example.