This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Change propagation updates are pending (1 job estimated) and it is recommended to wait with modifications to a category until the process has been finalized to prevent intermediary interruptions or contradictory specifications.
This category groups together all articles and subcategories related to the STM32PRG-TOOLBOX.
STM32PRG-TOOLBOX provides an open-source tools for STM32 Arm® Cortex® MPUs to flash and update the target flash memory using Fastboot mode.
This package is composed by:
- PRG-TOOLBOX-DFU: to install U-Boot, launch Fastboot mode and manage OTP.
- PRG-TOOLBOX-FB: to flash memory partitions through Fastboot interface.
The user can start from these preconfigured projects to configure its STM32 Arm® Cortex® MPUs and customize the boot/flashing sequence corresponding to its specific use case.
For more detailed information about each tool, please refer to the subcategory pages.
Subcategories
This category has the following 2 subcategories, out of 2 total.