This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or
pending task to finish installation of
Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
STM32CubeProgrammer is the official STMicroelectronics tool to download firmware into STMicroelectronics boards.
1. STM32CubeProgrammer - Version v2.15.0[edit source]
|
STM32CubeProgrammer for Linux® host PC |
STM32CubeProgrammer for Windows® host PC
|
Download
|
Version v2.15.0
- Go on st.com to download the STM32CubeProgrammer software
- Download the archive file on your host PC in a temporary directory
- Uncompress the archive file to get the STM32CubeProgrammer installers:
unzip en.stm32cubeprog.zip
|
Installation
|
- Execute the Linux installer, which guides you through the installation process.
$> ./SetupSTM32CubeProgrammer-2.15.0.linux
- The path to the STM32CubeProgrammer binary must be added to the PATH environment variable
- either in each Terminal program in which the STM32CubeProgrammer binary needs to be used, using the following command:
$> export PATH=<my STM32CubeProgrammer install directory>/bin:$PATH
- or once for all by creating a link to the STM32CubeProgrammer binary in a directory already present in PATH. For example, if "/home/bin" is in the PATH environment variable, run the following command:
$> ln -s <my STM32CubeProgrammer install directory>/bin/STM32_Programmer_CLI /home/bin/STM32_Programmer_CLI
|
- Execute the Windows installer, which guides you through the installation process.
|
User manual
|
|
Detailed release note
|
- Details about the content of this tool version are available from ST web site at Release Note .
|