DMAMUX internal peripheral

Revision as of 15:30, 16 September 2021 by Registered User (→‎Peripheral overview)
Applicable for STM32MP13x lines, STM32MP15x lines

Unspecified MPUs checklist


1. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the DMAMUX peripheral and its main features
  • indicate the level of security supported by this hardware block
  • explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
  • explain, when necessary, how to configure the DMAMUX peripheral.

2. Peripheral overview[edit source]

The DMAMUX peripheral is used to perform requestor line (or device controller) selection for each channel from DMA instances:

  • In STM32MP13x lines More info.png there is a first DMAMUX instance to cover both DMA1 and DMA2, and second DMAMUX instance to cover DMA3.
  • In STM32MP15x lines More info.png there is a single DMAMUX instance to cover both DMA1 and DMA2.

2.1. Features[edit source]

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.

2.2. Security support[edit source]

  • In STM32MP13x lines More info.png the first DMAMUX instance, covering both DMA1 and DMA2, is a non secure peripheral.
  • In STM32MP13x lines More info.png the second DMAMUX instance, covering DMA3, is a secure peripheral.

3. Peripheral usage and associated software[edit source]

3.1. Boot time[edit source]

The DMAMUX is not used at boot time.

3.2. Runtime[edit source]

3.2.1. Overview[edit source]

The DMAMUX manages DMA1 and DMA2 requestor line selection via different registers so it is possible to concurrently access to DMAMUX from Cortex®-A7 non-secure and Cortex®-M4 contexts, as far as each core is only configuring the requestor lines for the DMA instances (DMA1 and/or DMA2) assigned to itself.

Finally, DMAMUX can be allocated to:

  • the Arm® Cortex®-A7 non-secure core to be controlled in Linux® by the dmaengine framework

or

  • the Arm® Cortex®-M4 to be controlled in STM32Cube MPU Package by the DMA HAL driver

3.2.2. Software frameworks[edit source]

Internal peripherals software table template

| Core/DMA
| DMAMUX
| 
| Linux dmaengine framework
| STM32Cube DMAMUX driver
|
|-
|}

3.2.3. Peripheral configuration[edit source]

The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.

3.2.4. Peripheral assignment[edit source]

Internal peripherals assignment table template

| rowspan="1" | Core/DMA
| rowspan="1" | DMAMUX
| DMAMUX
|
| 
| 
| Shareable (multiple choices supported)
|-
|}