1. Article purpose[edit source]
This article describes the FlashLayout file format.
This file is used as an input by STM32CubeProgrammer tool in order to:
- define the Flash memory partitions (see STM32MP15_Flash_mapping)
- select the files used to boot (see Boot chain overview) and then populate each partition.
The embedded programming service processes this file on the device and interacts with STM32CubeProgrammer to update the Flash memory.
This is done by the stm32prog
command in U-Boot. This command is automatically executed for a serial boot (bootcmd on USB or UART boot). However you can launch it manually from the U-Boot console: this is useful if you want to perform a non-virgin board update front of STM32CubeProgrammer, without manipulating the boot pins.
See AN5275: USB DFU/USART protocols used in STM32MP1 Series bootloaders for protocol details and refer to STM32CubeProgrammer article to know how to use this tool.
The next chapters:
- describe the FlashLayout file format
- give Typical FlashLayout file with FIP
- give Typical FlashLayout file without FIP (deprecated)
- give FlashLayout file to load and start kernel that can be used to load a Linux kernel for direct execution
- give some hints on the Using of the provided FlashLayout files that come as part of STM32 MPU ecosystem deliveries
The FSBL, SSBL and FIP definitions can be found in the Boot chain overview; the FIP file include the required part loaded with FSBL=TF-A, SSBL=U-Boot and eventually OP-TEE.
2. FlashLayout file format[edit source]
The FlashLayout is a text file with a tab-separated-value format (tsv). It includes the below elements:
- one line per partition or device
- seven columns, one for each field, provided in the following order:
The lines beginning with the '#' character are ignored and treated as comments.
The "Binary" last column is not used by U-Boot. It is used by STM32CubeProgrammer on the host computer to select the files to be sent to the target.
Several tabulations (<tab>) can be used to allow the correct column alignment in the editor. They are ignored by STM32CubeProgrammer and by U-Boot.
Empty fields are not allowed. The FlashLayout file format supports the none reserved word.
2.1. Examples[edit source]
Below some valid FlashLayout files:
#opt Id Name Type Device Offset Binary - 0x01 fsbl-boot Binary none 0x00000000 tf-a-usb.stm32 - 0x03 fip-boot Binary none 0x00084400 fip.bin P 0x04 fsbl1 Binary mmc0 0x00004400 tf-a-sdcard.stm32 P 0x05 fsbl2 Binary mmc0 0x00044400 tf-a-sdcard.stm32 P 0x06 fip Binary mmc0 0x00084400 fip.bin P 0x10 bootfs System mmc0 0x00484400 bootfs.ext4 P 0x10 bootfs System mmc0 0x04484400 vendorfs.ext4 P 0x11 rootfs FileSystem mmc0 0x05484400 rootfs.ext4 P 0x12 userfs FileSystem mmc0 0x33E84400 userfs.ext4
Above, the first line contains only header information. This is not mandatory, as shown below:
- 0x01 fsbl_boot Binary none 0x0 tf-a-usb.stm32 - 0x03 fip_boot Binary none 0x0 fip.bin P 0x32 sdcard RawImage mmc0 0x0 sdcard.bin
2.2. Field1: Options[edit source]
The Options field defines the operations to perform with a combination of characters: - P D E provided in any order;
First select the line of the FlashLayout with '-' or 'P':
- '-' : none option, the partition or the device is not modified (mandatory if #Field5: Device = none)
- 'P' : Program the partition or the device
- U-Boot requests the binary to STM32CubeProgrammer and programs the partition or the Flash device.
- On the block devices (SD card or e•MMC), the GPT partitioning is performed if all partitions of the device are selected with P.
- For the 'P' option, two optional modifiers can be added:
- 'E' : Empty partition or device, update is not requested (associated "Id" is skipped)
- 'D' : Delete partition or device
The only supported combinations are the following (with character in any order):
- - : no action
- P : update = program the partition or the flash device
- PE : do not update (also {{HighlightParam|EP}) : allow the GPT partitioning with empty partition for the block device but equivalent to '-' for RAW flash device
- PD : delete and update (also DP)
- PDE : delete and keep empty (also PED / DPE / DEP / EPD / EDP)
All other combinations are invalid.
2.3. Field2: Id[edit source]
Id identifies in a unique way the "download phase" requested by the device to STM32CubeProgrammer.
It is used by the embedded programming service to identify the next binary that is downloaded to the device:
- ROM code and FSBL: binary loaded in RAM
- SSBL (U-Boot): binary populated in Flash memory
The FlashLayout supported ranges are :
Range | Partition |
---|---|
0x01 to 0x0F | Boot partitions with FIP header or with STM32 header: SSBL, FSBL, other (TEE, Cortex-M4 firmware) |
0x10 to 0xF0 | user partitions programmed without header (uimage, dtb, rootfs, vendorfs, userfs) |
All the other values are forbidden in FlashLayout file.
The Id 0x01 and 0x03 are reserved for FSBL and SSBL, respectively; the presence of these two Id in the FlashLayout file is mandatory to load the embedded service.
2.3.1. Reserved Id[edit source]
The reserved and allowed values in FlashLayout file are the following:
Code | Partition |
---|---|
0x01 | FSBL : used by ROM code, load in embedded RAM |
0x03 | SSBL : used by FSBL=TF-A, load in external RAM |
For information some other Id are reserved and used for the communication between the embedded programming service and STM32CubeProgrammer, but they are forbidden in FlashLayout file.
Code | Virtual Partition or State |
---|---|
0x00 | FlashLayout |
0xF1 | Command GetPhase |
0xF2 | OTP |
0xF3 | SSP |
0xF4 | PMIC NVM |
0xFE | State = End of operation |
0xFF | State = Reset |
2.3.2. Using Id for boot partition[edit source]
When the same FSBL and SSBL binaries can be loaded in RAM and programmed in Flash memory, a simple mapping is used:
Code | Comment | Partition Description |
---|---|---|
0x01 | reserved | FSBL first copy in Flash memory, also used for serial boot, loaded by ROM code |
0x02 | default | FSBL second copy in Flash memory |
0x03 | reserved | SSBL programmed in Flash memory, also used for serial boot, loaded by FSBL |
However, in the FlashLayout file, any other Id lower than 0x10 (boot partition with FIP header or STM32 header) can identify the FSBL and SSBL binaries to be programmed in Flash memory.
It enables having different binaries loaded in RAM (with Reserved ID 0x1 and 0x3) and programmed in Flash memory, for example when an updated feature is deactivated in the binaries to be programmed in Flash memory (see example in #Load and program different binaries).
You can also skip the Id 0x2 (not reserved) to have a more coherent order, as U-Boot request and program partition in Id order, the used mapping is:
Code | Comment | Partition |
---|---|---|
0x01 | reserved | FSBL to boot with serial load support: loaded by ROM code |
0x03 | reserved | SSBL to boot with programming support : loaded by FSBL |
0x04 | FSBL to program in Flash memory (first copy) | |
0x05 | FSBL to program in Flash memory (second copy) | |
0x06 | SSBL to program in Flash memory |
Since ecosystem release v3.0.0 , this behavior is required for the STM32 MPU boot chain with Trusted Firmware-A (TF-A) as FSBL and FIP (including U-Boot) as SSBL.
The recommanded mapping duplicates ID (0x03 and 0x06) for FIP file - same file to boot and to program- and skips the Id 0x02:
Code | Comment | File | Description |
---|---|---|---|
0x01 | reserved | tf-a-usb.stm32 | FSBL to boot with serial load support on usb: TF-A BL2 |
0x03 | reserved | fip.bin | SSBL to boot, included in FIP file |
0x04 | tf-a-<dev>.stm32 | FSBL for <dev> boot device to program: first copy | |
0x05 | tf-a-<dev>.stm32 | FSBL for <dev> boot device to program: second copy | |
0x06 | fip.bin | SSBL to program, same FIP binary than SSBL to boot |
Nevertheless the minimal mapping is:
Code | Comment | File | Description |
---|---|---|---|
0x01 | reserved | tf-a-usb.stm32 | FSBL to boot with serial load support on usb: TF-A BL2 |
0x03 | reserved | fip.bin | SSBL to boot and to program = FIP image (including secure monitor -TF-A or OP-TEE- and U-Boot) |
0x02 | tf-a-<dev>.stm32 | FSBL for <dev> boot device to program: first copy | |
0x04 | tf-a-<dev>.stm32 | FSBL for <dev> boot device to program: second copy |
2.4. Field3: Name[edit source]
Name of the alternate setting of the USB DFU[1] for U-Boot enumeration. This is a string descriptor that indicates the target memory segment (see Interface Descriptor in DFU spec [2])
This is also the name of the Block device GPT partition: SD card / e•MMC.
The requirements for the GPT partitions, only for device = mmc + instance, are:
- FSBL for SD card boot: the name must start with "fsbl"= fsbl, fsbl1, fsbl2... (ROM code requirement)
- If FIP is supported by TF-A:
- SSBL for e•MMC/SD card boot: the name must be "fip"
- If the FIP is not supported by TF-A (SSBL with STM32 header, deprecated):
- SSBL for e•MMC/SD card boot: the name must be "ssbl"
- TEE partition names (when present) must use the names expected by TF-A :
- OPTEE_HEADER_IMAGE_NAME "teeh"
- OPTEE_PAGED_IMAGE_NAME "teed"
- OPTEE_PAGER_IMAGE_NAME "teex"
- a partition named "rootfs", see specific behavior described in #GPT partuuid of rootfs partition.
These requirements are not verified by U-Boot during the Flash programming. If they are not fulfilled, the ROM code or TF-A does not find the boot stage binary and the boot from Flash memory fails.
2.5. Field4: Type[edit source]
Type is only used in U-Boot to select the part of Flash memory to be updated:
- one partition
- all the #Hardware device = RawImage
The supported values are:
GPT | MTD | ||||
---|---|---|---|---|---|
Type | SD card | e•MMC | NAND Flash memory | NOR Flash memory | RAM |
Binary | x | x | x | x | x |
Binary(N) | fsbl | ||||
FileSystem | x | x | x | x | dtb |
System | x | x | UBI | UBI | kernel |
RawImage | x | user data | x | x |
2.5.1. Block device GPT partition: SD card / e•MMC[edit source]
Refer to GPT standard for details [3].
The supported values, with associated partition type GUID (globally unique identifiers[4]), are:
- Binary : raw data / linux reserved
(GUID = 8DA63339-0007-60C0-C436-083AC8230908) - FileSystem : Linux filesystem data
(GUID = 0FC63DAF-8483-4772-8E79-3D69D8477DE4)
ext2/ext4/fat file system - System : FileSystem partition marked as bootable and used by U-Boot to find extlinux.conf configuration file (normally only one in the device, generic DISTRO feature)
For a Block device, the GPT header is updated only if all the partitions of this device are selected with the P option (full update).
2.5.2. Raw Flash device (NAND/NOR Flash memories) MTD partition[edit source]
The supported values are:
- Binary: raw data, skip bad block (partition erase is not needed)
- Binary(N): raw data, skip bad block. The loaded binary is repeated N times.
It is only supported for NAND Flash memories when the partition name start with "fsbl". It is used to avoid disturbances during the first boot (uncorrectable ECC errors).
The first good block is read from NAND and duplicated N times in the same partition (write skip bad block). - FileSystem: unspecified File system, raw data
- System : normally UBI volume, U-Boot erases all the blocks following the last data in the MTD partition to avoid mount errors.
2.5.3. Hardware device[edit source]
Export the associated device as one alternate setting by using Type=RawImage.
- For SD card, NOR and NAND Flash memories: all the devices
- For e•MMC: the user data area of e•MMC (see #Field6: Offset for access to the boot area partitions)
For RawImage, Offset=0x0 and PartId >= 0x10
2.5.4. RAM device (DDR)[edit source]
The supported values are:
- Binary: raw data
- FileSystem: device tree used in the
bootm
command - System : kernel image used in the
bootm
command (uImage.bin for example)
When a RAM device is present in the FlashLayout, the programming service will not reboot but start the loaded kernel image with the associated device tree (when present, when it is absent the U-Boot device tree is used).
2.6. Field5: Device[edit source]
Select the targeted device and the instance (starting at 0) as defined by U-Boot device tree:
- mmc + instance : mmc0, mmc1, mmc2
It is used for e•MMC or SD card on SDMMC. In the below examples:- SD card = mmc0 (SDMMC1)
- e•MMC = mmc1 (SDMMC2)
- nor + instance : nor0
It is used for NOR on QUADSPI. - nand + instance : nand0
It is used for parallel NAND Flash memories on FMC. - spi-nand + instance : spi-nand0
It is used for serial NAND Flash memories on QSPI. - none only used to load the programming service in RAM
It is allowed only for the reserved bootloaders partition (FSBL=0x1 and SSBL=0x3). In this case, the only allowed fields are: Type=Binary, Offset=0x0 and option=- - ram + instance : ram0
It is used for files loaded in RAM by the programming service, for example to load and execute kernel.
Several devices can be mixed in the same FlashLayout file.
2.7. Field6: Offset[edit source]
The supported values are:
- boot1: first boot area partition of e•MMC (offset is 0x0)
- boot2: second boot area partition of e•MMC (offset is 0x0)
- Offset in Bytes: offset in Flash memory area (in the user data area for e•MMC)
Refer to #Partition sizes for offset constraints.
2.8. Field7: Binary[edit source]
This file is used by STM32CubeProgrammer to find the file associated to each Id when it is requested by embedded programming service .
The file can be absent (Binary=none in the tsv file) only for skipped partitions tagged with the E option. In all other cases, this file is sent to U-Boot to update the Flash memory only for the partitions selected with the P option.
2.9. GPT partuuid of rootfs partition[edit source]
If #Field3: Name = rootfs for block device (SD card / e•MMC), U-Boot also sets a unique partition guid [4](PARTUUID) for each instance:
- mmc0: PARTUUID = "e91c4e10-16e6-4c0e-bd0e-77becf4a3582"
- mmc1: PARTUUID = "491f6117-415d-4f53-88c9-6e0de54deac6"
- mmc2: PARTUUID = "fd58f1c7-be0d-4338-8ee9-ad8f050aeb18"
This partition PARTUUID is distinct from the filesystem UUID and it is persistent.
Refer to GPT standard for details. [3]
This value can be used with the "root" argument in the kernel bootargs to identify the partition used for the "Root filesystem". For instance, "root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582" [5] starts with the partition named rootfs on mmc0.
2.10. Partition operations[edit source]
To update only one partition, use the same FlashLayout file, keep the #Field1: Options=P for the partition to update and change the others to -.
To update fip partition:
- 0x01 fsbl-boot Binary none 0x00000000 tf-a-usb.stm32 - 0x03 fip-boot Binary none 0x00084400 fip.bin - 0x04 fsbl1 Binary mmc0 0x00004400 tf-a-sdcard.stm32 - 0x05 fsbl2 Binary mmc0 0x00044400 tf-a-sdcard.stm32 P 0x06 fip Binary mmc0 0x00084400 fip.bin - 0x10 bootfs System mmc0 0x00484400 bootfs.ext4 - 0x11 rootfs FileSystem mmc0 0x04484400 vendorfs.ext4 - 0x12 rootfs FileSystem mmc0 0x05484400 rootfs.ext4 - 0x13 userfs FileSystem mmc0 0x33E84400 userfs.ext4
To delete only one partition, add the DE option on the corresponding line.
To delete fip partition:
- 0x01 fsbl-boot Binary none 0x00000000 tf-a-usb.stm32 - 0x03 fip-boot Binary none 0x00084400 fip.bin - 0x04 fsbl1 Binary mmc0 0x00004400 tf-a-sdcard.stm32 - 0x05 fsbl2 Binary mmc0 0x00044400 tf-a-sdcard.stm32 PDE 0x06 fip Binary mmc0 0x00084400 fip.bin - 0x10 bootfs System mmc0 0x00484400 bootfs.ext4 - 0x11 rootfs FileSystem mmc0 0x04484400 vendorfs.ext4 - 0x12 rootfs FileSystem mmc0 0x05484400 rootfs.ext4 - 0x13 userfs FileSystem mmc0 0x33E84400 userfs.ext4
2.11. Partition sizes[edit source]
The partitions are contiguous (no holes in Flash memory).
The last partition continues until the end of the selected Flash memory.
To reduce the size of the last partition, use an 'Empty' partition and leave it unused.
All the partitions need to be present in the FlashLayout file, even if they are not selected or empty.
Then the offset and size of each partition are compared with:
- pre-existing GPT partitioning, for updates on block devices (e•MMC or SD card)
- predefined partitioning for MTD devices (NOR and NAND): see mtdparts environment variable in U-Boot for more information.
In case of partition size error, compare the existing partition size in U-Boot with the offset in the FlashLayout file.
2.11.1. GPT partition sizes[edit source]
Each GPT partition must be aligned to:
- 512 bytes (LBA)
- e•MMC erase group size
The first partition starts after 17 Kbytes (default size of GPT header for 128 entries in U-Boot).
Prior to updating partitions in a block device, check the partition size by executing the U-Boot command "part list" on the selected device:
part list mmc 0 Partition Map for MMC device 0 -- Partition Type: EFI Part Start LBA End LBA Name Attributes Type GUID Partition GUID 1 0x00000022 0x00000221 "fsbl1" attrs: 0x0000000000000000 type: 8da63339-0007-60c0-c436-083ac8230908 guid: 35b71598-cc09-43f0-b9e2-f2a4037202ee 2 0x00000222 0x00000421 "fsbl2" attrs: 0x0000000000000000 type: 8da63339-0007-60c0-c436-083ac8230908 guid: 3a8bb930-75b1-473a-819b-0749b62893f7 3 0x00000422 0x00002421 "fip" attrs: 0x0000000000000000 type: 8da63339-0007-60c0-c436-083ac8230908 guid: 1014bf09-4e50-418c-82a3-807576a5f25c 4 0x00002422 0x00022421 "bootfs" attrs: 0x0000000000000004 type: 0fc63daf-8483-4772-8e79-3d69d8477de4 type: linux guid: 6a1a0147-cc61-41ed-b0a7-e8fed794d4ab 5 0x00022422 0x0002a421 "vendorfs" attrs: 0x0000000000000000 type: 0fc63daf-8483-4772-8e79-3d69d8477de4 type: linux guid: 28f351bb-f287-4223-9c35-c318e0d669b1 6 0x0002a422 0x001aa421 "rootfs" attrs: 0x0000000000000000 type: 0fc63daf-8483-4772-8e79-3d69d8477de4 type: linux guid: e91c4e10-16e6-4c0e-bd0e-77becf4a3582 7 0x001aa422 0x01dacbdc "userfs" attrs: 0x0000000000000000 type: 0fc63daf-8483-4772-8e79-3d69d8477de4 type: linux guid: 3c26f1ba-c7cd-4b58-ae90-340bfe9b02bd
Warning: Start and end are indicated in multiple of LBA (512 bytes by default).
To check the e•MMC erase group size in U-Boot, select the mmc device (here 1) and use the command "mmc info" in U-Boot.
mmc dev 1 switch to partitions #0, OK mmc1(part 0) is current device mmc info Device: STM32 SD/MMC Manufacturer ID: 11 OEM: 100 Name: 004GA Bus Speed: 52000000 Mode: MMC High Speed (52MHz) Rd Block Len: 512 MMC version 5.0 High Capacity: Yes Capacity: 3.7 GiB Bus Width: 8-bit Erase Group Size: 512 KiB HC WP Group Size: 4 MiB User Capacity: 3.7 GiB WRREL Boot Capacity: 2 MiB ENH RPMB Capacity: 512 KiB ENH Boot area 0 is not write protected Boot area 1 is not write protected
2.11.2. MTD partition sizes[edit source]
Each MTD partition must be aligned to the device erase block size (NOR/NAND Flash memory).
In U-Boot command :
nand info Device 0: nand0, sector size 256 KiB Page size 4096 b OOB size 224 b Erase size 262144 b subpagesize 4096 b options 0x00084200 bbt options 0x00060000
sf probe SF: Detected mx25l51235f with page size 256 Bytes, erase size 64 KiB, total 64 MiB
For MTD, the U-Boot uses the mtdparts variable. Execute the U-Boot command mtdparts to know the current value:
mtdparts
By default on ST board, the mtdpart variable is built dynamically in board_mtdparts_default() under CONFIG_SYS_MTDPARTS_RUNTIME with the ST configs:
- CONFIG_MTDPARTS_NAND0_BOOT = "2m(fsbl),4m(fip1),4m(fip2)"
- CONFIG_MTDPARTS_NOR0_BOOT = "256k(fsbl1),256k(fsbl2),4m(fip),512k(u-boot-env)"
- CONFIG_MTDPARTS_SPINAND0_BOOT = 2m(fsbl),4m(fip1),4m(fip2)"
When FIP is not supported in U-Boot (deprecated), the used configs are:
- CONFIG_MTDPARTS_NAND0_BOOT = "2m(fsbl),2m(ssbl1),2m(ssbl2)"
- CONFIG_MTDPARTS_NAND0_TEE = "512k(teeh),512k(teed),512k(teex)"
- CONFIG_MTDPARTS_NOR0_BOOT = "256k(fsbl1),256k(fsbl2),2m(ssbl),512k(u-boot-env)"
- CONFIG_MTDPARTS_NOR0_TEE = "256k(teeh),512k(teed),256k(teex)"
- CONFIG_MTDPARTS_SPINAND0_BOOT = 2m(fsbl),2m(ssbl1),2m(ssbl2)"
- CONFIG_MTDPARTS_SPINAND0_TEE = "512k(teeh),512k(teed),512k(teex)"
On NAND Flash, the last partition 'UBI' uses the remaining space.
On NOR Flash, the last partition named 'nor_user', is a free MTD partition which uses the remaining space.
We align each partition size on max supported erase block size (512 Kbytes on NAND and 256 Kbytes on NOR).
To change the MTP partitioning on NOR and NAND Flash memories, update these configurations in your U-Boot defconfig as explained in U-Boot and in 'MTD partitions in U-Boot' or override this behavior in your board.
2.11.3. NOR MTD partition on ST board[edit source]
The default MTD partitions used on the ST boards for NOR boot is, when FIP is supported in U-Boot:
mtdparts SF: Detected mx66l51235l with page size 256 Bytes, erase size 64 KiB, total 64 MiB device nand0 <nand0>, # parts = 1 #: name size offset mask_flags 0: UBI 0x40000000 0x00000000 0 device nor0 <nor0>, # parts = 5 #: name size offset mask_flags 0: fsbl1 0x00040000 0x00000000 0 1: fsbl2 0x00040000 0x00040000 0 2: fip 0x00400000 0x00080000 0 3: u-boot-env 0x00080000 0x00480000 0 4: nor_user 0x03b00000 0x00500000 0 active partition: nand0,0 - (UBI) 0x40000000 @ 0x00000000 defaults: mtdids : nand0=nand0,nor0=nor0 mtdparts: mtdparts=nand0:-(UBI);nor0:256k(fsbl1),256k(fsbl2),4m(fip),512k(u-boot-env),-(nor_user)
This default partitioning is compatible for any for any NOR device, as we align each partition size on max supported erase block size on = 256 Kbytes.
2.11.4. NAND MTD partition on ST board[edit source]
The default MTD partitions used on the ST boards for NAND boot is, when FIP is supported in U-Boot:
mtdparts device nand0 <nand0>, # parts = 4 #: name size offset mask_flags 0: fsbl 0x00100000 0x00000000 0 1: fip1 0x00400000 0x00200000 0 2: fip2 0x00400000 0x00600000 0 3: UBI 0x3f700000 0x00a00000 0 active partition: nand0,0 - (fsbl1) 0x00100000 @ 0x00000000 defaults: mtdids : nand0=nand0 mtdparts: mtdparts=nand0:2048k(fsbl),4096k(fip1),4096k(fip2),-(UBI)
This default partitioning is compatible for any NAND device, as we align each partition size on max supported erase block size on NAND = 512 Kbytes.
3. Typical FlashLayout file with FIP[edit source]
This chapter describes the Layout file for the typical boot use cases based on STM32MP15_Flash_mapping when FIP is used.
Data are presented in tables for better readability despite the Layout file is plain text.
In the next examples, the STM32MP15 boot chain is used together with the following files:
- FSBL = TF-A with 2 different binary
- FSBL to boot with serial boot over usb support = tf-a-usb.stm32 (TF-A BL2 with STM32CubeProgrammer support, replaced by tf-a-uart.stm32 when uart is used)
- FSBL to program = tf-a-<dev>.stm32 (TF-A with boot from <dev> support, <dev> = emmc, sdcard, nand, nor)
- SSBL = fip.bin (including secure monitor from TF-A = SPMIN or form OP-TEE, U-Boot binary and device tree)
3.1. NOR Flash memory and SD card with FIP[edit source]
NOR Flash memory in RAW, containing the bootloaders. It uses two copies for FSBL (for failsafe update) and one copy for FIP.
SD card using GPT: several EXT4 partitions.
We align each partition on max supported erase block size of NOR 256 Kbytes, based on default MTD partition on NOR but the size of ENV partition can be optimized for NOR with lower erase block size.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip.bin |
P | 0x04 | fsbl1 | Binary | nor0 | 0x00000000 | tf-a-nor.stm32 |
P | 0x05 | fsbl2 | Binary | nor0 | 0x00040000 | tf-a-nor.stm32 |
P | 0x06 | fip | Binary | nor0 | 0x00080000 | fip.bin |
PED | 0x07 | env | Binary | nor0 | 0x00480000 | none |
PE | 0x08 | unused | Binary | nor0 | 0x00500000 | none |
P | 0x10 | bootfs | System | mmc0 | 0x00004400 | bootfs.ext4 |
P | 0x11 | vendorfs | FileSystem | mmc0 | 0x04004400 | vendorfs.ext4 |
P | 0x12 | rootfs | FileSystem | mmc0 | 0x05004400 | rootfs.ext4 |
P | 0x13 | userfs | FileSystem | mmc0 | 0x33A04400 | userfs.ext4 |
The PartId 0x07 is empty/deleted in nor0 ('PED' flag), the U-Boot environment is cleared.
The PartId 0x08 is an empty/free (user partition associated to 'nor_user' MTD partition in U-Boot ('PE' flag).
The 'System' partition 0x10 named "bootfs" is marked 'bootable'.
The partition 0x12 named "rootfs" has a specific PARTUUID.
3.2. NAND Flash memory with FIP[edit source]
The next example is compatible for any NAND device, as we align each partition size on max supported erase block size on NAND = 512 Kbytes.
We have, based on the default MTD partitions on NAND:
- 2 copy of fsbl (Binary(2)) in a MTD partition of 2MB, with at least 4 block of 512kB and 2 remaining spare block to skip potential bad blocks.
- 2 copies of FIP in 2 MTD partition of 4MB: fip1 and fip2; the remaining spare block to skip potential bad blocks depends of the size of the FIP file = fip.bin.
For parallel NAND, the MTD device is nand0:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip.bin |
P | 0x04 | fsbl | Binary(2) | nand0 | 0x000000 | tf-a-nand.stm32 |
P | 0x05 | fip1 | Binary | nand0 | 0x200000 | fip.bin |
P | 0x06 | fip2 | Binary | nand0 | 0x600000 | fip.bin |
P | 0x10 | UBI | FileSystem | nand0 | 0xA00000 | ubi.bin |
For serial NAND, the MTD device is spi-nand0:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip.bin |
P | 0x04 | fsbl | Binary(2) | spi-nand0 | 0x000000 | tf-a-spi-nand.stm32 |
P | 0x05 | fip1 | Binary | spi-nand0 | 0x200000 | fip.bin |
P | 0x06 | fip2 | Binary | spi-nand0 | 0x600000 | fip.bin |
P | 0x10 | UBI | FileSystem | spi-nand0 | 0xA00000 | ubi.bin |
This partitioning can be optimized for NAND with erase block size lower than 512kB.
Nota: If you increase the number of copie of FIP, you need to update the MTD parttion in U-Boot.
3.3. e•MMC with FIP[edit source]
TF-A is copied in the two boot area partitions of e•MMC (hidden partition) for failsafe update.
The GPT partitioning is used on the user area. U-Boot starts just after the GPT header at 17-Kbyte offset.
The other partitions are pre-populated with ext4 partition.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip.bin |
P | 0x04 | fsbl1 | Binary | mmc1 | boot1 | tf-a-emmc.stm32 |
P | 0x05 | fsbl2 | Binary | mmc1 | boot2 | tf-a-emmc.stm32 |
PD | 0x06 | fip | Binary | mmc1 | 0x00080000 | fip.bin |
P | 0x10 | bootfs | System | mmc1 | 0x00480000 | bootfs.ext4 |
P | 0x11 | vendorfs | FileSytem | mmc1 | 0x04480000 | vendorfs.ext4 |
P | 0x12 | rootfs | FileSytem | mmc1 | 0x05480000 | rootfs.ext4 |
P | 0x13 | userfs | FileSytem | mmc1 | 0x33E80000 | userfs.ext4 |
The partition 0x6 fip is erased before update with option D to clean the U-Boot environment located at the end of this partition.
The 'System' partition named "bootfs" is marked 'bootable'.
The partition named "rootfs" has a specific PARTUUID.
3.4. SD card with FIP[edit source]
RAW partition: two TF-A partitions (for fail safe update), then U-Boot. The GPT partitioning is used so fsbl1 starts just after the GPT header at 17-Kbyte offset.
The other partitions are pre-populated with ext4 partition.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip.bin |
P | 0x04 | fsbl1 | Binary | mmc0 | 0x00004400 | tf-a-sdcard.stm32 |
P | 0x05 | fsbl2 | Binary | mmc0 | 0x00044400 | tf-a-sdcard.stm32 |
PD | 0x06 | fip | Binary | mmc0 | 0x00084400 | fip.bin |
P | 0x10 | bootfs | System | mmc0 | 0x00484400 | bootfs.ext4 |
P | 0x11 | vendorfs | FileSytem | mmc0 | 0x04484400 | vendorfs.ext4 |
P | 0x12 | rootfs | FileSytem | mmc0 | 0x05484400 | rootfs.ext4 |
P | 0x13 | userfs | FileSytem | mmc0 | 0x33E84400 | userfs.ext4 |
The partition 0x6 named "fip" is erased before update with option D to clean the U-Boot environment located at the end of this partition.
The 'System' partition named "bootfs" is marked 'bootable'.
The partition named "rootfs" has a specific PARTUUID.
4. Typical FlashLayout file without FIP[edit source]
The STM32 image header for SSBL is supported in ecosystem release ≤ v2.1.0 or if you activate CONFIG_STM32MP15x_STM32IMAGE in your U-Boot defconfig for ecosystem release v3.0.0 (this temporary option is only introduced to facilitate the FIP migration but it will be removed in the next Ecosystem release).
4.1. Typical FlashLayout file[edit source]
This chapter describes the Layout file for the typical boot use cases based on STM32MP15_Flash_mapping when TEE is not used and associated partitions are absent (teeh, teed and teex).
Data are presented in tables for better readability despite the Layout file is plain text.
In the next examples, the STM32MP15 boot chain is used together with the following files:
- FSBL = TF-A, with 2 different binary as by default TF-A as no STM32CubeProgrammer support
- FSBL to boot = tf-a-serialboot.stm32 (TF-A with STM32CubeProgrammer support)
- FSBL to program = tf-a.stm32 (TF-A without OP-TEE support)
- SSBL = u-boot.stm32
4.1.1. NOR Flash memory and SD card[edit source]
NOR Flash memory in RAW, containing the bootloaders. It uses two copies for FSBL (for failsafe update) and one copy for SSBL.
SD card using GPT: several user EXT4 partitions.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl | Binary | none | 0x0 | tf-a-serialboot.stm32 |
P | 0x02 | fsbl1 | Binary | nor0 | 0x0 | tf-a.stm32 |
P | 0x04 | fsbl2 | Binary | nor0 | 0x40000 | tf-a.stm32 |
P | 0x03 | ssbl | Binary | nor0 | 0x80000 | u-boot.stm32 |
PED | 0x20 | env | Binary | nor0 | 0x280000 | none |
PE | 0x21 | unused | Binary | nor0 | 0x300000 | none |
P | 0x10 | bootfs | System | mmc0 | 0x00004400 | bootfs.ext4 |
P | 0x11 | vendorfs | FileSystem | mmc0 | 0x04284400 | vendorfs.ext4 |
P | 0x12 | rootfs | FileSystem | mmc0 | 0x05284400 | rootfs.ext4 |
P | 0x13 | userfs | FileSystem | mmc0 | 0x35284400 | userfs.ext4 |
The PartId 0x20 is empty/deleted in nor0, the U-Boot environment is cleared.
The PartId 0x21 is an empty/free user partition associated to 'nor_user' MTD partition in U-Boot
The 'System' partition named "bootfs" is marked 'bootable'.
The partition named "rootfs" has a specific PARTUUID.
4.1.2. NAND Flash memory[edit source]
BootLoader using RAW and then U-Boot environment and file system in UBI volume.
FSBL (TF-A) uses two RAW copies to avoid NAND Flash memory disturbances inside one partition.
SSBL (U-Boot) uses two copies in two RAW partitions to avoid NAND Flash memory disturbances inside one partition.
One MTD partition for UBI with several volumes: uboot_config, uboot_config_r, rootfs, vendorfs, and userfs.
For parallel NAND, the MTD device is nand0:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl | Binary | none | 0x0 | tf-a-serialboot.stm32 |
P | 0x02 | fsbl | Binary(2) | nand0 | 0x0 | tf-a.stm32 |
P | 0x03 | ssbl1 | Binary | nand0 | 0x200000 | u-boot.stm32 |
P | 0x04 | ssbl2 | Binary | nand0 | 0x400000 | u-boot.stm32 |
P | 0x10 | UBI | FileSystem | nand0 | 0x600000 | ubi.bin |
For serial NAND, the MTD device is spi-nand0:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl | Binary | none | 0x0 | tf-a-serialboot.stm32 |
P | 0x02 | fsbl | Binary(2) | spi-nand0 | 0x0 | tf-a.stm32 |
P | 0x03 | ssbl1 | Binary | spi-nand0 | 0x200000 | u-boot.stm32 |
P | 0x04 | ssbl2 | Binary | spi-nand0 | 0x400000 | u-boot.stm32 |
P | 0x10 | UBI | FileSystem | spi-nand0 | 0x600000 | ubi.bin |
4.1.3. e•MMC[edit source]
TF-A is copied in the two boot area partitions of e•MMC (hidden partition).
The GPT partitioning is used on the user area. U-Boot starts just after the GPT header at 17-Kbyte offset.
The other partitions are pre-populated with ext4 partition.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl | Binary | none | 0x0 | tf-a-serialboot.stm32 |
P | 0x02 | fsbl1 | Binary | mmc1 | boot1 | tf-a.stm32 |
P | 0x04 | fsbl2 | Binary | mmc1 | boot2 | tf-a.stm32 |
PD | 0x03 | ssbl | Binary | mmc1 | 0x00080000 | u-boot.stm32 |
P | 0x10 | bootfs | System | mmc1 | 0x00280000 | bootfs.ext4 |
P | 0x11 | vendorfs | FileSytem | mmc1 | 0x04280000 | vendorfs.ext4 |
P | 0x12 | rootfs | FileSytem | mmc1 | 0x05280000 | rootfs.ext4 |
P | 0x13 | userfs | FileSytem | mmc1 | 0x35280000 | userfs.ext4 |
The partition 0x3 U-Boot is erased before update with option D to clean the U-Boot environment located at the end of this partition.
The 'System' partition named "bootfs" is marked 'bootable'.
The partition named "rootfs" has a specific PARTUUID.
4.1.4. SD card[edit source]
RAW partition: two TF-A partitions, then U-Boot. The GPT partitioning is used so fsbl1 starts just after the GPT header at 17-Kbyte offset.
The other partitions are pre-populated with ext4 partition.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl | Binary | none | 0x0 | tf-a-serialboot.stm32 |
P | 0x02 | fsbl1 | Binary | mmc0 | 0x4400 | tf-a.stm32 |
P | 0x04 | fsbl2 | Binary | mmc0 | 0x00044400 | tf-a.stm32 |
PD | 0x03 | ssbl | Binary | mmc0 | 0x00084400 | u-boot.stm32 |
P | 0x10 | bootfs | System | mmc0 | 0x00284400 | bootfs.ext4 |
P | 0x11 | vendorfs | FileSytem | mmc0 | 0x04284400 | vendorfs.ext4 |
P | 0x12 | rootfs | FileSytem | mmc0 | 0x05284400 | rootfs.ext4 |
P | 0x13 | userfs | FileSytem | mmc0 | 0x35284400 | userfs.ext4 |
The partition 0x3 U-Boot is erased before update with option D to clean the U-Boot environment located at the end of this partition.
The 'System' partition named "bootfs" is marked 'bootable'.
The partition named "rootfs" has a specific PARTUUID.
4.2. Typical FlashLayout file with TEE without FIP[edit source]
This chapter describes the Layout file with TEE partitions for the trusted typical boot use case based on STM32MP15_Flash_mapping.
Since TF-A binary for OPTEE does not support STM32CubeProgrammer, two different FSBL binaries are used:
- FSBL to boot = tf-a-serialboot.stm32 (TF-A with STM32CubeProgrammer support)
- FSBL to program= tf-a-optee.stm32(TF-A with OP-TEE support)
4.2.1. NOR Flash memory and SD card with TEE[edit source]
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl | Binary | none | 0x0 | tf-a-serialboot.stm32 |
P | 0x02 | fsbl1 | Binary | nor0 | 0x0 | tf-a-optee.stm32 |
P | 0x04 | fsbl2 | Binary | nor0 | 0x40000 | tf-a-optee.stm32 |
P | 0x03 | ssbl | Binary | nor0 | 0x80000 | u-boot.stm32 |
PED | 0x20 | env | Binary | nor0 | 0x280000 | none |
P | 0x05 | teeh | Binary | nor0 | 0x00300000 | tee-header.stm32 |
P | 0x06 | teed | Binary | nor0 | 0x00340000 | tee-pageable.stm32 |
P | 0x07 | teex | Binary | nor0 | 0x00380000 | tee-pager.stm32 |
PE | 0x21 | unused | Binary | nor0 | 0x400000 | none |
P | 0x10 | bootfs | System | mmc0 | 0x00004400 | bootfs.ext4 |
P | 0x11 | vendorfs | FileSystem | mmc0 | 0x04284400 | vendorfs.ext4 |
P | 0x12 | rootfs | FileSystem | mmc0 | 0x05284400 | rootfs.ext4 |
P | 0x13 | userfs | FileSystem | mmc0 | 0x35284400 | userfs.ext4 |
4.2.2. NAND Flash memory with TEE[edit source]
WARNING: the 'tee' partitions are not duplicated in the next example, possible reliability issue with NAND disturbance.
For parallel NAND, the MTD device is nand0:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl | Binary | none | 0x0 | tf-a-serialboot.stm32 |
P | 0x02 | fsbl1 | Binary(2) | nand0 | 0x0 | tf-a-optee.stm32 |
P | 0x03 | ssbl1 | Binary | nand0 | 0x200000 | u-boot.stm32 |
P | 0x04 | ssbl2 | Binary | nand0 | 0x400000 | u-boot.stm32 |
P | 0x05 | teeh | Binary | nand0 | 0x600000 | tee-header.stm32 |
P | 0x06 | teed | Binary | nand0 | 0x680000 | tee-pageable.stm32 |
P | 0x07 | teex | Binary | nand0 | 0x700000 | tee-pager.stm32 |
P | 0x10 | UBI | FileSystem | nand0 | 0x780000 | ubi.bin |
For serial NAND, the MTD device is spi-nand0:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl | Binary | none | 0x0 | tf-a-serialboot.stm32 |
P | 0x02 | fsbl1 | Binary(2) | spi-nand0 | 0x0 | tf-a-optee.stm32 |
P | 0x03 | ssbl1 | Binary | spi-nand0 | 0x200000 | u-boot.stm32 |
P | 0x04 | ssbl2 | Binary | spi-nand0 | 0x400000 | u-boot.stm32 |
P | 0x05 | teeh | Binary | spi-nand0 | 0x600000 | tee-header.stm32 |
P | 0x06 | teed | Binary | spi-nand0 | 0x680000 | tee-pageable.stm32 |
P | 0x07 | teex | Binary | spi-nand0 | 0x700000 | tee-pager.stm32 |
P | 0x10 | UBI | FileSystem | spi-nand0 | 0x780000 | ubi.bin |
4.2.3. e•MMC with TEE[edit source]
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl | Binary | none | 0x0 | tf-a-serialboot.stm32 |
P | 0x02 | fsbl1 | Binary | mmc1 | boot1 | tf-a-optee.stm32 |
P | 0x04 | fsbl2 | Binary | mmc1 | boot2 | tf-a-optee.stm32 |
PD | 0x03 | ssbl | Binary | mmc1 | 0x00080000 | u-boot.stm32 |
P | 0x05 | teeh | Binary | mmc1 | 0x00280000 | tee-header.stm32 |
P | 0x06 | teed | Binary | mmc1 | 0x00300000 | tee-pageable.stm32 |
P | 0x07 | teex | Binary | mmc1 | 0x00380000 | tee-pager.stm32 |
P | 0x10 | bootfs | System | mmc1 | 0x00400000 | bootfs.ext4.stm32 |
P | 0x11 | vendorfs | FileSytem | mmc1 | 0x04400000 | vendorfs.ext4 |
P | 0x12 | rootfs | FileSytem | mmc1 | 0x05400000 | rootfs.ext4 |
P | 0x13 | userfs | FileSytem | mmc1 | 0x35400000 | userfs.ext4 |
4.2.4. SD card with TEE[edit source]
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl | Binary | none | 0x0 | tf-a-serialboot.stm32 |
P | 0x02 | fsbl1 | Binary | mmc0 | 0x4400 | tf-a-optee.stm32 |
P | 0x04 | fsbl2 | Binary | mmc0 | 0x00044400 | tf-a-optee.stm32 |
PD | 0x03 | ssbl | Binary | mmc0 | 0x00084400 | u-boot.stm32 |
P | 0x05 | teeh | Binary | mmc0 | 0x00284400 | tee-header.stm32 |
P | 0x06 | teed | Binary | mmc0 | 0x002C4400 | tee-pageable.stm32 |
P | 0x07 | teex | Binary | mmc0 | 0x00344400 | tee-pager.stm32 |
P | 0x10 | bootfs | System | mmc0 | 0x00384400 | bootfs.ext4 |
P | 0x11 | vendorfs | FileSytem | mmc0 | 0x04384400 | vendorfs.ext4 |
P | 0x12 | rootfs | FileSytem | mmc0 | 0x05384400 | rootfs.ext4 |
P | 0x13 | userfs | FileSytem | mmc0 | 0x35304400 | userfs.ext4 |
5. FlashLayout file to load and start U-Boot[edit source]
To be abble to load U-Boot with STM32CubeProgrammer, you can use this file:
For USB:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip.bin |
For UART:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-uart.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip.bin |
6. FlashLayout file to load and start kernel[edit source]
Load programming service with Device=none.
Load kernel uImage and device tree in DDR, Device=ram0.
This Linux kernel is started by a bootm command after the STM32CubeProgrammer detach command.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip.bin |
P | 0x10 | kernel | System | ram0 | 0xC2000000 | uImage.bin |
P | 0x11 | dtb | FileSytem | ram0 | 0xC4000000 | stm32mp157f-ev1.dtb |
7. Using provided FlashLayout files[edit source]
The binary and the associated pre-defined FlashLayout files are provided by ST in the Discovery kit.
For example, in STM32MP15 Discovery kits, you can find the distribution images as well as the file FlashLayout_sdcard_stm32mp157f-ev1-trusted.tsv:
#Opt Id Name Type IP Offset Binary - 0x01 fsbl-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157f-ev1-usb.stm32 - 0x03 fip-boot Binary none 0x0 fip/fip-stm32mp157f-ev1-trusted.bin P 0x04 fsbl1 Binary mmc0 0x00004400 arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32 P 0x05 fsbl2 Binary mmc0 0x00044400 arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32 PD 0x06 fip Binary mmc0 0x00084400 fip/fip-stm32mp157f-ev1-trusted.bin P 0x10 boot System mmc0 0x00484400 st-image-bootfs-openstlinux-weston-stm32mp1.ext4 P 0x11 vendorfs FileSystem mmc0 0x04484400 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4 P 0x12 rootfs FileSystem mmc0 0x05484400 st-image-weston-openstlinux-weston-stm32mp1.ext4 P 0x13 userfs FileSystem mmc0 0x33E84400 st-image-userfs-openstlinux-weston-stm32mp1.ext4
You can use these FlashLayout files as a starting point and simply modify them:
7.1. Updating partitions[edit source]
To update only some partitions, change the FlashLayout and only "select" the partitions that need to be updated:
Options field inside the FlashLayout is kept to P for partition(s) that need to be updated, others are changed to -.
Then execute STM32CubeProgrammer as before.
Example to update only U-Boot binary and st-image-bootfs filesystem :
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | arm-trusted-firmware/tf-a-stm32mp157f-ev1-usb.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip/fip-stm32mp157f-ev1-trusted.bin |
- | 0x04 | fsbl1 | Binary | mmc0 | 0x00004400 | arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32 |
- | 0x05 | fsbl2 | Binary | mmc0 | 0x00044400 | arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32 |
PD | 0x06 | ssbl | Binary | mmc0 | 0x00084400 | fip/fip-stm32mp157f-ev1-trusted.bin |
P | 0x10 | bootfs | System | mmc0 | 0x00484400 | st-image-bootfs-openstlinux-weston-stm32mp1.ext4 |
- | 0x11 | vendorfs | FileSystem | mmc0 | 0x04484400 | st-image-vendorfs-openstlinux-weston-stm32mp1.ext4 |
- | 0x12 | rootfs | FileSystem | mmc0 | 0x05484400 | st-image-core-openstlinux-weston-stm32mp1.ext4 |
- | 0x13 | userfs | FileSystem | mmc0 | 0x33E84400 | st-image-userfs-openstlinux-weston-stm32mp1.ext4 |
The associated text file becomes :
#Opt Id Name Type IP Offset Binary - 0x01 fsbl-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157f-ev1-usb.stm32 - 0x03 fip-boot Binary none 0x0 fip/fip-stm32mp157f-ev1-trusted.bin - 0x04 fsbl1 Binary mmc0 0x00004400 arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32 - 0x05 fsbl2 Binary mmc0 0x00044400 arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32 PD 0x06 fip Binary mmc0 0x00084400 fip/fip-stm32mp157f-ev1-trusted.bin P 0x10 boot System mmc0 0x00484400 st-image-bootfs-openstlinux-weston-stm32mp1.ext4 - 0x11 vendorfs FileSystem mmc0 0x04484400 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4 - 0x12 rootfs FileSystem mmc0 0x05484400 st-image-weston-openstlinux-weston-stm32mp1.ext4 - 0x13 userfs FileSystem mmc0 0x33E84400 st-image-userfs-openstlinux-weston-stm32mp1.ext4
7.2. Updating partitions using official ST bootloaders[edit source]
If TF-A or FIP are modified, and the STM32CubeProgrammer support is lost for any reason (for example if the stm32prog command is removed), you can still program these new files by selecting the correct binary setting for the partitions 0x01 and 0x03 with Device=none and change the Id for the binaries to program in Flash, as indicated in chapter "Field2: Id".
For example, with ST board, you can flash Customer-modified binary by using the ST original file. The new Layout file is:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | arm-trusted-firmware/tf-a-stm32mp157f-ev1-usb.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip/fip-stm32mp157f-ev1-trusted.bin |
P | 0x04 | fsbl1 | Binary | mmc0 | 0x00004400 | <customer-tf-a>.stm32 |
P | 0x05 | fsbl2 | Binary | mmc0 | 0x00044400 | <customer-tf-a>.stm32 |
PD | 0x06 | ssbl | Binary | mmc0 | 0x00084400 | <customer-fip>.bin |
P | 0x10 | bootfs | System | mmc0 | 0x00484400 | st-image-bootfs-openstlinux-weston-stm32mp1.ext4 |
P | 0x11 | vendorfs | FileSystem | mmc0 | 0x04484400 | st-image-vendorfs-openstlinux-weston-stm32mp1.ext4 |
P | 0x12 | rootfs | FileSystem | mmc0 | 0x05484400 | st-image-core-openstlinux-weston-stm32mp1.ext4 |
P | 0x13 | userfs | FileSystem | mmc0 | 0x33E84400 | st-image-userfs-openstlinux-weston-stm32mp1.ext4 |
The associated text file becomes :
#Opt Id Name Type IP Offset Binary - 0x01 fsbl-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157f-ev1-usb.stm32 - 0x03 fip-boot Binary none 0x0 fip/fip-stm32mp157f-ev1-trusted.bin P 0x04 fsbl1 Binary mmc0 0x00004400 customer-tf-a.stm32 P 0x05 fsbl2 Binary mmc0 0x00044400 customer-tf-a.stm32 PD 0x06 fip Binary mmc0 0x00084400 customer-fip.bin P 0x10 boot System mmc0 0x00484400 st-image-bootfs-openstlinux-weston-stm32mp1.ext4 P 0x11 vendorfs FileSystem mmc0 0x04484400 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4 P 0x12 rootfs FileSystem mmc0 0x05484400 st-image-weston-openstlinux-weston-stm32mp1.ext4 P 0x13 userfs FileSystem mmc0 0x33E84400 st-image-userfs-openstlinux-weston-stm32mp1.ext4
8. Other FlashLayout examples[edit source]
8.1. NOR and NAND Flash memories[edit source]
NOR Flash memory in RAW: TF-A uses several partitions for failsafe update, then FIP.
NAND Flash memory in UBI: only one large MTD partition for UBI volumes and UBIFS.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip.bin |
P | 0x04 | fsbl1 | Binary | nor0 | 0x000000 | tf-a.stm32 |
P | 0x05 | fsbl2 | Binary | nor0 | 0x040000 | tf-a.stm32 |
P | 0x06 | fip | Binary | nor0 | 0x080000 | fip.bin |
PED | 0x10 | env | Binary | nor0 | 0x480000 | none |
PE | 0x11 | unused | Binary | nor0 | 0x500000 | none |
P | 0x20 | UBI | FileSystem | nand0 | 0x00000000 | ubi.bin |
The PartId 0x11 is an empty/free user partition associated to 'nor_user' MTD partition in U-Boot.
8.2. NAND with SSBL in UBI[edit source]
FSBL (TF-A) uses two partitions (for failsafe update), with two copies in each partition .
FIP is present in a RAW volume of the UBI partition, loaded by FSBL.
The FIP binary is present in FlashLayout file to be loaded in RAM (Opt=-, Part=0x3, Device=none).
One MTD partition for UBI with several volumes: u-boot, uboot_config, uboot_config_r, rootfs, vendorfs, and userfs.
As it is not the ST default configuration, the MTD partitioning must be changed in U-Boot.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip.bin |
P | 0x04 | fsbl | Binary(2) | nand0 | 0x00000000 | tf-a-nand.stm32 |
P | 0x05 | fsbl | Binary(2) | nand0 | 0x00100000 | tf-a-nand.stm32 |
P | 0x10 | UBI | FileSystem | nand0 | 0x00200000 | ubi.bin |
Warning: UBI is not supported in TFA (tf-a-nand.stm32), it is only a example for FlashLayout.
8.3. SD card: FAT[edit source]
Below an example with FAT bootfs partition (kernel and RAMFS) and an empty userfs partition, deleted and formatted by Linux on first boot:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip.bin |
P | 0x04 | fsbl1 | Binary | mmc0 | 0x000000 | tf-a-sdcard.stm32 |
P | 0x05 | fsbl2 | Binary | mmc0 | 0x040000 | tf-a-sdcard.stm32 |
P | 0x06 | fip | Binary | mmc0 | 0x080000 | fip.bin |
P | 0x10 | bootfs | System | mmc0 | 0x200000 | bootfs.vfat |
PED | 0x11 | userfs | Empty | mmc0 | 0x400000 | none |
8.4. Load and program different binaries[edit source]
Same example, but with a specific fip file to boot (fip-boot.bin).
Userfs is empty but not deleted.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip-boot.bin |
P | 0x04 | fsbl1 | Binary | mmc0 | 0x040000 | tf-a-sdcard.stm32 |
P | 0x05 | fsbl2 | Binary | mmc0 | 0x000000 | tf-a-sdcard.stm32 |
P | 0x06 | fip | Binary | mmc0 | 0x080000 | fip.bin |
P | 0x10 | rootfs | System | mmc0 | 0x200000 | rootfs.vfat |
PE | 0x11 | userfs | FileSytem | mmc0 | 0x400000 | none |
8.5. RawImage[edit source]
The SD card content is exported as RAW device and updated with the image.sdcard file:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip.bin |
P | 0x10 | sdcard | RawImage | mmc0 | 0x0 | image.sdcard |
You can also erase the device before performing the update, by adding D in option.
8.6. Deleting device content[edit source]
For example, NOR and NAND Flash memories are deleted with:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | none | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | none | none | 0x0 | fip.bin |
PDE | 0x10 | nor | RawImage | nor0 | 0x0 | none |
PDE | 0x11 | nand | RawImage | nand0 | 0x0 | none |
To erase all other devices, including the e•MMC boot partition, proceed as follows:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip.bin |
PDE | 0x10 | sdcard | RawImage | mmc0 | 0x0 | none |
PED | 0x20 | emmc_boot1 | Binary | mmc1 | boot1 | none |
DPE | 0x21 | emmc_boot2 | Binary | mmc1 | boot2 | none |
EPD | 0x22 | emmc | RawImage | mmc1 | 0x0 | none |
DPE | 0x30 | nand | RawImage | nand0 | 0x0 | none |
PDE | 0x40 | nor | RawImage | nor0 | 0x0 | none |
Warning: A timeout may occur in STM32CubeProgrammer since deleting NOR Flash memory might be slow. To avoid this issue you can delete only the used partitions (Option=PED), for example:
#Opt Id Name Type Device Offset Binary
- 0x01 fsbl-boot Binary none 0x0 tf-a-usb.stm32
- 0x03 fip-boot Binary none 0x0 fip.bin
#delete ALL devices
EPD 0x10 sdcard RawImage mmc0 0x0 none
PED 0x20 emmc_b1 Binary mmc1 boot1 none
PED 0x21 emmc_b2 Binary mmc1 boot2 none
PED 0x22 emmc RawImage mmc1 0x0 none
PED 0x30 nand RawImage nand0 0x0 none
# on NOR (slow device): delete ALL used MTD partitions
PE 0x40 nor RawImage nor0 0x00000000 none
PED 0x41 fsbl1_nor Binary nor0 0x00000000 none
PED 0x42 fsbl2_nor Binary nor0 0x00040000 none
PED 0x43 fip_nor Binary nor0 0x00080000 none
PED 0x44 env_nor Binary nor0 0x00280000 none
PE 0x45 unused Binary nor0 0x002C0000 none
8.7. Complex use case[edit source]
Update SD card (mmc0 on SDMMC1). The GPT partition is created since all partitions are selected and Userfs is deleted and empty.
Erase all other devices, including e•MMC hidden boot partition.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | node | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip.bin |
P | 0x04 | fsbl1 | Binary | mmc0 | 0x00004400 | tf-a-sdcard.stm32 |
P | 0x05 | fsbl2 | Binary | mmc0 | 0x00044400 | tf-a-sdcard.stm32 |
P | 0x06 | fip | Binary | mmc0 | 0x00084400 | fip.bin |
P | 0x10 | bootfs | System | mmc0 | 0x00484400 | bootfs.stm32 |
P | 0x11 | rootfs | FileSytem | mmc0 | 0x08484400 | rootfs.ext4 |
DEP | 0x12 | userfs | FileSytem | mmc0 | 0x28484400 | none |
PED | 0x60 | emmc_boot1 | Binary | mmc1 | boot1 | none |
DPE | 0x61 | emmc_boot2 | Binary | mmc1 | boot2 | none |
EPD | 0x62 | emmc | RawImage | mmc1 | 0x0 | none |
EPD | 0x10 | nand | RawImage | nand0 | 0x0 | none |
9. Reference list[edit source]
- ↑ https://en.wikipedia.org/wiki/USB#Device_Firmware_Upgrade
- ↑ USB Device Class Specification for Device Firmware Upgrade, Version 1.1, (available at http://www.usb.org/developers/docs): https://www.usb.org/sites/default/files/DFU_1.1.pdf
- ↑ 3.0 3.1 https://en.wikipedia.org/wiki/GUID_Partition_Table
- ↑ 4.0 4.1 https://en.wikipedia.org/wiki/Universally_unique_identifier
- ↑ https://wiki.archlinux.org/index.php/persistent_block_device_naming