How to compile the device tree with the Developer Package

Revision as of 14:53, 28 June 2019 by Registered User

Template:ArticleMainWriter Template:ArticleFirstDraftVersion Template:ReviewersList


1. Purpose[edit source]

This article explains how to update boot chain (trusted mode) in case of use of a "customised" devicetree.
As exemple, CubeMX is able to generate "customised" devicetree.

This article describes how to update the DTB (devicetree compiled) part of the boot binaries.

Info white.png Information
Even if STMicroelectronics strongly recommends to use a Linux® environment, this article works in WSL2 (Windows Sub-system Linux 2) from Windows 10® (builds 2019 or later)

2. Rationale[edit source]

The rationale to not use the devicetree provided by OpenSTLinux distribution and prefer a "customised" devicetree is various;

  • You made your own board
  • You need to swap some IPs from MCU side to MPU side (or reverse)
  • For any other reason...

3. Pre-requisites[edit source]

This article only need to update three software of the complete boot chain (trusted mode); Trusted Firmware A (TF-A), u-boot and the Linux kernel.
Modifying those software need to handle :

  • need flashlayout and images to flash provided from file IMAGES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz
  • Need components sources and patches of the the software to update provided in file SOURCES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz
  • Need mkimage for stm32 and dtc utilities which could be provided by file SDK-x86_64-st-image-weston-openstlinux-weston-stm32mp1.tar.xz
  • Notice this is optional since 'dtc' and 'mkimage for stm32' could also be provided by your Linux distribution (as Ubuntu, even Ubuntu though WSL)
  • Host tools for binary manipulation : tar, patch, ssh/scp, dd and mount loop device
  • Those tools are very basic and available in any Linux distribution even on WSL.
  • In case of using WSL, mount loop device is only available from WSL2.


  • Custom devicetree sources:
  • For the rest of document the custom devicetree are considered generated by STM32CubeMX and stored in a tarball MyDeviceTree_fromCubeMX.tar.xz with following file tree:
MyDeviceTree_fromCubeMX
|-- kernel
|   |-- stm32mp157c-mydevicetree-mx.dts
|-- tf-a
|  |-- stm32mp15-mx.h
|  |-- stm32mp157c-mydevicetree-mx.dts
|-- u-boot
|  |-- stm32mp15-mx.h
|  |-- stm32mp157c-mydevicetree-mx-u-boot.dtsi
|  |-- stm32mp157c-mydevicetree-mx.dts

4. Prepare your environnement[edit source]

As seen in #Pre-requisites, there are numerus inputs so here a proposition to organize your environment.
Better is to create a dedicated WORKDIR somewhere in your HOME. Then copy all inputs quoted in #Pre-requisites in that just created WORKDIR:

cd
mkdir WORKDIR
cd WORKDIR
export WORKDIR="$PWD"
cp <IMAGES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz> $WORKDIR/
tar xf <IMAGES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz> -C $WORKDIR/
cp <SOURCES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz> $WORKDIR/
tar xf <SOURCES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz> -C $WORKDIR/
cp <MyDeviceTree_fromCubeMX.tar.xz> $WORKDIR/
tar xf <MyDeviceTree_fromCubeMX.tar.xz> -C $WORKDIR/
(optional) cp <SDK-x86_64-st-image-weston-openstlinux-weston-stm32mp1.tar.xz> $WORKDIR/
(optional) tar xf <SDK-x86_64-st-image-weston-openstlinux-weston-stm32mp1.tar.xz> -C $WORKDIR/

5. Kernel device tree update[edit source]

Updating the devicetree of kernel only needs to replace the 'dtb' file of '/boot' partition.
Indeed 'extlinux.conf' explicitly points on the dtb the kernel should use (something like '/boot/<devicetree>.dtb'). Below the procedure to generate and then copy new DTB in target:

5.1. Kernel : unpack and patch sources[edit source]

Run following command into a shell:

pushd $WORKDIR
mkdir -p kernel
tar xf st-image-weston-openstlinux-weston-stm32mp1/sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/linux-4.19.*.tar.xz -C kernel
mv kernel/linux-* kernel/kernel-sources/
pushd kernel/kernel-sources/
for p in $(ls -1 ../../st-image-weston-openstlinux-weston-stm32mp1/sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/*.patch); do patch -p1 < $p; done
popd
popd

5.2. Kernel : generate DTB[edit source]

pushd $WORKDIR
cp -r MyDeviceTree_fromCubeMX/kernel kernel/dts
ls kernel/dts/
stm32mp157c-mydevicetree-mx.dts
pushd $WORKDIR
gcc -E -nostdinc -I kernel-sources/include/ -I kernel-sources/arch/arm/boot/dts -I dts -undef -D__DTS__ -x assembler-with-cpp -o stm32mp157c-mydevicetree-mx.dts.tmp dts/stm32mp157c-mydevicetree-mx.dts
dtc -I dts -O dtb -o stm32mp157c-mydevicetree-mx.dtb stm32mp157c-mydevicetree-mx.dts.tmp
Template:Highlight3
popd
popd

5.3. Kernel : copy DTB on target/bootfs[edit source]

  • SCP method (require a up and running target with ssh service):
scp stm32mp157c-mydevicetree-mx.dtb root@<Target_IP>:/boot/
  • mount loop device method:
Under construction.png Coming soon

Then if needed [#update extlinux] of target according this new dtb filename. This is only needed if the filename of the dtb generated is diferent from the one used by extlinux to boot.


6. U-Boot device tree update[edit source]

Updating the devicetree of u-boot needs to replace the 'dtb'part of the u-boot binary.
Indeed u-boot binary is the "concatenation' of the 'dtb' and the 'u-boot' and then packaged with 'mkimage' for stm32.

Below the procedure to generate u-boot with a new DTB and then flash it on "u-boot" partition:

Warning white.png Warning
reminder: only trusted mode is supported

6.1. U-boot : unpack and patch sources[edit source]

pushd $WORKDIR
mkdir -p u-boot
tar xf st-image-weston-openstlinux-weston-stm32mp1/sources/arm-openstlinux_weston-linux-gnueabi/u-boot-stm32mp-*/v*.tar.gz -C u-boot
mv u-boot/u-boot* u-boot/u-boot-sources/
pushd u-boot/u-boot-sources
for p in $(ls -1 ../../st-image-weston-openstlinux-weston-stm32mp1/sources/arm-openstlinux_weston-linux-gnueabi/u-boot-stm32mp-*/*.patch); do patch -p1 < $p; done
popd

6.2. U-boot : generate DTB[edit source]

pushd $WORKDIR/u-boot
cp -r ../MyDeviceTree_fromCubeMX/u-boot dts
ls -1 dts
stm32mp157c-mydevicetree-mx.dts
stm32mp157c-mydevicetree-mx-u-boot.dtsi
stm32mp15-mx.h
## Need to include dtsi u-boot file into dts of u-boot
echo '#include "stm32mp157c-mydevicetree-mx-u-boot.dtsi"' >> dts/stm32mp157c-mydevicetree-mx.dts
gcc -E -nostdinc -I u-boot-sources/include/ -I u-boot-sources/arch/arm/dts -I dts -undef -D__DTS__ -x assembler-with-cpp -o stm32mp157c-mydevicetree-mx.dts.tmp dts/stm32mp157c-mydevicetree-mx.dts
dtc -I dts -O dtb -o u-boot.dtb stm32mp157c-mydevicetree-mx.dts.tmp
popd

6.3. U-boot : regenerate u-boot.stm32[edit source]

pushd $WORKDIR/u-boot
cat st-image-weston-openstlinux-weston-stm32mp1/sources/arm-openstlinux_weston-linux-gnueabi/u-boot-stm32mp-*/intermediate-binaries/trusted/u-boot-nodtb.bin u-boot.dtb > u-boot-dtb.bin
#464650
export SYS_TEXT_BASE=0xC0100000
mkimage -T stm32image -a $SYS_TEXT_BASE -e $SYS_TEXT_BASE -d u-boot-dtb.bin u-boot.stm32

6.4. U-boot : copy u-boot on target[edit source]

  • Because of 'extlinux' and before flashing the new u-boot.stm32, make sure the 'extlinux.conf' file, present in '/boot' and used for boot, has an entry ('LABEL') according the 'compatible' value in DTS file.

The 'compatible' value is at head of the DTS file. The compatible should looks like something as : "st,stm32mp157c-mydevicetree-mx"

  • For exemple if you are using a DK-2 board and booting on sdcard, then the extlinux.conf file is located in "/boot/mmc0_stm32mp157c-dk2_extlinux/".
    If "mmc0_<something>_extlinux" directory is not available, add an entry in "/boot/extlinux/extlinux.conf" file instead.
    If needed update 'DEFAULT' value also.
 menu title Select the boot mode
 MENU BACKGROUND ../splash.bmp
 TIMEOUT 20
 DEFAULT stm32mp157c-mydevicetree-mx
 LABEL stm32mp157c-dk2-sdcard
         KERNEL /uImage
         FDT /stm32mp157c-dk2.dtb
         APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200
 LABEL stm32mp157c-dk2-a7-examples-sdcard
         KERNEL /uImage
         FDT /stm32mp157c-dk2-a7-examples.dtb
         APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200
 LABEL stm32mp157c-dk2-m4-examples-sdcard
         KERNEL /uImage
         FDT /stm32mp157c-dk2-m4-examples.dtb
         APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200
 LABEL stm32mp157c-mydevicetree-mx
        KERNEL /uImage
        FDT /stm32mp157c-mydevicetree-mx.dtb
        APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200

At least 2 methods exist to update the "/boot" filesystem partition, please refer to #update bootfs chapter.

Warning white.png Warning
Do not forget to synchronize the file system before rebooting the target
sync

7. TF-A device tree update[edit source]

Updating the devicetree of TF-A needs to replace the 'dtb'part of the TF-A binary.
TF-A binary allocates just after the 'mkimage" headers a 'fixed' zone for DTB. DTB is smaller than the reserved zone, padding is done with zero.

Below the procedure to generate TF-A with a new DTB and then flash it on target:

7.1. TF-A : unpack and patch sources[edit source]

pushd $WORKDIR
mkdir -p tf-a
tar xf st-image-weston-openstlinux-weston-stm32mp1/sources/arm-openstlinux_weston-linux-gnueabi/tf-a-stm32mp-*/v*.tar.gz -C tf-a
mv tf-a/arm-trusted-firmware-* tf-a/tf-a-sources
pushd tf-a/tf-a-sources
for p in $(ls -1 ../../st-image-weston-openstlinux-weston-stm32mp1/sources/arm-openstlinux_weston-linux-gnueabi/tf-a-stm32mp-*/*.patch); do patch -p1 < $p; done
popd
popd

7.2. TF-A : generate DTB[edit source]

pushd $WORKDIR/tf-a
cp -r ../MyDeviceTree_fromCubeMX/tf-a dts
ls -1 dts/
stm32mp157c-mydevicetree-mx.dts
stm32mp15-mx.h
gcc -E -nostdinc -I tf-a-sources/include/ -I tf-a-sources/fdts -I dts -undef -D__DTS__ -x assembler-with-cpp -o stm32mp157c-mydevicetree-mx.dts.tmp dts/stm32mp157c-mydevicetree-mx.dts
dtc -I dts -O dtb -o tf-a.dtb stm32mp157c-mydevicetree-mx.dts.tmp
popd

7.3. TF-A : regenerate TF-A.stm32[edit source]

## OFFSET of DTB in tf-a.bin (fixed offset) : 0xBB00 (47872 in decimal)
## OFFSET of BL2 in tf-a.bin (fixed offset)  : 0x17B00 (97024 in decimal)
cp st-image-weston-openstlinux-weston-stm32mp1/sources/arm-openstlinux_weston-linux-gnueabi/tf-a-stm32mp-*/intermediate-binaries/trusted/tf-a-Template:LightBlue.bin tf-a.bin
# Delete dtb from tf-a.bin
dd conv=notrunc if=/dev/zero of=tf-a.bin bs=97024 count=1

# copy new dtb into tf-a.bin

dd conv=notrunc if=tf-a.dtb of=tf-a.bin seek=47872 obs=1

#464650 #464650

mkimage -T stm32image -a $SYS_TEXT_DATA -e $SYS_TEXT_BL2 -d tf-a.bin tf-a.stm32

7.4. TF-A : copy DTB on target/bootfs[edit source]