This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Template:ArticleMainWriter Template:ArticleFirstDraftVersion Template:ReviewersList
1. Purpose[edit source]
This article explains how to compile a device tree in a Windows® environment, and how to deploy the compiled devicetree.
2. Rationale[edit source]
STM32CubeMX can be used in both Linux® and Windows® environments.
The use of STM32MPU_Embedded_Software_distribution depends on a Linux® environment.
Nevertheless, the generation of a devicetree from STM32CubeMX and its compilation can be managed in a Windows® environment for some components.
3. Pre-requisites[edit source]
- Install a cross-compiler
- A cross compiler is needed to parse and prepare the devicetree (.dts) file.
- System Workbench for STM32 is recommended.
- The zip file with the gcc can be found at <INSTALL_DIR>\plugins\fr.ac6.mcu.externaltools.arm-none.win32_1.16.0.201807130628\tools
- mingw64 is also a good alternative.
- System Workbench for STM32 is recommended.
- A cross compiler is needed to parse and prepare the devicetree (.dts) file.
- Install a device tree compiler
- To install a community device tree compiler, please refer to Device Tree Compiler (MSYS2 version)
- Upon request, STMicroelectronics may provide an executable binary, without warranty nor support
4. Kernel device tree update[edit source]
- Get the Linux® source code
- Apply patches to the Linux® source code
- Create a workdir directory
- mkdir workdir
- Copy from source code of Linux the dt-bindings and dt files
- cp <KernelSources>/include/dt-bindinds workdir
- cp <KernelSources>/arch/arm/boot/dts/* workdir/
- Copy your dts into workdir
- cp <Your/dts/file.dts> workdir/
- Prepare dts
- cd workdir
- arm-none-eabi-gcc.exe -E -nostdinc -I . -undef -D__DTS__ -x assembler-with-cpp -o <yourDTS.dts>.tmp <yourDTS.dts>
- compile dts.tmp with dtc.exe
- dtc.exe -I dts -O dtb -o <DTBresult.dtb> <yourDTS.dts>.tmp