Arm CoreSight overview

Revision as of 15:59, 7 January 2021 by Registered User

1. Article purpose[edit source]

The purpose of this article is to give information about the Arm® CoreSight hardware subsystem.
It explains what are the principle peripherals of this subsystem.

2. Peripheral overview[edit source]

Arm® CoreSight products include a wide range of trace macrocells for Arm® processors, system and software instrumentation and a comprehensive set of IP blocks to enable the debug & trace of the most complex, multi-core SoCs. Arm® has defined an open CoreSight architecture to allow SoC designers to add debug & trace capabilities for other IP cores in to the CoreSight infrastructure.

Alternate text
CoreSight overview

2.1. Components description[edit source]

The debug features are based on Arm® CoreSight™ components:
• SWJ-DP: JTAG/Serial-wire debug port
• AXI-AP: AXI access port
AHB-AP: AHB access port
APB-AP: APB access port
ITM: Instrumentation Trace Macrocell
• DWT: Data Watchpoint and Trace
ETM: Embedded Trace Macrocell
• ETF: Embedded Trace FIFO
• TPIU: Trace Port Interface Unit
• SWO: Serial Wire Output
• CTI: Cross Trigger Interface
• CTM: Cross Trigger Matrix
• TSGEN: Timestamp Generator
STM: System Trace Macrocell
More information about these components can be found in the Arm® website [1]

2.2. Features[edit source]

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are really implemented.

3. References[edit source]