ETM internal peripheral

Revision as of 11:00, 7 January 2021 by Registered User

1. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the ETM peripheral and its main features
  • indicate the level of security supported by this hardware block
  • explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
  • explain, when necessary, how to configure the ETM peripheral.

2. Peripheral overview[edit source]

The ETM peripheral is used to log the Cortex-A7 execution trace into the embedded trace FIFO (ETF). Once in the ETF buffer, the trace can directly be dumped from the Cortex®-A7 or to the trace port interface unit (TPIU), connected to an external probe able to decode it.
This peripheral has two instances, one for each Cortex®-A7 core.

2.1. Features[edit source]

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are really implemented.

2.2. Security support[edit source]

The ETM is a non secure peripheral.

3. Peripheral usage and associated software[edit source]

3.1. Boot time[edit source]

The ETM can be used to debug the boot sequence using external probe.

3.2. Runtime[edit source]

3.2.1. Overview[edit source]

The ETM can be used to debug the run time application using external probe .

3.2.2. Software frameworks[edit source]

There is no software dedicated to the ETM internal peripheral delivered with STM32MPU ecosystem. Nevertheless, the ETM trace can be captured using an external probe.

3.2.3. Peripheral configuration[edit source]

Configuration of the ETM is done via JTAG scripts. Those scripts must be built by user thanks to STM32MP15 reference manuals .

3.2.4. Peripheral assignment[edit source]

Internal peripherals assignment table template

| rowspan="2" | Trace & Debug
| rowspan="2" | ETM
| ETM0
| 
| 
|
|
|-
| ETM1
| 
| 
| 
|
|-


|}

4. References[edit source]