This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. STM32CubeMX 6.11.0 - MPU support[edit source]
1.1. Features already supported in previous releases[edit source]
- Support of STM32CubeMP13 package running on the Arm® Cortex®-A7 processor.
- Support of STM32CubeMP15 package running on the Arm® Cortex®-A7 and Arm® Cortex®-M4 processors.
- Support of STM32CubeMP15 ecosystem release running on the Arm® Cortex®-A7 and Arm® Cortex®-M4 processors.
- Support for Azure RTOS ThreadX, FileX, LevelX, NETX and USBX, for STM32CubeMP13 package release
1.2. Main changes coming with new release[edit source]
- STM32MP135x A/C CPU max frequency was wrongly set to 900 MHZ instead of 650 MHZ.
- CLK_RTC_LSE not generated in TF-A DT (default configuration)
1.3. Known limitations[edit source]
1.3.1. With STM32CubeMP13 package[edit source]
- Only STM32CubeIDE is supported
- Only application context is supported
- Standard version of LevelX, USBX, NetX middlewares integrated without STM32MP13 platform specific patches.
- When using the STM32CubeMP13 package and activating Azure® RTOS ThreadX, the STM32CubeIDE linker file must contain the following section to avoid compilation issues:
.stack :
{
_stack_bottom = ABSOLUTE(.) ;
/* Allocate room for stack. This must be big enough for the
IRQ, FIQ, and SYS stack if nested interrupts are
enabled.*/
. = ALIGN(8) ;
. += 32768 ;
_sp = . - 16 ;
_stack_top = ABSOLUTE(.) ;
} >RAM
_end = .;
2. How to get STM32CubeMX[edit source]
STM32CubeMX for Linux®, Windows® and macOS ® | ||
---|---|---|
Download |
Version 6.11.0
| |
Installation guide |
| |
User manual |
| |
Detailed release note |
|
Minor releases may be available from the update site.