STM32CubeMX release note

Revision as of 17:57, 8 August 2023 by Registered User
Applicable for STM32MP13x lines, STM32MP15x lines

1. STM32CubeMX 6.9.0 - MPU support[edit source]

Main updates

  • The bundled JRE™ is Adoptium® Temurin™ 17.0.6 and JavaFX-17.0.2

Main fixes

  • 155060 - [STM32CubeMX] [RCC] PLL2R initialization not generated in device tree.
  • 141444 - Keep ST boards compatibility in DT when selecting a project from Board selector
  • 136275 - [DTGen] SocAllIPs IOCs do not compile due to missing driver in OSTL


Version 6.9.0
  • Download the all-in-one Windows installer from st.com
    • Windows Installer - STM32CubeIDE-Mac
STM32CubeMX for Linux®, Windows® and macOS ®
Download

Version 6.9.0

  • Download the preferred all-in-one Linux installer from st.com
    • Generic Linux Installer - STM32CubeMX-Lin
    • Windows Installer - SSTM32CubeMX-Win
    • MacOs Installer - STM32CubeMX-Mac
Installation guide
  • Refer to STM32CubeMX installation guide (UM1718) available on st.com.
User manual
  • When the installation is completed, see additional information about STM32CubeMX in st.com:
    • STM32CubeMX quick start guide (UM1718)
Detailed release note
  • Details about the content of this tool version are available in the STM32CubeMX release v6.9.0 release note from st.com

Minor releases may be available from the update site.