TIM device tree configuration

Revision as of 11:49, 25 January 2021 by Registered User
Warning white.png Warning
This section has NOT been yet updated/tested for/with the STM32 MPU ecosystem-v5.
Information provided in this section may not be fully applicable for v5 and you may need to proceed to some adaptations.
We apologize for this inconvenient.

1. Article purpose[edit source]

The purpose of this article is to explain how to configure the timer (TIM)[1] when the peripheral is assigned to Linux® OS:

  • Configuring the timer peripheral to enable PWM, trigger or quadrature encoder.
  • Configuring the board, e.g. TIM pins.

The configuration is performed using the device tree mechanism[2].

It is used by the TIM Linux driver that registers relevant information in PWM and IIO frameworks.

If the peripheral is assigned to another execution context, refer to How to assign an internal peripheral to a runtime context article for guidelines on peripheral assignment and configuration.


2. DT bindings documentation[edit source]

The TIM internal peripheral[1] is a multifunction device (MFD).

Each function is represented by a separate compatible string:

  • st,stm32-timers deals with core resources. (e.g. registers, clock, DMAs)
  • st,stm32-pwm deals with PWM resources. (e.g. PWM input/output pins)
  • st,stm32-timer-trigger deals with other internal peripheral triggering.
  • st,stm32-timer-counter deals with quadrature encoder resources and external events counter.
  • st,stm32-timer-timer deals with clock sources.

The required and optional configuration properties of these function are documented in STM32 TIM MFD device tree bindings[3]

3. DT configuration[edit source]

This hardware description is a combination of both STM32 microprocessor and board device tree files. Refer to Device tree for more explanations about device tree file split.

The STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.

3.1. DT configuration (STM32 level)[edit source]

TIM nodes are declared in stm32mp151.dtsi[4].

DT root node (e.g. timers1...) and DT child nodes describe the TIM features such as:

  • PWM
  • trigger and quadrature encoder

They also describe hardware parameters such as registers address, clock and DMA.

timers1: timer@address {
	/* timer common resources */
	compatible = "st,stm32-timers";
	...
	pwm {
		/* PWM*/
		compatible = "st,stm32-pwm";
	};
	timer@0 {
		/* trigger and quadrature encoder */
		compatible = "st,stm32h7-timer-trigger";
		/* trigger identifier (e.g. 0 for TIM1 triggers, 1 for TIM2... */
		reg = <0>;
	};
};
Warning white.png Warning
This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.

3.2. DT configuration (board level)[edit source]

This part is used to configure and enable the TIM hardware used on the board:

  • Enabling DT root node for the TIM instances in use (e.g timers1...) by setting status = "okay";
  • Enabling DT child node(s) for the feature(s) in use (PWM input/output, trigger and quadrature encoder) by setting status = "okay";
  • Configuring pins in use via pinctrl through pinctrl-0, pinctrl-1 and pinctrl-names.

To enable PWM capture on the board (optional), DMA must be configured:

  • Enable DMA channel(s) corresponding to the PWM input(s) by setting dmas = <...>, <...>; and matching dma-names = "ch1", "ch3";.

When PWM capture isn't used, it's recommended to disable DMA channels by default, to spare them for other usage:

  • Disable DMA channels by setting /delete-property/dmas and /delete-property/dma-names

3.3. DT configuration examples[edit source]

3.3.1. TIM configured in PWM mode[edit source]

The example below shows how to configure TIM1 channel 1 to act as:

/* select TIM1_CH1 alternate function 1 on 'PE9' */
pwm1_pins_a: pwm1-0 {
	pins {
		pinmux = <STM32_PINMUX('E', 9, AF1)>;
		bias-pull-down;
		drive-push-pull;
		slew-rate = <0>;
	};
};

/* configure 'PE9' as analog input in low-power mode */
pwm1_sleep_pins_a: pwm1-sleep-0 {
	pins {
		pinmux = <STM32_PINMUX('E', 9, ANALOG)>;
	};
};
Info white.png Information
The PWM output doesn't require any DMA channel. Disable them if they are configured by default in the .dtsi file.
/* PWM DT provider on TIM1: "pwm1" */
&timers1 {
	status = "okay";
	/* spare all DMA channels since they are not needed for PWM output */
	/delete-property/dmas;
	/delete-property/dma-names;
	/* define pwm1 label */
	pwm1: pwm {
		/* configure PWM pins on TIM1_CH1 */
		pinctrl-0 = <&pwm1_pins_a>;
		pinctrl-1 = <&pwm1_sleep_pins_a>;
		pinctrl-names = "default", "sleep";
		/* enable PWM on TIM1 */
		status = "okay";
	};
};
  • PWM DT user example
Info white.png Information
The TIM PWM DT user specifier encodes 3 cells:
  • PWM number (0 for CH1, 1 for CH2 and so on)
  • PWM period in nanoseconds
  • PWM polarity (0 for normal polarity or PWM_POLARITY_INVERTED)
/ {
	...
	/* PWM DT user on TIM1_CH1: "pwm1", example with "pwm-leds"[5] */
	pwmleds {
		compatible = "pwm-leds";
		example {
			label = "stm32-pwm-leds-example";
			/* Use pwm1 channel 0 (e.g. TIM1_CH1) */
			/* period in nanoseconds (500000), normal polarity (0) */
			pwms = <&pwm1 0 500000 0>;
			max-brightness = <127>;
		};
	};
};

3.3.2. TIM configured in PWM mode and trigger source[edit source]

The example below shows how to configure TIM1 channel 1 to act as:

/* select TIM1_CH1 alternate function 1 on 'PE9' */
pwm1_pins_a: pwm1-0 {
	pins {
		pinmux = <STM32_PINMUX('E', 9, AF1)>;
		bias-pull-down;
		drive-push-pull;
		slew-rate = <0>;
	};
};

/* configure 'PE9' as analog input in low-power mode */
pwm1_sleep_pins_a: pwm1-sleep-0 {
	pins {
		pinmux = <STM32_PINMUX('E', 9, ANALOG)>;
	};
};
Info white.png Information
The PWM output doesn't require any DMA channel. Disable them if they are configured by default in the .dtsi file.
&timers1 {
	status = "okay";
	/* spare all DMA channels since they are not needed for PWM output */
	/delete-property/dmas;
	/delete-property/dma-names;
	pwm {
		/* configure PWM on TIM1_CH1 */
		pinctrl-0 = <&pwm1_pins_a>;          
		pinctrl-1 = <&pwm1_sleep_pins_a>;
		pinctrl-names = "default", "sleep";
		/* enable PWM on TIM1 */
		status = "okay";
	};
	timer@0 {
		/* enable trigger on TIM1 */
		status = "okay";
	};
};

3.3.3. TIM configured in PWM input capture mode[edit source]

The example below shows how to configure TIM1 channel 1 in PWM input capture mode (e.g. period and duty cycle):

/* select TIM1_CH1 alternate function 1 on 'PE9' */
pwm1_in_pins_a: pwm1-in-0 {
	pins {
		pinmux = <STM32_PINMUX('E', 9, AF1)>;
		bias-disable;
	};
};

/* configure 'PE9' as analog input in low-power mode */
pwm1_in_sleep_pins_a: pwm1-in-sleep-0 {
	pins {
		pinmux = <STM32_PINMUX('E', 9, ANALOG)>;
	};
};

A DMA channel is required and must be configured depending on the PWM input channel:

  • Select DMA channel 1, "ch1", to capture PWM input channel 1 and/or 2
  • Select DMA channel 3, "ch3", to capture PWM input channel 3 and/or 4
  • Select both "ch1" and "ch3" dmas to enable capture on all PWM input channels
&timers1 {
	status = "okay";
	/* Enable DMA "ch1" for PWM input on TIM1_CH1 */
	dmas = <&dmamux1 11 0x400 0x5>;
	dma-names = "ch1";
	pwm {
		/* configure PWM input pins, e.g. TIM1_CH1 */
		pinctrl-0 = <&pwm1_in_pins_a>;
		pinctrl-1 = <&pwm1_in_sleep_pins_a>;
		pinctrl-names = "default", "sleep";
		/* enable PWM on TIM1 */
		status = "okay";
	};
};
Info white.png Information
DMA channels 1 and/or 3 for each TIM can be picked from the "dmas" list in stm32mp151.dtsi[4] file

3.3.4. TIM configured as quadrature encoder interface[edit source]

The example below shows how to configure TIM1 to interface with a quadrature encoder:

tim1_in_pins_a: tim1-in-pins-0 {
	pins {
		pinmux = <STM32_PINMUX('E', 9, AF1)>, /* TIM1_CH1 */
			 <STM32_PINMUX('J', 11, AF1)>; /* TIM1_CH2 */
		bias-disable;
	};
};

tim1_in_pins_sleep_a: tim1-in-pins-sleep-0 {
	pins {
		pinmux = <STM32_PINMUX('E', 9, ANALOG)>, /* TIM1_CH1 */
			 <STM32_PINMUX('J', 11, ANALOG)>; /* TIM1_CH2 */
	};
};
&timers1 {
	status = "okay";
	/delete-property/dmas;                       /* spare all DMA channels since they are not required for quadrature encoder interface */
	/delete-property/dma-names;
	timer@0 {
		pinctrl-0 = <&tim1_in_pins_a>;       /* configure TIM1_CH1 and TIM1_CH2 as encoder input pins */
		pinctrl-1 = <&tim1_in_pins_sleep_a>;
		pinctrl-names = "default", "sleep";
		status = "okay";                     /* enable Encoder interface mode on TIM1 */
	};
};

4. How to configure the DT using STM32CubeMX[edit source]

The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.

5. References[edit source]

Please refer to the following links for additional information: