Hardware components

This category groups together all articles and subcategories related to the hardware components used on the STM32 MPU boards, and for which additional software information is needed.

An internal peripheral (a.k.a. hardware block ) is embedded inside a STM32 MPU microprocessor device, whereas a hardware component is outside the microprocessor, but delivered with an STM32 MPU board. It is either soldered on a STM32 MPU board (e.g. the Cirrus cs42l51 audio codec for the STM32MP157x_DKx Discovery kits), or plugged into a STM32MPU board via a hardware port (such as the OmniVision OV5640 camera sensor for the STM32MP157C-EV1 Evaluation board).

A hardware component is natively managed by the STM32MPU Embedded Software distributions.

Hardware components




Subcategories

This category has the following 6 subcategories, out of 6 total.

Attachments

Discussions