STiRoT for STM32G5

STiRoT stands for ST immutable (unchangeable) Root of Trust. This is a ROM code developed by STMicroelectronics that targets a SESIP Level-3-certified implementation. Because STiRoT requires hardware cryptographic features, it is only available on the following product lines.

A detailed description of STiRoT is provided in AN6523.

List of applicable products:

Type Products
Microcontroller STM32G564xx

1. STiRoT services

STiRoT provides two services:

  • The Secure Boot (root of trust services) is an immutable code that is always executed after a system reset. First, it activates runtime protections, then it verifies the authenticity and integrity of the application code and data before every execution.
  • The Secure Firmware Update application is an immutable code that detects whether a new application code or data image is available. First, it verifies the authenticity of the code or data, then it checks the integrity of the new image before installing it after decryption.

2. STiRoT activation

STiRoT is activated in two different use cases:

  • One boot stage: STiRoT directly manages the user application, as illustrated in the schematic below.

  • Two boot stages: STiRoT manages an updatable boot stage (OEMuRoT), which manages the user application, as illustrated in the schematic below. The updatable boot stage can be personalized to customer needs.

Refer to AN6523 for more details on the STiRoT activation use cases.

Examples on how to start with STiRoT are provided in the section Getting started with STM32G5 security articles.

3. STiRoT configuration

The STiRoT configuration provides mainly the possibility to:

  • Define the user flash memory mapping: select the location and the size of each area.
  • Configure the authentication and encryption keys.
  • Activate the optional management of a data image.
  • Allow the jump in the bootloader (external access) when no valid image is installed.

Refer to AN6523 to get the exhaustive list of all configuration parameters.

The product provisioning to activate and configure STiRoT is done following the three steps below when executing provisioning.py script:

  1. STiRoT configuration. At this stage, the number of managed images (firmware image only, or firmware and data images), the location of the images, and the cryptographic keys are defined.
  2. Image generation. Two types of images are generated:
    • initial image: Image in clear to be programmed in installation area during initial device programming.
    • update image: Encrypted image to be programmed in download area. Will be installed during secure firmware update process.
  3. Programming the option bytes, OBKeys, and image(s) in the device.

These three stages are illustrated in the figure below. Security:Security STIROT Provisioning.png

Information
The entire provisioning process is managed through a provisioning script that guides the user step-by-step. For more information, refer to Getting started with STM32G5 security articles

Refer to AN6523 for more details on the STiRoT provisioning process, including OBkey configuration files and image generation.