Introduction to external serial memories (XSPI) interoperability for STM32


The purpose of this article is to:

  • Give an overview of the external memory
  • Briefly introduce the QuadSPI, OctoSPI, HSPI and XSPI controllers integrated within the STM32 microcontrollers (MCUs).
  • Explain how to configure the peripheral
  • List all the available resources to help users get started

1. Acronyms and definitions

Term Definition
DTR Double data rate
HSPI Hexadeca Serial Peripheral Interface
OCTOSPI Octal Serial Peripheral Interface
OCTOSPIM OCTOSPI IO manager
QUADSPI Quad Serial Peripheral Interface
SDR Single data rate
XSPI Extended Serial Peripheral Interface
XSPIM XSPI IO manager

2. What is External Memory?

As application complexity increases, driven by the demand for richer, more intuitive graphical user interfaces (GUIs) and human-machine interfaces (HMIs), as well as advanced processing capabilities such as big data and artificial intelligence (AI), the limited on-chip memory of microcontroller units (MCUs) often becomes a bottleneck. Moreover, the need for additional storage to support future firmware upgrades further increases these memory requirements.

To address these challenges, External Memory serves as a practical solution to expand storage capacity beyond the constraints of on-chip memory, thereby enhancing overall system performance and enabling more sophisticated applications.

Types of External Memory

External memory can be broadly categorized into:

  • Non-Volatile External Memory

Used primarily for storing persistent graphical data assets such as bitmaps, fonts, language translations, and application code (e.g., TouchGFx). This memory retains data even when power is removed.

  • Volatile External Memory

Employed for temporary storage needs such as framebuffers and runtime code execution. This memory requires continuous power to maintain its contents.

To meet these demands, STMicroelectronics offers a range of MCUs that integrate advanced external serial memory controllers. These controllers enable seamless interfacing and communication with external memories. The controllers, including SDMMC, FMC, QUADSPI, OCTOSPI, HSPI, and XSPI, are designed to support various types of external memories, thereby addressing the limitations of on-chip memory, ensuring high data throughput, and providing greater flexibility for designers, particularly for new Flash-less MCUs.

The diagram below provides a brief overview of the external memories.

Caption

This article aims to provide essential documentation on key interfaces—QuadSPI, OctoSPI, HSPI, and XSPI—offering a brief overview and helpful resources to help users start their applications without extensive searching.

3. QuadSPI, OctoSPI, HSPI and XSPI overview

The Quad Serial Peripheral Interface (QUADSPI) is the first interface introduced by STMicroelectronics in the STM32F4 series that allows communication on up to four data lines between the STM32 and an external serial memory. This interface supports single, dual, and quad-SPI memories.

The Octal Serial Peripheral Interface (OCTOSPI) was first introduced in the STM32L4 series to further enhance the QSPI interface by using eight data lines between the STM32 and an external serial memory allowing to interface with octo-SPI memories. This interface supports single, dual, quad-SPI, and octo-SPI memories.

The Hexadeca Serial Peripheral Interface (HSPI), introduced in the STM32U5 series for STM32U59x/5Ax and STM32U5Fx/5Gx devices, extends to 16 I/O data lines the memory interface and can operate up to 160 MHz. In this mode, only the data phase uses a 16-bit line width, while the command and address phases use an 8-bit line width.

The Extended Serial Peripheral Interface (XSPI), introduced in the STM32H7RS series, also employs 16 I/O data lines and can operate up to 200 MHz. This interface is designed to support a wide range of external memory types, ensuring optimal performances and scalability for complex applications. It supports single, dual, quad-SPI, octo-SPI, and 16-bit memories.

Caption

Refer to the product datasheet and reference manual to see which interface is implemented and the available pins.

Information
Some STM32 MCUs are equipped with dual instances of OCTOSPI or XSPI, necessitating the use of an arbiter known as the IO manager (OCTOSPIM or XSPIM). This low-level peripheral facilitates efficient pin assignment for OCTOSPI/XSPI by leveraging a comprehensive I/O matrix (prior to alternate function mapping). It also enables the multiplexing of single, dual, quad, octal, and 16-bit SPI interfaces over a shared bus.

Supported Features

These interfaces integrated into STM32 MCUs offer several key features. Below are the main features:

  • OCTOSPI, HSPI, and XSPI are designed to support JESD251C, HyperBus™ and Xccela™ protocols
  • Operating modes: indirect, automatic status-polling, and memory-mapped
    • Indirect mode: In this mode all the operation are performed using the controller registers to preset commands, addresses, data, and transfer parameters
    • Automatic status-polling mode: In this mode the external memory status is periodically read, and an interrupt on a matching flag can be generated in case of flag setting. This mode is used only in regular-command protocol, and it depends on whether the external memory supports it (useful for checking the end of the erase or the end of programming)
    • Memory mapped-mode: In this mode the external memory device is seen by the system as it was an internal memory, only 256Mbytes can be addressed
  • Support eXecute In Place (XIP)
  • SDR (Single Data Rate) and DTR (Double Transfer Rate) support
  • Data strobe support
  • Integrated FIFO for reception and transmission
  • 8-, 16-, and 32-bit data accesses allowed
  • DMA protocol support
  • Interrupt generation on FIFO threshold, timeout, operation complete, and access error
  • Supports the following protocols with associated frame formats, allowing compatibility with almost all memory available on the market
  1. The regular-command frame is the classical frame format where the peripheral communicates with the external memory device by using commands; each command can include the following phases and, at least, one of the five phases must be present.
    • Instruction phase
    • Address phase
    • Alternate-byte phase
    • Dummy-cycle phase
    • Data Phase
  2. The HyperBus™ frame format to support HyperRAM™ and HyperFlash™ memories. The HyperBus frame composed of two phases:
    • Command/adddess phase (CA)
    • Data phase

On the command/address phase, the HyperRam/HyperFlash memory will use the read-recovery time (RWDS) to check if an additional initial access latency has to be inserted. Two modes are available on HyperBus protocol:

  • HyperBus memory mode: This mode allows the read/write access from/to HyperBus memory
  • HyperBus register mode: This mode allows to access the memory device register space
Warning

The data strobe feature is not supported by the QUADSPI peripheral.

HyperBus protocol is not available for QUADSPI controller since HyperBus is using 8-bit or 16-bit data mode.

For a complete list of features refer to the STM32 products reference manuals.

Supported memories

Information
These memory controllers are compatible with a range of memory providers, such as Macronix, APMemory, Infineon, Winbond, and ISSI. Thanks to the regular-command frame format flexibility and to the HyperBus protocol. Below is a brief list of memory components that have been tested with STM32 products implementing these peripherals. Nevertheless, users are recommended to verify whether or not the specific memory part chosen for their custom application meets all the criteria and requirements of these interfaces to ensure compatibility and optimal performance.
  1. The STM32L4Rxxx and STM32L4Sxxx series do not support PSRAM.
STM32 Product Vendor Memory reference Voltage (V) Standard
STM32 with QSPI interface Quad-SPI
Micron MT25QL128A 3 -
NUMONIX N25Q256A 2.7-3.6 -
Macronix MX25L5124G 2.7-3.6 -
Infineon S25FS128SIFI000 1.8 -
STM32L4(1)

STM32L5

STM32H7

STM32U5

STM32H5

STM32U3

STM32C5

Octo-SPI
Flash
Macronix MX25UM51245G 1.8 OCTABUS
Macronix MX25LMS51245G 3-3.3 OCTABUS
Infineon S71KL512SC0BHI00 3 Hyper COMBO FLASH/RAM (HyperBus)
RAM
APmemory APS6408L-3OBM-BA 2.7-3.6 Xccela
ISSI IS66WVH8M8BLL-100B1LI 3 HyperRAM(HyperBus)
Winbond W955D8MBYA 1.7-1.95 HyperRAM(HyperBus)
STM32U59x/5Ax

STM32U5Fx/5Gx

HSPI
APmemory APS256XXN-OBR-BG 1.62-1.98 Xccela
Winbond W958D6NBMA 1.7-2.0 HyperRAM(HyperBus)
STM32H7R/S

STM32N6

XSPI
Macronix MX66UW1G45GXDI00 1.8 OCTABUS(NorFlash:Support read while write feature)
APmemory APS256XXN-OBR-BG 1.62-1.98 Xccela
Information
We highly recommend reviewing the datasheet's section on QUAD/OCTOSPI/HSPI/XSPI interface characterization to ascertain the maximum speed of each interface and the corresponding test conditions.

4. Configuring peripherals

Before any data can be transferred to or from the external memory, the peripheral needs to be configured. This configuration can be accomplished using the STM32CubeMX graphical tool, with additional manual adjustment if needed.

The configuration steps are generally similar for all peripherals, but there is specific difference for the OCTOSPI, HSPI, and XSPI peripherals compared to the QSPI.

Configuration steps

Once The STM32CubeMX is created, the user must follow the steps below:

1. Select Pinout and Configuration tab, under connectivity, select the available peripheral on your desired product 2. Select the memory mode you wish to use, the mode depends on the memory and its communication protocol

Caption

3. Depending on the selected instance select and configure the pins as shown in the figure below. Ensure that the pins used are dedicated for the serial external serial memory controller. Refer to the product datasheet for more details

Caption

Make sure that the output speed is set to "Very high" for all the GPIOs.

Caption

4. Configure the system and the external serial memory controller clock 5. Once all the GPIOs and the clock configuration have been done, the user must configure the controller parameter, these parameters depend on the used memory and its communication protocol

Caption

For more details about this step, users can refer to section 7.2.4 'OCTOSPI Configuration and Parameter Settings' of AN5050 or to the following FAQ

Information
Refer to the following application notes for a detailed description of the operation and configuration of these controllers:

Quad-SPI interface on STM32 microcontrollers and microprocessors: AN4760

Getting started with Octo-SPI, Hexadeca-SPI, and XSPI interfaces on STM32 MCUs: AN5050

Warning
We recommend consulting the product Errata-sheet to be aware of all relevant usage notes and known bugs with these interfaces and others. The Errata-sheet can be found in the technical documentation section of the product.

5. Security

With the ability to store code/data and perform Over-The-Air (OTA) updates comes the need to protect code and firmware with robust security measures. Ideally, data should be secured where it resides, not just within the processor. Storing code in external memory introduces the necessity to secure the memory interface as well.

To address this, STMicroelectronics is proactively tackling this security challenge by integrating advanced security peripherals when interfacing with external serial memories, such as the OTFDEC and MCE engines.

  • The OTFDEC (On-The-Fly Decryption): designed to decrypt encrypted of the Arm® AXI or AHB traffic based on the read request address information.
  • The Memory Cipher Engine (MCE): designed to provide encryption and decryption services for data stored in internal or external memory.

For more details about these two features and how they can be used by these interfaces, refer to the following application notes:

How to use OTFDEC for encryption/decryption in trusted environment on STM32H7Bxxx and STM32H73xx microcontrollers OTFDEC

How to use MCE for encryption/decryption on STM32 MCUs MCE

Check the STM32 product datasheets to find out the availably of these peripherals.

6. Recommended PCB Routing Guidelines for External Memory

The speed at which these interfaces operate depends on several factors, including the board layout and pad speeds. With a good layout, it is possible to achieve maximum speeds. Therefore, the layout should be optimized to ensure the best performance. For detailed guidance, refer to the application note "Getting started with STM32H7Rx/7Sx MCUs hardware development" AN5935 available on the STMicroelectronics website, specifically section "10.4.3 Extended-SPI interface (XSPI)".

Please note that each product from STMicroelectronics comes with its specific "Getting Started" guide to help you with the hardware development process.

7. STMicroelectronics resources

ST provides drivers and middleware, along with extensive examples, to help users understand these controllers and quickly start their applications.

Caption

Below is a list of the available resources and their links:

  • Applications note:

AN4760 Quad-SPI interface on STM32 microcontrollers and microprocessors
AN5050 Getting started with Octo-SPI, Hexadeca-SPI, and XSPI Interface on STM32 MCU

  • Examples

Preconfigured examples for supported MCUs are available to help users get started quickly. These examples can be found under:

STM32Cube_FW_xx\Projects\STM32xxx\Examples\

These examples describe how to use:

  • Write and read data in memory-mapped mode in the OCTOSPI HyperRAM memory
  • Execute code from NOR/PSRAM memory after code loading
  • NOR/PSRAM memory in memory-mapped mode
  • NOR/PSRAM memory in DMA mode
  • Middleware

Middleware components are provided to streamline the integration and usage of these peripherals in various application. One such component is the External Loader. This middleware facilitates the programming, erasing, and reading of external memory devices without changing the internal flash memory.

ST provides examples loaders for:

  • Macronix QuadSPI/OctoSPI NOR Flash​
  • Micron NOR Flash ​

External loader examples can be found following this link: Github

For more detailed about the External loader users can refer to the following application note and wiki pages introducing new middleware appearing on the STM32H7RS series to ease the use of external serial NOR memories: Introduction to external memory manager and external memory loader middleware for boot flash MCU AN6101

https://wiki.st.com/stm32mcu/wiki/Introduction_to_External_memory_Manager

https://wiki.st.com/stm32mcu/wiki/Introduction_to_External_memory_Loader

Getting started with External memory Manager and External memory loader


  • Drivers

Based on the selected MCU, users can refer to available resources provided in the STM32Cube Firmware package. Drivers and BSP component drivers can be found under:

STM32Cube_FW_xx\Drivers\STM32xxxx_HAL_Driver
STM32Cube_FW_xx\Drivers\BSP\Components

ST provides drivers examples for: