This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article describes the setup used to measure the power consumption of H.264 encode use cases.
These measurements have been done using STM32N6570-DK (version C01) and STLINK-V3PWR.
1. Using external SMPS
1.1. Board rework
Current injection using I_SENS_EXT before the external SMPS (3.3 V)
Remove R23, R24, and C27.
Note: The efficiency of the SMPS must be considered when measuring power.
For instance: TPS62088: Efficiency is approximately 85% (for DK version C01)
1.2. STLINK-V3PWR connection