STM32WBA Bluetooth® LE hardware setup

Click here for Bluetooth® LE overview.

1. STM32WBA boards

1.1. NUCLEO-WBA55CG Nucleo-WBA65RI boards

NUCLEO-WBA55CG[1] and NUCLEO-WBA65RI [2] are a Bluetooth® Low Energy wireless and ultra-low-power board embedding a powerful and ultra-low-power radio compliant with the Bluetooth® Low Energy SIG specification v5.4, IEEE 802.15.4-2015 PHY and MAC, supporting Thread®, Matter®, and Zigbee®.

Called the Ultra-low-power wireless STM32WBA series microcontroller based on the Arm® Cortex®‑M33 core, featuring:

  • 1 Mbyte of flash memory and 128 Kbytes of SRAM in a UFQFPN48 package for NUCLEO-WBA55CG
  • 2 Mbytes of flash memory and 512 Kbytes of SRAM in a VFQFPN68 package for NUCLEO-WBA65RI

The NUCLEO-WBA55CG and NUCLEO-WBA65RI are composed of:

  • MCU RF board (MB1803 and MB2130, respectively):
    • 2.4 GHz RF transceiver supporting Bluetooth® specification v5.4
    • IEEE 802.15.4-2015 PHY and MAC, supporting Thread®, Matter®, and Zigbee®
    • Arm® Cortex® M33 CPU with TrustZone®, MPU, DSP, and FPU
    • Integrated PCB antenna
  • Mezzanine Board (MB1801)
    • Three user LEDs
    • Three user and one reset push button
    • Board connectors:
      • USB Type-C®
      • ARDUINO® Uno V3 expansion connector
      • ST morpho headers for full access to all STM32 I/Os
    • Flexible power-supply options: ST-LINK USB VBUS or external sources
    • On-board STLINK-V3 debugger/programmer with USB reenumeration capability: mass storage, virtual COM port, and debug port
    • Comprehensive free software libraries and examples available with the STM32CubeWBA MCU Package[3]
    • Support of a wide choice of integrated development environments (IDEs) including IAR Embedded Workbench®, MDK-ARM, and STM32CubeIDE
NUCLEO-WBA55CG NUCLEO-WBA65RI
Connectivity:Connectivity Nucleo WBA55CG.png

1.2. STM32WBA55G-DK1 & STM32WBA65I-DK1 boards

The STM32WBA55G-DK1 and STM32WBA65I-DK1 are complete demonstration and development platform for the STM32WBA55CG and STM32WBA65CG microcontrollers, featuring an Arm® Cortex®‑M33 core with Arm® TrustZone® and mainline security extension.

Called the Ultra-low-power wireless STM32WBA series microcontroller based on the Arm® Cortex®‑M33 core, featuring:

  • 1 Mbyte of flash memory and 128 Kbytes of SRAM in a UFQFPN48 package for STM32WBA55G-DK1
  • 2 Mbytes of flash memory and 512 Kbytes of SRAM in a VFQFPN68 package for STM32WBA65I-DK1


The STM32WBA55G-DK1 and STM32WBA65I-DK1 are composed of:

  • MCU RF board (MB1803 and MB2130, respectively):
    • 2.4 GHz RF transceiver supporting Bluetooth® specification v5.4
    • Bluetooth® Low Energy specification supporting LE audio
    • Arm® Cortex® M33 CPU with TrustZone®, MPU, DSP, and FPU
    • Integrated PCB antenna
  • Mezzanine Board (MB1802)
    • One digital microphone
    • OLED display
    • One user LED
    • User joystick with 4-direction control and selector button
    • One reset push button
    • Board connectors:
      • USB Type-C®
      • One jack socket with stereo line input and one jack socket with stereo output and microphone input
      • Battery
      • Grove
      • MIPI10
      • Tag‑Connect™ 10‑pin footprint
      • ARDUINO® Uno V3 expansion connector
      • STMod+ expansion connector
    • Flexible power-supply options: ST-LINK USB VBUS or external sources
    • On-board STLINK-V3 debugger/programmer with USB reenumeration capability: mass storage, virtual COM port, and debug port
    • Comprehensive free software libraries and examples available with the STM32CubeWBA MCU Package[3]
    • Support of a wide choice of integrated development environments (IDEs) including IAR Embedded Workbench®, MDK-ARM, and STM32CubeIDE
STM32WBA55G-DK1 STM32WBA65I-DK1
Connectivity:STM32WBA55G-DK1.jpg

2. Hardware platform configuration

2.1. Debug log via UART interface

The NUCLEO-WBA55CG [1] embeds the ST-LINK/V3 in-circuit debugger and programmer for STM32 microcontrollers.
The STM32WBA microcontroller supports the STM32 virtual COM port driver for communication with a PC using a serial interface.

Use any convenient software terminal to open the serial communication port of the PC to check the messages from the board. Select the serial port and set up the connection as follows (example done with Tera Term software).

Set a new serial connection to the ST platform:

Tera Term setup (1/2)

Set up the serial connection as below:

Tera Term setup (2/2)

2.2. How to connect external debuggers

This paragraph explains how to connect an external debugger to the NUCLEO-WBA55CG[1] platform. This could be either an ST-LINK or a J-LINK debugger. To disconnect the embedded ST-LINK, set SW1 to position 3.

2.2.1. Setup using ST-LINK

  • On the miniboard, check if the CN3 is fitted with an STDC14 connector. Add one if not.
  • Place 47 Ohm resistors (type 0402) for R2-R9 (that is, eight components).
  • Remove the jumpers JP1 and JP2.
  • Connect the ST-LINK output OUT to connector JP2.2.
  • Connect ST-LINK GND to CN13.1.
  • Connect a ribbon between ST-LINK DEBUG and CN3.
ST-link debugger connected to a NUCLEO-WBA55CG[1] board

2.2.2. Setup using J-LINK

  • On the miniboard, check if the CN3 is fitted with an STDC14 connector. Add one if not.
  • Place 47 Ohm resistors (type 0402) for R2-R9 (that is, eight components).
  • Plug the JLINK 10-pin patch adapter into the J-LINK.
  • Connect a ribbon between this adapter and JP1 on the WBA5x miniboard.
Correspondence of pins from CN3 footprint to STDC14 or MIPI10 connector
J-Link debugger connected to NUCLEO-WBA55CG[1] board
The Segger patch adapter needs to be inserted between the J-Link and the NUCLEO-WBA55CG[1]

3. Going further

4. References