BLE smartphone applications

1. Bluetooth® LE collector applications for STM32WBA

The following table shows the different collector applications (Smartphone & webBluetooth) and the compatibility for each Bluetooth® LE STM32WBA project.

Collector applications and project compatibility
Smartphone applications / Projects
ST BLE Sensor
ST BLE ToolBox
Web Bluetooth®
BLE_Beacon ●
BLE_HealthThermometer ● ●
BLE_HeartRate ● ● ●
BLE_p2pServer ● ● ●
BLE_p2pRouter ● ●
BLE_DataThroughput ● ●
BLE_Fuota (Firmware Update Over The Air) ● ● ●
BLE_p2pServer_Ext ●
BLE_BloodPressure ● ●
BLE_ContinuousGlucoseMonitoring ● ●
BLE_RunningSpeedAndCadence ● ●
BLE_WeightScale ● ●
BLE_InsulinDelivery ●
BLE_GenericHealthSensor ● ●
BLE_HID-Keyboard ●
BLE_p2pServer_Simplest ● ●
BLE_Sensor ●
BLE_HR_P2PServer ● ● ●

2. Bluetooth® LE smartphone applications for STM32WB

The following table shows the different smartphone applications and the compatibility for each Bluetooth® LE STM32WB project.

Smartphone applications and project compatibility
Smartphone applications / Projects
ST BLE Sensor
ST BLE ToolBox
ST BLE Mesh
Web Bluetooth®
BLE_BloodPressure ●
BLE_HealthTermometer ●
BLE_HeartRate ● ● ●
BLE_Proximity ●
BLE_DataThroughput ● ●
BLE_Ota ● ● ●
BLE_p2pServer ● ● ●
BLE_p2pRouter ● ●
BLE_Peripheral_Lite ● ●
BLE_RfWithFlash ● ●
BLE_Sensor ● ● ●
BLE_MeshLightingLPN ●
BLE_MeshLightingPRFNode ●
BLE_MeshLightingProvisioner ●

3. Bluetooth® LE collector applications for STM32WB0

The following table shows the different collector applications (Smartphone) and the compatibility for each Bluetooth® LE STM32WB0 project.

Collector applications and project compatibility
Smartphone applications / Projects
ST BLE Sensor
ST BLE ToolBox
BLE_Beacon ●
BLE_HealthThermometer ●
BLE_HeartRate ● ●
BLE_HeartRate_ota ● ●
BLE_p2pServer ● ●
BLE_p2pServer_ota ● ●
BLE_p2pRouter ●
BLE_DataThroughput ●
BLE_p2pServer_Ext ●


4. ST BLE Toolbox

ST BLE Toolbox is a user-friendly application which interacts with and debugs ST Bluetooth®LE devices.
Upon launch, the app scans for Bluetooth®LE devices.
For each device found, it is possible to:

  • display advertisements
  • connect to it, showing all the peripheral services, characteristics and descriptors.

ST BLE Toolbox allows performing read/write and notification interaction with any Bluetooth characteristic from any device.

In addition, certain services (used in projects from the official STM32WB, STM32WBA and STM32WB0 packages) have a custom panel, allowing you to interact with the device in a more visual and user-friendly way.


List of application having a custom panel in ST BLE Toolbox for STM32WB and STM32WBA
BLE Application & Documentation Source Code
Heart Rate
BLE_HeartRate
Blood Pressure
BLE_BloodPressure
Health Thermometer
BLE_HealthThermometer
p2pServer
BLE_p2pServer
Firmware Update Over the Air
BLE_ApplicationInstallManager
p2pRouter
BLE_p2pRouter
Data Throughput
BLE_DataThroughput_Server
BLE_DataThroughput_Client
Continious Glucose Monitoring
BLE_ContinuousGlucoseMonitoring
Running Speed and Cadence
BLE_RunningSpeedAndCadence




List of application having a custom panel in ST BLE Toolbox for STM32WB0
BLE Application & Documentation Source Code
Heart Rate
BLE_HeartRate
Health Thermometer
BLE_HealthThermometer
p2pServer
BLE_p2pServer
Firmware Update Over the Air
BLE_ApplicationInstallManager
p2pRouter
BLE_p2pRouter
Data Throughput
BLE_DataThroughpu_Server
BLE_DataThroughput_Client





Glimpse of user-friendly application interfaces available with the STBLE Toolbox
Running Speed and Cadence Continuous Glucose Monitoring

Application store:

  • ST BLE Toolbox Android Application[1]
  • ST BLE Toolbox iOS Application[2]

More information is available on ST website :

  • ST BLE Toolbox Application[3]

4.1. Home Panel

Let's have a quick overview of the ST BLE Toolbox.
The main page is the Scan panel, where you can interact with BLE devices.

You can enable or disable the scan by clicking on this button
Use the radio buttons to sort the discovered devices
Choose to display only or exclude certain devices
Click on the star next to a device to add it to your list of favorite devices
Connect" button to start the connection with the BLE device
ST BLE Toolbox : Home Panel


4.2. Left Menu

To open the menu, you can either click on the menu icon or slide from left to right. The following functionalities are available in the menu, which we will detail below:

ST BLE Toolbox Left Menu
ScanFavoritesPhone Supported FeaturesRecognized Services and CharacteristicsLogsSettingsUseful Links


4.3. Favorites

This panel lists all of your favorite devices.

ST BLE Toolbox : Favorite Devices



4.4. Phone Supported Features

This panel allows you to know which functionalities are supported by your phone.

ST BLE Toolbox : Phone Supported Features



4.5. Recognized Services and Characteristics

This tab lists the services and characteristics recognized by the Bluetooth SIG, the Custom ST ones, as well as those added by the user.

ST BLE Toolbox : Recognized Services and Characteristics



4.6. Logs

The Logs tab displays the trace history. You can manage the capture of these traces and extract them by clicking on the share button.

ST BLE Toolbox : Logs



4.7. Settings

This panel allows you to configure your preferred parameters, track a connection with analytics, manage application logs, and customize the visual appearance of the ST BLE Toolbox application.

ST BLE Toolbox : Settings


4.8. Useful Links

This panel will display useful links such as the Wiki pages for developing and evolving through the STM32 BLE ecosystem.

ST BLE Toolbox : Useful Links


5. ST BLE Sensor

ST BLE Sensor application shows the data exported by a Bluetooth® LE device using the BlueST protocol. [4]
It is an interface between the smartphone application and the Bluetooth® Low Energy drivers that allows easy access to the data exported via BLE such as, inertial or environmental sensor data, battery information. The application show different panels based on the data types exported by the firmware, including:

  • environmental data
  • MEMS sensor fusion
  • BlueVoice, speech to text
  • node status
  • ...

The applications support as well dedicated features such as:

  • Fast firmware update over the air (FUOTA)
  • Bluetooth secure pairing with numeric comparison

In June 2023, this app has been split into two different apps:
- ST BLE Sensor Classic, supporting all legacy boards and demos (won't be updated anymore unless bugs have to be fixed)
- ST BLE Sensor, entirely re-written in a more modern language, supporting only recent boards and demos (regular updates with new boards and demos)

ST BLE sensor application illustration


Application store:

  • ST BLE Sensor Android Application[5]
  • ST BLE Sensor Classic Android Application[6]
  • ST BLE Sensor iOS Application[7]
  • ST BLE Sensor Classic iOS Application[8]

More information available on ST website:

  • ST BLE Sensor Application[9]

6. ST BLE Mesh

ST BLE Mesh application allows you to create your own Bluetooth® Mesh Profile compliant mobile Apps. The App can be used for provisioning, configuring and controlling multiple Bluetooth® Mesh Profile compliant devices in a Bluetooth®LE Mesh network for Internet of Things (IoT) solutions.
More information can be found on Getting Started document for Android[10] and iOS[11].

ST BLE Mesh application illustration


Application store:

  • ST BLE Mesh Android Application[12]
  • ST BLE Mesh iOS Application[13]

More information available on ST website :

  • ST BLE Mesh Application[14]

7. References