STM32WB Bluetooth® LE - STM32CubeMX Application Conception

Click here for Bluetooth® Low Energy Overview.

1. Introduction

STM32CubeMX tool is a graphical tool that helps you to generate a first application targeting the MCU of your choice, with initialization code based on the configuration you specify. In the tools interface, you can select the right MCU, configure pins, clocks, peripherals, middleware, and it generates code project based on your setup.

This wiki page defines how to generate a Bluetooth® Low Energy (BLE) server custom application for STM32WB55RG MCU using STM32CubeMX software.

2. Build a Bluetooth® Low Energy application on STM32WB with CubeMX

The STM32WB Nucleo board, flashed with the application generated by STM32CubeMX, can send data to a smartphone (using ST BLE ToolBox application), and receive commands from it through Bluetooth® Low Energy.

System presentation


This GATT Server application shall be able to expose two services:

  • First service exposes two characteristics
  • Second service exposes three characteristics

The first service (My_P2P_Server) looks like P2P Server (STM proprietary) with two characteristics:

  • Characteristic 1 has Write property
  • Characteristic 2 has Notify property

Writing to characteristic 1 toggles blue LED.
Pressing SW1 on Nucleo board send data to the phone

Custom Service



The following steps are recommended to build this application example:

Step 1: STM32CubeMX initialization for STM32WB55RGx
Initialize a CubeMX project targeting STM32WB55RGx platform.

Step 2: STM32WB IP configuration
Enable required system resources and peripherals to make BLE application to work.

Step 3: Clock configuration
Setup project clocks.

Step 4: Project Setup
Define project settings for C code generation as project name, IDE, Firmware location.

Step 5: Bluetooth® LE GAP/GATT Custom Application Configuration
Define BLE Application as Advertising parameters, Services and Characteristics.


Services and Characteristics configuration are given in the following table:

Service Long Name My_P2P_Server
Service Short Name My_P2P
UUID Type 128 bits
UUID 0xFE40
Characteristic Long Name My_LED_Char My_Switch_Char
Characteristic Short Name LED_C SWITCH_C
UUID Type 128 bits 128 bits
UUID 0xFE41 0xFE42
Char Properties Read + Write w/o response Notify
Char Permissions None None
Char GATT Events GATT_NOTIFY_ATTRIBUTE_WRITE GATT_NOTIFY_ATTRIBUTE_WRITE

3. Tools

3.1. Software tools

To make and use this project, the needed software tools to complete the application are:

  • STM32CubeMX[1] software (from v6.14.0)
  • STM32CubeWB MCU Package[2] (from v1.22.0)
  • IDE: STM32CubeIDE[3] or IAR[4]
  • Serial Terminal (TeraTerm[5])
  • Smartphone application ST BLE ToolBox

3.2. Hardware tools

A STM32WB Nucleo board and a micro-B to Type-A USB cable are also needed.

Hardware presentation


The PC is connected to the ST-LINK connector of the NUCLEO board (right connector from the top view).

ST-LINK connection


4. CubeMX initialization for P-NUCLEO-WB55

4.1. STM32CubeMX initial setup

Open STM32CubeMX and start a new project from the Access to MCU selector button

New Project Menu


Chose the MCU and then start the new project:

Check STM32WB in MCU/MPU Selector tab
Select the STM32WB55RG part number
Start the project
Project Interface


4.2. Pinout and IP configuration

To configure the system, enable all the required system resource and peripherals clicking on A->Z to display all IPs.

Pinout & configuration interface


BLE mode is reachable once the following system resources and peripherals are turned to enable.

  • HSEM :activated
  • IPCC : activated, ITs enabled
  • RCC : HSE and LSE on Crystal/Ceramic resonator
  • RTC : activate clock source and enable internal wakeup
  • RF : activate RF1
  • STM32WPAN : BLE
IP list

4.2.1. HSEM

The Hardware SEMaphore (HSEM) is needed to manage shared resources between the two CPU cores in the STM32WB.

Select HSEM
Activate it
HSEM activation

4.2.2. IPCC

Configuration of Inter-Processor Controller Communication (IPCC) is done as follows:

Select IPCC
Activate it
Go to NVIC Settings tab
Enable IPCC RX occupied interrupt
Enable IPCC TX free interrupt
IPCC activation & setup

4.2.3. RCC

On Reset and Clock Controller (RCC), High Speed clock (HSE) and Low Speed Clock (LSE) are mandatory for Bluetooth® LE radio.

Select RCC
Choose Crystal/Ceramic Resonator for HSE
Choose Crystal/Ceramic Resonator for LSE
RCC setup

4.2.4. RTC

Configuration of Real Time Counter (RTC) is done as follows:

Select RTC
Activate clock source
Set WakeUp as internal WakeUp
Go to NVIC Settings tab
Enable RTC wake up interrupt through EXTI line 19
RTC activation & setup

4.2.5. RF

Activate RF1:

Select RF
Activate RF1
RF activation

4.2.6. Enable BLE

Finally, under STM32_WPAN interface, check BLE box:

Select STM32_WPAN
Select BLE
Bluetooth® LE activation

4.3. Clock configuration

On clock configuration tab, run the automatic clock issue solver:


Then:

Set RTC/LCD Source MUX on LSE
Set System Clock MUX on HSE_SYS
Set RFWKP Clock MUX to LSE
Set SMPS Clock MUX to HSE
Set SMPS Div on /4
Clock configuration

4.4. Project manager

All the project configuration is done on the Project Manager pane within three sections, and done as follows :

4.4.1. Project

Configure the project
Define the project name
Chose the project location
Select the Toolchain IDE and version
Define linker settings
Use default FW location
Project configuration


4.4.2. Code generator

Manages files, packages and embedded software packs

Project generation


4.4.3. Advanced settings

Definition of drivers to use (HAL/LL) and generated function calls.

  • Uncheck Do Not Generate Function Call checkbox for APPE_Init
Advanced settings interface

5. BLE GAP/GATT Custom application configuration

Now, we can start configuring and defining the BLE middleware.

  • Bluetooth® LE Peripheral Custom Template GATT Server Application can be defined:
    • On STM32WB
    • With STM32CubeMX
  • GAP peripheral : advertising configuration
  • GATT server configuration:
    • five services maximum
    • five characteristics maximum per service
  • ACI commands:
    • AN5270: STM32WBx5 Bluetooth® Low Energy (BLE) wireless interface[6].

5.1. BLE applications and services

To start the definition of the Bluetooth® LE application :

Open Pinout & Configuration interface
Select STM32_WPAN
Go to BLE Application and Services tab
Enable Custom Template and disable Custom P2P Server


STM32_WPAN Interface: Application & Services Settings

5.2. Advertising configuration

Advertising parameters are defined under BLE Advertising tab:

  • advertising configuration data are located in app_conf.h and ble_conf.h files
  • advertising elements data are located in app_ble.c file
STM32_WPAN Interface: Bluetooth® LE Advertising tab


Open Advertising Configuration and set the CFG_GAP_DEVICE_NAME to something of your liking, for example MY_APPLI.

STM32_WPAN Interface: Bluetooth® LE Advertising configuration


In the generated code these parameters are defined in :
1. app_conf.h file:

  • #define ADV_TYPE
  • #define BLE_ADDR_TYPE
  • #define FILTER
  • #define CFG_GAP_DEVICE_NAME

2. ble_conf.h file:

  • #define BLE_CFG_PERIPHERAL
  • #define BLE_CFG_CENTRAL
STM32_WPAN Interface: Bluetooth® LE Advertising configuration (2)


In Advertising elements:

  • Turn to “yes” the elements to add in the advertising packet payload as described in the image below :
    - Tx power: AD_TYPE_TX_POWER_LEVEL
    - Complete local name: AD_TYPE_COMPLETE_LOCAL_NAME
    - 16 bits service UUID: AD_TYPE_16_BIT_SERV_UUID_CMPLT_LIST
    - Manufacturer specific data: AD_TYPE_MANUFACTURER_SPECIFIC_DATA
  • Set the value for the other elements as mentioned in the image below :
    - Complete Local name: AD_TYPE_COMPLETE_LOCAL_NAME = MyCST
    - Service 1 UUID: UUID 1 = 180D
STM32_WPAN Interface: Advertising elements


The advertising information is represented by advertising data elements, which are standardized on the Bluetooth SIG.
These elements are included in the advertising packet payload and are located in app_ble.c file (here the advertising packet structure’s length = 19 bytes).

Advertising elements: corresponding code


Warning
Pay attention to not oversize the ad_data[ ] length array.

This array size is automatically calculated by STM32CubeMX and can't exceed 28 bytes


5.3. Services and characteristics definition

All created services and characteristics are managed in custom_stm.c file. Each service and characteristic is added in SVCCTL_InitCustomSvc() function using:

  • aci_gatt_add_service(…) for services,
  • aci_gatt_add_char(…) for characteristics.

5.3.1. Services definition

Each created service is defined in a dedicated CubeMX tab:

  • Up to five characteristics per service
  • UUID type can be defined as 16 or 128 bits
  • UUID definition
  • Type value is primary or secondary service


A custom application can define up to five services.
In the following example, we define one service: My_P2P_Server.

You can set the number of services to define in the BLE GATT tab (present in STM32_WPAN interface):

Go to BLE GATT Tab,
Enter the number of services to define,
Enter the long and short names,
For each service, a tab with the given service long name is created.
Bluetooth® LE GATT services definition


For each defined service , set the number of characteristics and the service UUID value as defined in the following images .
two characteristics for My_P2P_Server service and service UUID is 0xFE40.

Bluetooth® LE GATT services definition


Information
If UUID type is 128 bits reduced, the UUID value (on 16 bits) is encapsulated in a 128 bits data thanks to COPY_xxx_UUID macro (where xxx is service or characteristic long name) to bring it in 128 bits.

For example an UUID of 0xFE41 is encapsulated as : 0x00,0x00,0xfe,0x41,0x8e,0x22,0x45,0x41,0x9d,0x4c,0x21,0xed,0xae,0x82,0xed,0x19.

If UUID type is 16bits, the UUID value is used as this to create the service or characteristic.

5.3.2. Characteristics definition

For each characteristic the following parameters must be defined

  • General
  • Properties
  • Permissions
  • GATT events

My_P2P_Server Characteristics:
My_P2P_Server service have 2 characteristics:

  • First characteristic:
    • Long name: My_LED_Char
    • Short name: LED_C
    • UUID type: 128 bits UUID(0x02)
    • UUID 128 input type: reduced
    • UUID: 0xFE41
    • Value length: 2
    • Length characteristic: Variable
    • Properties: CHAR_PROP_READ and CHAR_PROP_WRITE_WITHOUT_RESP
    • GATT events: only GATT_NOTIFY_ATTRIBUTE_WRITE
  • Second characteristic:
    • Long name: My_Switch_Char
    • Short name: SWITCH_C
    • UUID type: 128 bits UUID(0x02)
    • UUID 128 input type: reduced
    • UUID: 0xFE42
    • Value length: 2
    • Length characteristic: Variable
    • Properties: CHAR_PROP_NOTIFY
    • GATT events: only GATT_NOTIFY_ATTRIBUTE_WRITE

Defined as follows:

MY_P2P_Server characteristics definition


5.3.3. Pairing definition

Pairing is done to support secure connection method.
All pairing parameters defined in the BLE_Pairing tab are located in app_conf.h file.
When PAIRING_PARAMETERS is set to ON, pairing parameters are available on the interface and can be defined as follows:

Pairing definition


Once configuration is done in STM32CubeMX, the code can be generated by following the steps described inCode Generation chapter.
If you want to enable traces before generating the project, go to next chapter.
If you want to setup User button and LED, you can refer to P2P Server: Notifications and Writes management chapter.

6. Enable traces

6.1. USART configuration

Go to USART1 setup interface and select Asynchronous Mode:

USART Setup Interface


Then, go to DMA Settings tab , click on Add button and select USART1_TX .

USART Setup : DMA Settings


Ensure DMA1 Channel1 is selected, and click on USART1_TX line to show DMA Request Settings.

USART Setup : DMA Settings 2


Go to NVIC Settings tab and enable USART1 global interrupt .

USART Setup : NVIC Settings


6.2. NVIC configuration

Go to NVIC Settings interface and set DMA1 Channel 1 global interrupt Preemption Priority to 15 (lowest priority) .
Check that USART1 global interrupt is enabled .

6.3. USART1 pinout definition

Go to Pinout view .
Set UASRT1_TX on PB6 and USART1_RX on PB7:

  • Click on PB6
  • Select USART1_TX in the list
  • Click on PB7
  • Select USART1_RX in the list

You can use the search located in the bottom right of the pinout view window to find a pin or signal name easily (here PB6 and PB7)

Pinout View


6.4. STM32_WPAN configuration

Go to STM32_WPAN setup interface and select the Configuration tab .
Enable the application traces , set CFG_DEBUG_TRACES_UART on hw_uart1 .
Configure the debug traces to manage the different types of logs .

STM32WPAN Setup


6.5. Project manager settings

Project Manager interface and select the Advanced Settings tab .
Configure MX_UASRT1_UART_Init function as:

  • Check Do Not Generate Function Call checkbox.
  • Uncheck Visibility (Static) checkbox.
MX_UASRT1_UART_Init function Settings


Once the traces configuration is done in STM32CubeMX, the code can be generated by following the steps described in Code Generation chapter.

7. P2P Server notifications and writes management

In order to use P2P Server Notification and Write characteristics, several points have to be configured:

  • User Button and the related Interrupt, to Notify the P2P Client
  • Blue LED, to receive a P2P Client write operation
  • Custom application code to manage SW1 and write operation on P2P Server service
STM32WB Nucleo board


7.1. User button and LED pinout

In the Nucleo board, LED pinout is:

  • Blue LED : PB5
  • Green LED: PB0
  • Red LED: PB1

Switch (user button) pinout is:

  • SW1: PC4
  • SW2: PD0
  • SW3: PD1

When used:

  • Switch pins are declared as GPIO_EXTIx (x = pin number)
  • LED pins are declared as GPIO_OUTPUT





7.2. LED and button setup

To configure the buttons and LEDs in this example, we will use the BSP files that we will include in the project at the end of this wikipage.

7.3. Code modification: User sections

Once your SW1 Button and Blue LED GPIOs are correctly setup, generate your project by following the steps described in Code Generation chapter.

The generated source code contains several sections calledUser Sections where users can add custom application code parts.
These sections are not erased/modified at project regeneration from CubeMX.

In order to manage SW1 and write operation on P2P Server service, some code parts have to be added in User Sections of the following files and their respective header files:

Files to update


  • In app_conf.h:

Define the task for the characteristic My_Switch_Char of My_P2P_Server by adding code in CFG_Task_Id_With_HCI_Cmd_t User Code Section:

/**< Add in that list all tasks that may send a ACI/HCI command */
typedef enum
{
    CFG_TASK_ADV_CANCEL_ID,
#if (L2CAP_REQUEST_NEW_CONN_PARAM != 0)
    CFG_TASK_CONN_UPDATE_REG_ID,
#endif
    CFG_TASK_HCI_ASYNCH_EVT_ID,
/* USER CODE BEGIN CFG_Task_Id_With_HCI_Cmd_t */
    CFG_TASK_SW1_BUTTON_PUSHED_ID,                                              /* Code Line to add */
/* USER CODE END CFG_Task_Id_With_HCI_Cmd_t */
    CFG_LAST_TASK_ID_WITH_HCICMD,                                               /**< Shall be LAST in the list */
} CFG_Task_Id_With_HCI_Cmd_t;


#define CFG_LED_SUPPORTED         1
#define CFG_BUTTON_SUPPORTED      1

#define PUSH_BUTTON_SW1_EXTI_IRQHandler     EXTI4_IRQHandler
#define PUSH_BUTTON_SW2_EXTI_IRQHandler     EXTI0_IRQHandler
#define PUSH_BUTTON_SW3_EXTI_IRQHandler     EXTI1_IRQHandler



  • In app_entry.c:

In order to make the application able to manage debug messages, app_entry.c file must be updated.
In MX_APPE_Init() function, add a call to APPD_Init() function into the USER CODE APPE_Init_1 section as follows:

void MX_APPE_Init( void )
{
  System_Init( );       /**< System initialization */

  SystemPower_Config(); /**< Configure the system Power Mode */

  HW_TS_Init(hw_ts_InitMode_Full, &hrtc); /**< Initialize the TimerServer */

/* USER CODE BEGIN APPE_Init_1 */
  APPD_Init();

  /**
   * The Standby mode should not be entered before the initialization is over
   * The default state of the Low Power Manager is to allow the Standby Mode so an request is needed here
   */
  UTIL_LPM_SetOffMode(1 << CFG_LPM_APP, UTIL_LPM_DISABLE);

  Led_Init();

  Button_Init();

/* USER CODE END APPE_Init_1 */
  appe_Tl_Init();	/* Initialize all transport layers */


Define the callback for handling the interrupts from SW1 presses by adding code in FD_WRAP_FUNCTIONS User Code Section:

/* USER CODE BEGIN FD_WRAP_FUNCTIONS */
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{                                                                                                 
  switch (GPIO_Pin)                                                                  
  {                                                                                             
    case BUTTON_SW1_PIN:                                                          
      APP_BLE_Key_Button1_Action();                                      
      break;                                                                                 
    default:                                                                                 
      break;                                                                                
  }                                                                                             
  return;                                                                                   
}                                                                                              
/* USER CODE END FD_WRAP_FUNCTIONS */


As well as initializing the LEDs and buttons:

/* USER CODE BEGIN PFP */
static void Led_Init( void );
static void Button_Init( void );
/* USER CODE END PFP */


/* USER CODE BEGIN FD_LOCAL_FUNCTIONS */
static void Led_Init( void )
{
#if (CFG_LED_SUPPORTED == 1)
  /**
   * Leds Initialization
   */
  BSP_LED_Init(LED_BLUE);
  BSP_LED_Init(LED_GREEN);
  BSP_LED_Init(LED_RED);

  BSP_LED_On(LED_GREEN);
#endif

  return;
}

static void Button_Init( void )
{
#if (CFG_BUTTON_SUPPORTED == 1)
  /**
   * Button Initialization
   */
  BSP_PB_Init(BUTTON_SW1, BUTTON_MODE_EXTI);
  BSP_PB_Init(BUTTON_SW2, BUTTON_MODE_EXTI);
  BSP_PB_Init(BUTTON_SW3, BUTTON_MODE_EXTI);
#endif

  return;
}
/* USER CODE END FD_LOCAL_FUNCTIONS */




  • In app_ble.c:

Define function for SW1 action by adding code in FD_SPECIFIC_FUNCTIONS User Code Section:

/* USER CODE BEGIN FD_SPECIFIC_FUNCTIONS */
void APP_BLE_Key_Button1_Action(void)
{
  P2PS_APP_SW1_Button_Action();
}
/* USER CODE END FD_SPECIFIC_FUNCTIONS */


  • In app_ble.h:

Declare the APP_BLE_Button1_Action() function, in EF User Code Section:

/* Exported functions ---------------------------------------------*/
  void APP_BLE_Init( void );

/* USER CODE BEGIN EF */
void APP_BLE_Key_Button1_Action(void);        /* Code Line to add */
/* USER CODE END EF */


  • In custom_app.h:

Declare P2PS_APP_SW1_Button_Action function, in EF User Code Section:

/* Exported functions ---------------------------------------------*/
  void Custom_APP_Init( void );
  void Custom_APP_Notification( Custom_App_ConnHandle_Not_evt_t *pNotification );
/* USER CODE BEGIN EF */
  void P2PS_APP_SW1_Button_Action(void);        /* Code Line to add */
/* USER CODE END EF */


  • In custom_app.c:

Add SW1_Status variable in CUSTOM_APP_Context_t User Code Section:

/* Private typedef -----------------------------------------------------------*/
typedef struct
{
  /* My_P2P_Server */
  uint8_t               Switch_c_Notification_Status;

  /* USER CODE BEGIN CUSTOM_APP_Context_t */
  uint8_t               SW1_Status;                      /* Code Line to add */
  /* USER CODE END CUSTOM_APP_Context_t */

  uint16_t              ConnectionHandle;
} Custom_App_Context_t;

/* USER CODE BEGIN PTD */

/* USER CODE END PTD */


In the same file, update snippets shown. The following traces code is to indicate the Smartphone requests to enable or disable notifications and write requests on My_P2P_Server service.
In CUSTOM_STM_LED_C_WRITE_NO_RESP_EVT User Section:

/* Functions Definition ------------------------------------------------------*/
void Custom_STM_App_Notification(Custom_STM_App_Notification_evt_t *pNotification)
{
  /* USER CODE BEGIN CUSTOM_STM_App_Notification_1 */

  /* USER CODE END CUSTOM_STM_App_Notification_1 */
  switch(pNotification->Custom_Evt_Opcode)
  {
    /* USER CODE BEGIN CUSTOM_STM_App_Notification_Custom_Evt_Opcode */

    /* USER CODE END CUSTOM_STM_App_Notification_Custom_Evt_Opcode */

  /* My_P2P_Server */
    case CUSTOM_STM_LED_C_READ_EVT:
      /* USER CODE BEGIN CUSTOM_STM_LED_C_READ_EVT */

      /* USER CODE END CUSTOM_STM_LED_C_READ_EVT */
      break;

    case CUSTOM_STM_LED_C_WRITE_NO_RESP_EVT:
      /* USER CODE BEGIN CUSTOM_STM_LED_C_WRITE_NO_RESP_EVT */
      APP_DBG_MSG("\r\n\r** CUSTOM_STM_LED_C_WRITE_NO_RESP_EVT \n");
      APP_DBG_MSG("\r\n\r** Write Data: 0x%02X %02X \n", pNotification->DataTransfered.pPayload[0], pNotification->DataTransfered.pPayload[1]);
      if(pNotification->DataTransfered.pPayload[1] == 0x01)
      {
        BSP_LED_On(LED_BLUE);
      }
      if(pNotification->DataTransfered.pPayload[1] == 0x00)
      {
        BSP_LED_Off(LED_BLUE); 
      } 
     /* USER CODE END CUSTOM_STM_LED_C_WRITE_NO_RESP_EVT */
      break;


In CUSTOM_STM_SWITCH_C_NOTIFY_ENABLED_EVT and CUSTOM_STM_SWITCH_C_NOTIFY_DISABLED_EVT User Sections:

case CUSTOM_STM_SWITCH_C_NOTIFY_ENABLED_EVT:
      /* USER CODE BEGIN CUSTOM_STM_SWITCH_C_NOTIFY_ENABLED_EVT */
      APP_DBG_MSG("\r\n\r** CUSTOM_STM_BUTTON_C_NOTIFY_ENABLED_EVT \n");

      Custom_App_Context.Switch_c_Notification_Status = 1;        /* My_Switch_Char notification status has been enabled */
      /* USER CODE END CUSTOM_STM_SWITCH_C_NOTIFY_ENABLED_EVT */
      break;

    case CUSTOM_STM_SWITCH_C_NOTIFY_DISABLED_EVT:
      /* USER CODE BEGIN CUSTOM_STM_SWITCH_C_NOTIFY_DISABLED_EVT */
      APP_DBG_MSG("\r\n\r** CUSTOM_STM_BUTTON_C_NOTIFY_DISABLED_EVT \n");

      Custom_App_Context.Switch_c_Notification_Status = 0;        /* My_Switch_Char notification status has been disabled */
      /* USER CODE END CUSTOM_STM_SWITCH_C_NOTIFY_DISABLED_EVT */
      break;


Add code snippets in Custom_App_Init() function to register the send notification task that is started when SW1 button is pressed, in CUSTOM_APP_Init User Section:

void Custom_APP_Init(void)
{
  /* USER CODE BEGIN CUSTOM_APP_Init */
  UTIL_SEQ_RegTask(1<< CFG_TASK_SW1_BUTTON_PUSHED_ID, UTIL_SEQ_RFU, Custom_Switch_c_Send_Notification);

  Custom_App_Context.Switch_c_Notification_Status = 0;   
  Custom_App_Context.SW1_Status = 0;                 

  /* USER CODE END CUSTOM_APP_Init */
  return;
}


And code snippet to allow the task to run once SW1 is pressed, in FD_LOCAL_FUNCTIONS User Section:

/* USER CODE BEGIN FD_LOCAL_FUNCTIONS*/
  void P2PS_APP_SW1_Button_Action(void)
  {
    UTIL_SEQ_SetTask(1<<CFG_TASK_SW1_BUTTON_PUSHED_ID, CFG_SCH_PRIO_0);

    return;
  }
/* USER CODE END FD_LOCAL_FUNCTIONS*/


Add code snippet for sending notification request to the smart phone, in Switch_c_NS User Section:

void Custom_Switch_c_Send_Notification(void) /* Property Notification */
{
  uint8_t updateflag = 0;

  /* USER CODE BEGIN Switch_c_NS_1*/
  if (Custom_App_Context.Switch_c_Notification_Status)
  {
    updateflag = 1;
    
    if (Custom_App_Context.SW1_Status == 0)
    {
      Custom_App_Context.SW1_Status = 1;
      NotifyCharData[0] = 0x00;
      NotifyCharData[1] = 0x01;
    }
    else
    {
      Custom_App_Context.SW1_Status = 0;
      NotifyCharData[0] = 0x00;
      NotifyCharData[1] = 0x00;
    }

    APP_DBG_MSG("-- CUSTOM APPLICATION SERVER  : INFORM CLIENT BUTTON 1 PUSHED \n");
  }
  else
  {
    APP_DBG_MSG("-- CUSTOM APPLICATION : CAN'T INFORM CLIENT -  NOTIFICATION DISABLED\n");
  }     
  /* USER CODE END Switch_c_NS_1*/

  if (updateflag != 0)
  {
    Custom_STM_App_Update_Char(CUSTOM_STM_SWITCH_C, (uint8_t *)NotifyCharData);
  }

  /* USER CODE BEGIN Switch_c_NS_Last*/

  /* USER CODE END Switch_c_NS_Last*/

  return;


  • In custom_stm.c:

Update Custom_STM_Event_Handler() function to manage My_LED_Char write, in CUSTOM_STM_Service_1_Char_1_ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE User Section:

static SVCCTL_EvtAckStatus_t Custom_STM_Event_Handler(void *Event)
{
  […]
 event_pckt = (hci_event_pckt *)(((hci_uart_pckt*)Event)->data);

  switch(event_pckt->evt)
  {
    case HCI_VENDOR_SPECIFIC_DEBUG_EVT_CODE:
      blecore_evt = (evt_blecore_aci*)event_pckt->data;
      switch(blecore_evt->ecode)
      {
        case ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE:
        […]
          else if(attribute_modified->Attr_Handle == (CustomContext.CustomLed_CHdle + CHARACTERISTIC_VALUE_ATTRIBUTE_OFFSET))
          {
            return_value = SVCCTL_EvtAckFlowEnable;
            /* USER CODE BEGIN CUSTOM_STM_Service_1_Char_1_ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE */
            Notification.Custom_Evt_Opcode = CUSTOM_STM_LED_C_WRITE_NO_RESP_EVT;
            Notification.DataTransfered.Length=attribute_modified->Attr_Data_Length;
            Notification.DataTransfered.pPayload=attribute_modified->Attr_Data;
            Custom_STM_App_Notification(&Notification);
            /* USER CODE END CUSTOM_STM_Service_1_Char_1_ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE */
          } /* if(attribute_modified->Attr_Handle == (CustomContext.CustomLed_CHdle + CHARACTERISTIC_VALUE_ATTRIBUTE_OFFSET))*/
          /* USER CODE BEGIN EVT_BLUE_GATT_ATTRIBUTE_MODIFIED_END */

          /* USER CODE END EVT_BLUE_GATT_ATTRIBUTE_MODIFIED_END */
          break;



  • In stm32wbxx_it.c:
/**
 * @brief  This function handles External line
 *         interrupt request.
 * @param  None
 * @retval None
 */
void PUSH_BUTTON_SW1_EXTI_IRQHandler(void) // JOE
{
  HAL_GPIO_EXTI_IRQHandler(BUTTON_SW1_PIN);
}


8. Inserting external files to complete the creation of our P2P server project, we will now add the following external BSP files:

To complete the creation of our P2P server project, we will now add the following external BSP files:

  • stm32wbxx_nucleo.c
  • stm32wbxx_nucleo.h
  • stm32wbxx_nucleo_conf.h
  • stm32wbxx_nucleo_errno.h

You can download all BSP STM32WBXX-NUCLEO components here.
These files provide a set of firmware functions to manage the LEDs and push buttons available on the STM32WBxx-Nucleo board.

Add the stm32wbxx_nucleo.c and stm32wbxx_nucleo.h files in your project folder BLE_Custom\Drivers\BSP.

Then rename the stm32wbxx_nucleo_conf_template.h file to stm32wbxx_nucleo_conf.h.

Now, add stm32wbxx_nucleo_conf.h and stm32wbxx_nucleo_errno.h in your project folder (BLE_Custom\Core\Inc).

To add external code files, we recommend using the .extSettings file (For more details, visit UM1718 User Manual section 6.4.

The .extsettings file allows you to add additional settings which can be used when external tools call STM32CubeMX to generate the project and require specific project settings.

.extSettings file


Your .extSettings file should contain the following:

[ProjectFiles]
HeaderPath=..\Drivers\BSP\
[Others]
Define=USE_STM32WBXX_NUCLEO
[Groups]
Drivers/BSP/P-NUCLEO-WB55.Nucleo=../Drivers/BSP/stm32wbxx_nucleo.c;

The path in HeaderPath indicates where the stm32wbxx_nucleo.h file is stored in your project. In Groups, you need to specify where you want the code file to appear in your workspace, and where it is stored.

9. Code generation

Once configuration is done in STM32CubeMX, the code can be generated :

Code Generation


Project can then be open :

Generated project pop-up


Open Project with IAR IDE, (\EWARM\ Project.eww) and ensure project options are correctly defined:

IAR Project Setup


Project build from IAR IDE:

  • Check there is no error when building the project from IAR.
Warning
Some build warnings could be listed due to declared functions but never referenced, or variables not used when pairing is off.
  • Connect the Nucleo board to the PC with USB cable.
  • Flash the binary file into the P-NUCLEO-WB55[7] board.
  • Run the application to make it advertise.
  • Connect MyCST application thanks to ST BLE ToolBox application. Refer to ST BLE Toolbox Application chapter.

10. TeraTerm configuration

This chapter describes how to setup TeraTerm in order to display traces from the STM32WB projects.
The ST-Link of the Nucleo board is displayed as a Virtual COM Port (as shown in the Device Manager window below).
USART1 pins are routed through this port, which is connected to serial terminal (TeraTerm) to display traces.

Device Configuration manager


In TeraTerm interface, select the corresponding serial port:

TeraTerm Serial port selection


Set the Serial Port configuration as follows:

TeraTerm Serial port configuration


Once the TeraTerm is configured and connected to the Nucleo board you can run your code and the enabled logs must be displayed.


11. ST BLE toolbox application

The following chapter describes ST BLE ToolBox application utilization.

11.1. Scan and connect

When you launch ST BLE ToolBox smartphone application, it scans to search WB devices. On the scan interface, the name (MyCST) of the application previously generated and build using STM32CubeMX and IAR must be displayed once discovered.

Select the application by clicking on his name, then click on Connect button:

ST BLE Toolbox: scan interface

11.2. Discover services and characteristics

When connected to MyCST, scroll on services to find the defined ones.

  • P2P Server Service:

Tap P2P Server to display the associated characteristics:

ST BLE Toolbox Services interface


As defined in STM32CubeMX we see P2P Server’s characteristics and associated properties:

Service P2P Server : UUID = 0xFE40
Characteristic 1 : UUID = 0xFE41 is Readable and Writable
Characteristic 2 : UUID = 0xFE42 is Notify
ST BLE Toolbox : P2P Server Characteristics interface


In the profile tab, a dedicated user interface lets you activate the LED and receive notification of the button:

ST BLE Toolbox : P2P Server UI


12. References