| Back to main page |
|---|
1. Introduction
The ST67W611M1 has a built-in UART interface used at boot to:
- Flash the module binary
- Retrieve the module's OTP values
- Perform RF tests with the RF test tool.
- Configure a user-defined/customer-defined MAC address.
This boot selection follows the bootstrap configuration described in the BOOT section.
The ST67W611M1 built-in UART can also be used during software development to retrieve debug traces.
The interface is mapped to the following module pins:
- UART_RX (23) pin: UART data to the module.
- UART_TX (22) pin: UART data from the module.
2. UART interface specification and features
The UART interface includes various features and is configured as follows:
- Full-duplex asynchronous communication.
- Data bit length: 8 bits.
- Stop bit length: 1 bit.
- Parity: None.
- Hardware flow control (RTS/CTS): None.
- Baud rate: 2,000,000 Bauds.
- UART signal levels: VDDIO logic levels.
3. UART interface hardware implementation
The module UART pins must be routed to ensure accessibility by a UART master. This could be the application host (connection to its UART pins) or an off-board UART master or bridge (through on-board test points or a provisioned connector).
Both UART signals are push-pull, so on-board pull-ups are not required. There are no specific constraints on routing these two signals since UART is not used during normal operation, as explained above.