ST67W611M1 power supplies and grounding

Back to main page


1. Introduction

The power domains of the ST67W611M1 are divided into analog and digital domains. The analog domain is supplied through VDD33 (16) pin and the digital domain through VDDIO (9 and 25) pins. The mother board must provide these voltage supplies to the module.

2. Power supply specification

VDD33 is specified at 3.3 V typical with 2.97 V to 3.63 V range.

VDDIO can be supplied within two ranges to be decided by the customer according to the IO interface voltage of the Host:

  • 3.3 V typical with 2.97 V to 3.63 V range.
  • 1.8 V typical with 1.62 V to 1.98 V range.

Warning: Unlike the other ST67W611M1 I/Os which are VDDIO I/Os, CHIP_EN is a 3.3 V analog input pin. Ensure that CHIP_EN signal uses 3.3 V logic levels even when VDDIO is set to 1.8 V.

LDOs and bucks can be used to generate these supply voltages. Current consumption figures are provided in the datasheet to help select the right LDOs/bucks and size the power tracks.

3. Grounding implementation

Connect all GND pins directly to a solid GND plane. Place at least 5 vias on each central PAD to ensure a good power dissipation. Drill multiple ground vias on the top and bottom layers to minimize the current return path.

4. Power supplies implementation

The power supplies for the ST67W611M1 can be generated using LDOs or bucks as mentioned above. It is necessary to make sure the supply voltages are clean with minimum ripple and, in all cases, that they never go outside the specified ranges. Additional care must be given in the case of the buck layout.

When using 3.3 V for VDDIO, a single power supply source can be used for both VDD33 and VDDIO.

It is recommended to use one 10 μF decoupling capacitor per VDD pin. Decoupling capacitors must be placed as close as possible to their corresponding pins with the ground pad of each capacitor connected to the board ground through a dedicated via.