| STM32CubeMX |
| Back to main page |
|---|
1. Introduction
The X-CUBE-ST67W61.pack is available in the STM32CubeMX ecosystem.
It can be installed from the “Software Packs” menu, more precisely from the "Manage Software packs” (Alt+U) and “Select Components” (Alt+O) panels.
The projects provided in the X-CUBE-ST67W61 are generated using the STM32CubeMX for NUCLEO-U575ZI-Q, NUCLEO-H7S3L8, NUCLEO-H563ZI and NUCLEO-N657X0-Q boards and defined as below:
| Project name | NUCLEO-U575ZI-Q | NUCLEO-H7S3L8 | NUCLEO-H563ZI | NUCLEO-N657X0-Q |
|---|---|---|---|---|
| ST67W6X_BLE_Commissioning | MX | - | - | - |
| ST67W6X_BLE_p2pClient | MX | - | - | - |
| ST67W6X_BLE_p2pServer | MX | - | - | - |
| ST67W6X_CLI | MX | MX | MX | MX |
| ST67W6X_CLI_LWIP | MX | MX | MX | MX |
| ST67W6X_Echo | MX | MX | MX | MX |
| ST67W6X_FOTA | MX | - | - | - |
| ST67W6X_FOTA_LWIP | MX | - | - | - |
| ST67W6X_HTTP_Server | MX | - | - | - |
| ST67W6X_HTTPS_Client | MX | - | - | - |
| ST67W6X_WiFi_Commissioning | MX | - | - | - |
| ST67W6X_MQTT | MX | - | - | - |
| ST67W6X_MQTT_LWIP | - | - | MX | - |
The scope of X-CUBE-ST67W61.pack within STM32CubeMX is to help users:
- Create their own project
- Port existing application examples to other devices
- Combine both of the above tasks
The prerequisites are to have the latest:
- STM32CubeMX version installed - version 6.17.0 was used to make this tutorial
- X-CUBE-ST67W61 installed - version 1.3.0 was used for this tutorial
1.1. Hardware requirements
- 256 KB of flash memory
- 48 KB of RAM memory
- At least, SPI and DMA must be present
Remember to flash the updated code in the ST67W611M1, refer to How to flash the ST67W611M1.
1.2. FreeRTOS
All the applications available in the X-CUBE-ST67W61 expansion package are based on FreeRTOS v11.2.0 available in the X-CUBE-FREERTOS V1.4.0.
- STM32N6 requires at least X-CUBE-FREERTOS V1.3.1 expansion package based on FreeRTOS 10.6.2 version
- CM33 core-based families need at least X-CUBE-FREERTOS V1.3.0
- Old devices use legacy FreeRTOS (that is, FreeRTOS provided directly in the middleware without the need to select the X-CUBE-FREERTOS expansion package) and the version of such FreeRTOS depends on the device families.
- STM32L0, STM32F0, use FreeRTOS v10.2.1
- STM32H7, STM32L4, STM32G0 and STM32F4 use FreeRTOS v10.3.1
- STM32H7Rx/7Sx uses FreeRTOS V10.6.2
Required adjustments:
- Setting the heap size bigger than default size (set to xxx by default by the STM32CubeMX). In the provided examples, it is set to 30 KB. Refer to Heap Size adjustment.
- For few device families, the associated FreeRTOS version can be wrongly detected. In such case, it might be necessary to change the Appli/App/main_app.c to include the correct FreeRTOS API file (app_freertos.h or FreeRTOS.h).
1.3. User code sections limitations
The X-CUBE-ST67W61 applications implement some basic support of USER CODE SECTION to be compatible with STM32CubeMX methodology but not with the intention to cover all cases.
The STM32CubeMX GUI (within component selector) provides the user application which allows the user to write his own application code within USER CODE SECTION.
1.4. X-CUBE-ST67W61 migration know limitation
There is a migration feature in the Software Packs Component Selector interface that allows you to upgrade the installed package to the latest available version.
This migration generates two issues that must be fixed manually:
- The Platform Settings are reset and must be reconfigured with the IP defined in the project.
- The FreeRTOS component may become corrupted during the migration operation, and part of its configuration must be restored manually.
Close STM32CubeMX. Open the locally generated *.bkp_ioc file, which contains a backup of the previous configuration.
Copy the last two lines of the FreeRTOS configuration section and paste them into the current *.ioc file, just before the last line of the same section.
Save the file and reopen it in STM32CubeMX to verify that FreeRTOS is fully enabled again.
2. X-CUBE-ST67W61.pack configuration
2.1. Component Selector overview
The pack consists of various layers and components.
The Component Selector lets the user choose which modules are compiled and linked to the project. Some modules are always required, some depend on the chosen application, and others are optional (for example for enhanced logs, statistics, performance measures, trace dumping, low power, and more).
2.1.1. Main components
These two components must always be selected to use the applications delivered in the X-CUBE-ST67W61.
| Component | Description |
|---|---|
| ST67 architecture |
|
| ServiceAPI | Wi-Fi®, Bluetooth® LE, Network, HTTP, MQTT, OTA and system APIs. Required to provide interfaces to the chosen application. |
| ATDriver | Implementation of AT layer driver and SPI Bus Management. Required to exchange with the ST67W611M1 module. |
2.1.2. Applications component
| Component | Description |
|---|---|
| Application | X-CUBE-ST67W61 contains ten functional applications and one user application. If the user wants to create its own application based on the ST67W6X_Network_Driver Middleware,
it is suggested to select the user application as a starting point. |
Some applications provided in the X-CUBE-ST67W61 are extended compared to what STM32CubeMX generates starting from an empty directory.
In particular:
- FOTA application for NUCLEO-U575ZI-Q implements also the host firmware to be updated. The related code strongly depends on the host device and on its flash memory. Refer to FOTA application for details.
- HTTP server and Wi-Fi commissioning applications embeds an HTTP Server. Refer to How to generate html_page.h for details.
- MQTT and HTTPS client applications are functional with the embedded (default) certificate. Refer to Security and certificates to generate your own certificates.
2.1.3. Utilities
These three elements are optional but may be required, depending on the application chosen.
If a component is not selected, the associated files are not linked in the project structure.
| Component | Description |
|---|---|
| Logging | Redirect all middleware and application traces to the selected hardware output. By default, UART is chosen as the output solution. If the Logging component is not selected in the Component Selector, printf / putchar is used instead. Users have the option to implement their own module by adhering to the API, which can be achieved by overriding the function vLoggingPrintf(). When Logging is selected in the Component Selector, the default settings configure the OUTPUT_MODE to OUTPUT_MODE_USART and the LOG_LEVEL to DEBUG for all applications. Users can modify these settings through the GUI in the parameter settings panel. |
| Service Shell | Shell functions to manage the API functions directly into the UART terminal. The Shell utility is required to use the Service Shell features. |
| Shell utility | Provide a command line interface solution for the user to interact with the program via a serial command. When the component is selected, the feature is disabled by default. The SHELL_ENABLE parameter can be modified in the Parameter Settings tab. |
| Statistics | Provide some tools to evaluate the performances of the RTOS or network. When the component is selected, the features are disabled by default. The TASK_PERF_ENABLE, MEM_PERF_ENABLED, IPERF_ENABLED parameters can be modified in the Parameter Settings tab. |
When using the Shell utility, all Service Shell functions must be placed in specific region of the flash memory.
Depending on the IDE chosen, the following change must be applied to the project structure:
| IDE | Shell utility specific region requirement |
|---|---|
| EWARM | In the linker script file (as example stm32u575xx_flash.icf):
keep { section FSymTab };
place in ROM_region { readonly, ro section FSymTab };
|
| STM32CubeIDE | In the linker script file (as example STM32U575ZITXQ_FLASH.ld):
/* The program code and other data into "FLASH" Rom type memory */
.text :
{
*(.text) /* .text sections (code) */
...
. = ALIGN(4);
__fsymtab_start = .;
KEEP(*(FSymTab))
__fsymtab_end = .;
_etext = .; /* define a global symbols at end of code */
} >FLASH
|
| MDK-ARM | In Misc controls field of the project Linker options (Project->Options->Linker->Misc controls) add the following options:
--keep *.o(FSymTab) --diag_suppress L6319W The diag suppress is needed to avoid the warning about the unused section. |
2.1.4. Third-party middlewares
These five optional components provide specific features for some applications.
| Component | Version | Description |
|---|---|---|
| LwIP | 2.2.1 | Small independent implementation of the TCP/IP protocol suite. Mandatory when ST67 architecture T02 is selected. |
| MQTT-C | 1.1.6 | Lightweight publisher-subscriber-based messaging MQTT protocol. Compliant with ST67 architecture T02 and LwIP component. |
| mbedTLS | 3.6.4 | The Mbed cryptography library is a reference implementation of the cryptography interface of the Arm Platform Security Architecture (PSA). Compliant with ST67 architecture T02 and LwIP component. |
| cJSON | 1.7.19 | Ultralightweight JSON parser used by several applications (CLI, MQTT, HTTPS client, FOTA). |
| LittleFS | 2.11.1 | Minimal File System used by projects to export certificates files to the ST67W611M1 module. These certificates are needed for the security methods (HTTPS, MQTTS, SSL). |
| TraceRecorder | 4.10.3 | Percepio Trace tool used to analyze the real-time operating system execution. More details : How to debug with Percepio Trace |
2.1.5. Low-power
The tiny low-power mode (LMP) provides a set of macros to enter and exit a chosen low-power mode (Sleep, Stop, Standby).
When selected, FreeRTOS tickless may be required to manage low power directly in the operating system sequencer.
The feature is disabled by default. The LOW_POWER_MODE parameter can be modified in the Parameter Settings tab.
The low-power code is provided for the STM32U5 family. For other platforms, a warning is raised to inform the user to verify compatibility.
2.1.6. Components used by projects
The projects available in the X-CUBE-ST67W61 are defined with the following components:
- AT Driver, service API and utility logging are always enabled
- FreeRTOS tickless and utility LPM are enabled for all projects based on NUCLEO-U575ZI-Q host board
| Project name | Application | ST67 Architecture | Service Shell/Utility shell | Utility statistics | LwIP | MQTT-C | mbedTLS | cJSON | LittleFS |
|---|---|---|---|---|---|---|---|---|---|
| ST67W6X_BLE_Commissioning | BLE_Commissioning | T01 | No | No | No | No | No | No | No |
| ST67W6X_BLE_p2pClient | BLE_p2pClient | T01 | No | No | No | No | No | No | No |
| ST67W6X_BLE_p2pServer | BLE_p2pServer | T01 | No | No | No | No | No | No | No |
| ST67W6X_CLI | CLI | T01 | Yes | Yes | No | No | No | Yes | Yes |
| ST67W6X_CLI_LWIP | CLI | T02 | Yes | Yes | Yes | Yes | No | No | Yes |
| ST67W6X_Echo | Echo | T01 | No | No | No | No | No | No | No |
| ST67W6X_FOTA | FOTA | T01 | No | No | No | No | No | Yes | No |
| ST67W6X_FOTA_LWIP | FOTA | T02 | No | No | Yes | No | Yes | Yes | No |
| ST67W6X_HTTP_Server | HTTP_Server | T01 | No | No | No | No | No | No | No |
| ST67W6X_HTTPS_Client | HTTPS_Client | T01 | Yes | No | No | No | No | Yes | Yes |
| ST67W6X_WiFi_Commissioning | WiFi_Commissioning | T01 | No | No | No | No | No | No | No |
| ST67W6X_MQTT | MQTT | T01 | No | No | No | No | No | Yes | Yes |
| ST67W6X_MQTT_LWIP | MQTT | T02 | No | No | Yes | Yes | Yes | Yes | Yes |
2.2. Configuration panel
The "Parameters Setting" panel is used to select the features to be initialized (Wi-Fi®, Bluetooth® LE, Network, etc.) and configure the ST67W6X_Network_Driver.
The "Platform Settings" is used to map the IPs instances (for example: SPI, USART, and more).
2.2.1. Parameter Settings tab
Parameters are spread across several configuration files:
| Section | Description |
|---|---|
| W6X Init Modules | The ST67W6X_Network_Driver Service API and AT Driver components are composed by different "modules" (Wi-Fi®, Bluetooth® LE, network, MQTT). The user can choose which module to initialize:
The API code for these modules is always generated, but it is not linked if not initialized. |
| Basic parameters | Setup the global common configuration used by the application and the middleware components. |
| Logging-Shell parameters | Setup the Logging and Shell components in the "logging_config.h" and "shell_config.h" files. |
| W6X parameters | Setup the API default configurations (mainly used at initialization) in the "w6x_config.h" file. |
| W61 driver parameters | Setup the AT drivers default configuration in the "w61_driver_config.h" file. |
2.2.2. Platform Settings tab
Mapping between the IPs used by the ST67W61 applications versus the IPs that have been enabled on the device.
| IP | Description |
|---|---|
| SPI | Communication to the modem uses SPI. |
| USART | User can decide to not output log, use ITM or use its own system. However, when shell component is enabled USART is mandatory. |
| LPTIM | Required only in case FreeRTOS tickless component is selected (used for low-power with STM32U5) |
3. How to generate projects
Three cases are covered:
- How to generate a project starting from an existing ioc
- How to export a project to a pinout compatible MCU
- How to generate a project starting from scratch
3.1. How to generate a project starting from an existing ioc
This can be done for one of the devices available in the pack (NUCLEO-U575ZI-Q, NUCLEO-H563ZI, NUCLEO-H7S3L8 and NUCLEO-N657X0-Q).
For other devices than NUCLEO-U575ZI-Q, the X-CUBE-ST67W61 only provides two projects (CLI and Echo),
This method allows to generate easily the other projects for the other mentioned devices.
| Steps | Description | Graphical view |
|---|---|---|
| Step 1 | Copy an ioc file in a new directory. | |
| Step 2 | Choose the application you want to generate (for example: User). | |
| Step 3 | Adapt the parameters values if needed (Parameter Settings, Platform Settings). | |
| Step4 | Select the IDE and Press Generate code button. | |
| Step5 (Optional) | Skip the step5, enable the Flat directory structure, select the IDE and Press Generate code button. To use flat directory structure (that is, driver and MW directories copied into your project directory) |
If the component shell is used, the linker file has to be customized, see Utilities.
The examples above demonstrate how to generate the user application, but this method can be applied to any applications not provided for a specific target (for example, it can be applied to NUCLEO-H7S3L8, NUCLEO-H563ZI, and NUCLEO-N657X0-Q).
Remember that USER CODE SECTIONS for applications other than user may not meet all requirements.
3.2. How to export a project to a pinout compatible MCU
Exporting a project is done by starting from an existing IOC file and using the “Pinout compatible MCU” feature. The feature is deeply described in the chapter 15 of the following STM32CubeMX tutorial:
UM1718 - STM32CubeMX for STM32
Within the IOC provided in the pack (NUCLEO-U575ZI-Q, NUCLEO-H563ZI, NUCLEO-H7S3L8 or NUCLEO-N657X0-Q), choose the one with the package, board, and pinout most similar to the device needing the application port.
For example, to generate for STM32L552ZCTxQ, the IOC provided for NUCLEOS U575ZI-Q are a good starting point because STM32L552ZCTxQ is full pin compatible.
- If the device to which user wishes to port the code is available and if it is Pinout Fully compatible, the expected exporting time is rather quick.
- If the device to which user wishes to port the code is available, but it needs HW changes, additional work (and time) is required, depending on the incompatibilities.
- If the device to which user wishes to port the code is not available, porting becomes more complex. Refer to next chapter: Generate from scratch.
Double-clicking on the desired device creates a new IOC, based on that device.
Note that all IPs (SPI, UART) and GPIO labels and settings are automatically ported.
The user might need to apply minor adaptations:
- The interrupt priority if they are not in the same range.
- When passing from a device using X-CUBE_FreeRTOS to a device family using legacy FreeRTOS, the FreeROS must be reenabled and reconfigured. Refer to X-CUBE-ST67W61-pack_FreeRTOS.
- The X-CUBE-ST67W61 parameters might also need to be updated, in particular the platform settings. Refer to X-CUBE-ST67W61-pack_configuration.
- Check the SPI clock settings, where the transmission speed must be a maximum of 40 Mbps (clock domain adjustment may be required).
Once everything is configured, press the "Generate code" button.
The image below shows the code generated for the selected family. In this example STM32L5xx_HAL_Driver is included.
If the shell component is used, the linker file must be customized, refer to Shell.
3.3. How to generate a project starting from scratch
This is necessary to generate a project from scratch when the device family, the type of package or the shield are not pin-compatible with the IOC delivered as examples.
A step by step description based on a NUCLEO-G0B1RE board is shown below. The following flow can be applied to other Nucleo family boards (STM32U5, STM32H7Rx/7Sx, STM32H5, ...).
3.3.1. Step 1: Project creation
Open STM32CubeMX and create the new project
Note: Nucleo-64 is selected since STM32G0 is chosen as a target example, but Nucleo-144 could be chosen for other STM32.
3.3.2. Step 2: Pinout & Configuration
Provides all the different steps to configure the hardware pinouts and the relevant middleware
3.3.2.1. Pinout
When generating an application from scratch and if X-NUCLEO-67W61M1 is used, the pinout must be set in accordance with the ST67W61M1 Arduino interfaces.
The table below summarizes the available Arduino interfaces:
| Pin function | Arduino Connector | NUCLEO pin name | GPIO mode | GPIO pull mode | GPIO speed |
|---|---|---|---|---|---|
| SPI_CLK | CN5.D13 | PA5 | AF PP | No pull | Very high |
| SPI_MISO | CN5.D12 | PA6 | AF PP | No pull | Very high |
| SPI_MOSI | CN5.D11 | PA7 | AF PP | No pull | Very high |
| SPI_CS | CN5.D10 | PB0 | Output PP | No pull | High |
| USER_BUTTON | N/A | PC13 | EXTI Falling | Pull-up | N/A |
| CHIP_EN | CN9.D5 | PB4 | Output PP | No pull | High |
| BOOT | CN9.D6 | PB4 | Output PP | No pull | Low |
| SPI_RDY | CN9.D3 | PB3 | EXTI Falling/Rising | No pull | N/A |
For reference, the X-NUCLEO-67W61M Arduino view is shown below:
| Setting | Description |
|---|---|
| UART GPIO | USART2 Mode: Asynchronous
In the Project Manager Menu, under Advanced Settings, enable the UART register callback. |
| SPI GPIO | SPI1 Mode: Full-duplex Master
|
| Channels DMA | DMA1 Channels DMA setting - association with SPI
|
3.3.2.2. Configuration
| Setting | Description | |
|---|---|---|
| Low Power Timer | The following LPTIM1 setting is just given as a "how to do" in case of low-power application requirements. This low-power and FreeRTOS tickless requirement are only available on STM32U5 platform. Refer to Low Power requirements. | |
| GPIO | ||
| Timer | ||
| NVIC Settings |
3.3.3. Step 3: Clock configuration
In the ''Clock Configuration'' panel, set the SPI clock to a maximum of 40 MHz. In this example, the system clock is set to maximum frequency of 64 MHz, prescaler set 2, increasing the SPI clock speed to 32 MHz
3.3.4. Step 4: Middleware and software packs
After having configured the hardware pinouts, the real time kernel and software package must be selected and configured.
3.3.4.1. FreeRTOS parameters adjustments
FreeRTOS component can be either selected from middleware (FREERTOS) or from the software pack (X-CUBE-FREERTOS) depending on the chosen STM32.
The size heap value should be set at least to 40 Kbytes. In order to optimize the memory, this value can be adjusted during integration and validation tests of the application.
3.3.4.2. X-CUBE-ST67W61 software component
By selecting the X-CUBE-ST67W61 software component, up to 10 different applications (Echo, WiFi_Commissioning, CLI, BLE_Commissioning, BLE_p2p_Client, BLE_p2p_Server, FOTA, HTTP_Server, HTTPS_Client, MQTT) and one user project can be selected.
See Component Selector overview for more details.
After selecting an application (in this case, "Echo"), enable the software pack components using the associated checkboxes.
The platform setting tab must also be set.
See Configuration panel for more details.
3.3.5. Step 5: Generate and build the project
After completing the "Project Manager" setting, press "Generate Code" button.
For STM32 on CM0/CM0+ cores with FreeRTOS version older than 10.6, add the definition of xPortIsInsideInterrupt() as defined in macroport.h cf legacy FreeRTOS
Click on "Open Project". At this point, two options are displayed:
- Launch directly a "Rebuilt all" IAR command to generate a new executable. The user can face compilation issues, which can be solved using manual user modifications described above.
- Enter "Manual user modifications" before launching the "Rebuilt all" IAR command to generate a new executable.
Whatever the options chosen, the final build should be OK
Now, binary is ready to download and run on the target device, allowing you to debug the application if any functional issues arise.