ST67W611M1 Bluetooth® Low Energy – Wi-Fi® Commissioning

Back to main page

1. Wi-Fi® commissioning over Bluetooth® Low Energy presentation

This application aims to demonstrate how to provision Wi-Fi® credentials via Bluetooth® Low Energy to establish a Wi-Fi® connection to an access point.
It also provides an example of how to update the ST67W611M1 firmware over the air via BLE (see Bluetooth® Low Energy FUOTA).

The solution uses a vendor-specific, dedicated Bluetooth® Low Energy profile and a remote client interface (ST BLE Toolbox smartphone application or ST Web Bluetooth®).

Bluetooth® Low Energy commissioning solution overview
WW6 Commissioning Description


2. Requirements

2.1. Software and system requirements

Note
Each project uses a specific ST67W611M1 binary, ST67W6X_BLE_Commissioning requires st67w611m_mission_t01_v2.x.y.bin

More information is available in ST67W611M1 Hardware setup wiki page.

The software requirements are as follows (minimum IDE versions):

  • STM32CubeIDE toolchain V2.1.0 [1].
  • IAR Embedded Workbench for Arm (EWARM) toolchain V9.30.1
  • RealView Microcontroller Development Kit (MDK-ARM) toolchain V5.39

Programmer:

  • STM32CubeProgrammer [2] to program the board with a pre-generated binary file

HyperTerminal:

  • Use the application through the serial link
  • Open a HyperTerminal client connected to the host ST-LINK COM port

The serial COM port must be configured as shown below:

Baudrate 921600
Data 8b
Stopbit 1b
Parity None
Flow control None
Rx LF
Tx LF
Local Echo Off

For further details, refer to the HyperTerminal setup page.

2.2. Hardware requirements

This example runs on the NUCLEO-U575ZI-Q [3] board combined with the X-NUCLEO-67W61M1 board.

The X-NUCLEO-67W61M1 board is plugged into the NUCLEO-U575ZI-Q board via the Arduino® connectors:

  • The 5V, 3V3, GND through the CN6
  • The SPI (CLK, MOSI, MISO), SPI_CS and USER_BUTTON signals through the CN5
  • The BOOT, CHIP_EN, SPI_RDY and UART TX/RX signals through the CN9

The USER_BUTTON refers to the button mounted on the X-NUCLEO-67W61M1. Indeed, the user button on the STM32 Nucleo board is not used in external interrupt mode due to a conflict with another EXTI pin requirement. The button must be defined with the user label USER_BUTTON and EXTI falling mode.

3. Wi-Fi® commissioning profile

The Wi-Fi® commissioning profile is a Generic Attribute Profile (GATT)-based low-energy profile defined by STMicroelectronics with proprietary UUIDs (128 bits).
The Wi-Fi® commissioning application demonstrates point-to-point communication using proprietary service and characteristics. It acts as a Peripheral device with one GATT service and four characteristics.

The Wi-Fi® commissioning server:

  • Contains the Wi-Fi® commissioning service, which exposes four characteristics: Wi-Fi® Control (write), Wi-Fi® Configure (write), Wi-Fi® Access Point List (notification), Monitoring (Notification) in order to control and monitor a Wi-Fi® connection
  • Is the GATT server

The Client Collector:

  • Accesses the information exposed by the Wi-Fi® commissioning application, configures and controls the Wi-Fi® connection with the write characteristics, monitors the Wi-Fi® connection status by receiving notifications from it
  • Is the GATT client

The diagram below describes how the ST67W6X_BLE_Commissioning application and the web client interface interact.

Bluetooth® Low Energy commissioning and ST67W6X
ST67W6X_BLE_Commissioning Description


3.1. Commissioning profile overview

The table below describes the structure of the commissioning service:

Bluetooth® Low Energy commissioning service specification
Service Characteristic Mode UUID size
Wi-Fi® commissioning 0000FF9A-cc7a-482a-984a-7f2ed5b3e58f
Wi-Fi® Control Write with Response/Read 0000FE9B-8e22-4541-9d4c-21edae82ed19 1
Wi-Fi® Configure Write with Response/Read 0000FE9C-8e22-4541-9d4c-21edae82ed19 240
Wi-Fi® AP List Notify 0000FE9D-8e22-4541-9d4c-21edae82ed19 240
Monitoring Notify 0000FE9E-8e22-4541-9d4c-21edae82ed19 240

Wi-Fi® commissioning is exposed as a service.

  • Wi-Fi® control characteristic:
    • Used to control Wi-Fi® by launching scans, connecting, or disconnecting from a network
Wi-Fi® commissioning - Wi-Fi® control
Byte Index 0
Name Action
Value 0x01: Wi-Fi® Start Scan
0x03: Wi-Fi® Connect
0x04: Wi-Fi® Disconnect
0x05: Wi-Fi® Ping


  • Wi-Fi® configure characteristic:
    • Used to set up Wi-Fi® parameters before establishing a connection
Wi-Fi® commissioning - Wi-Fi® configure
Byte Index 0 1
Name Type Data[ ]
Value 0x01: AP-SSID
0x02: PWD
“ASCII”
"ASCII"


  • Wi-Fi® access point list characteristic:
    • Used to notify information about scanned access points
Wi-Fi® Commissioning - Wi-Fi® AP List
Byte Index 0 1 2 to 3 4 to 7 8 to 40
Name SSID Length Channel Signal level Security Flag SSID
Value 0x00 ... 0x20 0x00 ... 0xFF 0x00 ... 0xFFFF Security_Flag[ ] Data[ ]
  • Monitoring characteristic:
    • Used to notify information about the Wi-Fi® network.
Wi-Fi® commissioning - Wi-Fi® monitoring
Byte Index 0 1 up to 239
Name Type Data[ ]
Value 0x03: Connecting
0x04: Connection established
0x05: Ping response
0x06: Error
X
SSID
Refer to table below
0x01: Connection Timeout
Wi-Fi® ping response format
Byte Index 0 1 to 2 3 4 to 7
Value 0x05:
ping response
Number of pings
High byte -> Low byte
Packet loss
in %
Average ping value
High byte -> Low byte

3.2. Advertising data

At startup, the commissioning application starts advertising.
Advertising data refers to information broadcast by a device and is composed as follows:

Commissioning advertising packet
Description Length AD Type Value
Device Name 11 0x09 ST_WiFi_XX (XX: last byte of BD address)
Manufacturer Data 15 0xFF See table below
Flags 2 0x01 0x06
(GeneralDiscoverable, BrEdrNotSupported)


Manufacturer data are based on the STMicroelectronics BlueST SDK v2 advertising format, as described below:

STMicroelectronics manufacturer advertising data
Byte Index 0 1 2-3 4 5 6 7 8 9 10-15
Function Length Manufacturer ID Company BlueST Protocol Version Device ID Firmware ID Option 1 Option 2 Option 3 Device Address
Value 0x0F 0xFF 0x0030 STMicro 0x02 0x9A - ST67W611 0xFE - Commissioning 0x00 0x00 0x00 0xXXXXXXXXXXXX

4. ST67W6X_BLE_Commissioning application

4.1. Project directory

The "ST67W6X_BLE_Commissioning" application is available by downloading the X-CUBE-ST67W61 Expansion Package.

Refer to the Project directory wiki page for project directory information.

4.2. Project description

The application acts as a peripheral device embedding the commissioning profile and its four characteristics.
At startup, the application starts advertising.

ST Web Bluetooth® Interface (ST Web Bluetooth® application) or ST BLE Toolbox Android/iOS application (ST BLE Toolbox commissioning interface) can be used to scan and connect to the commissioning application.

Once connected, a Wi-Fi® commissioning interface is available on the remote connected application.

This interface allows you to:

  • Scan Wi-Fi® networks
  • Establish a connection to a Wi-Fi® network
  • Disconnect from a Wi-Fi® network
  • Ping a Wi-Fi® access point
Example of flow diagram between ST67W61 and ST Web Bluetooth® Interface
WiFi Commissioning Flow Diagram


4.3. Project structure

The software project structure with the most important parts is shown below.

Commissioning project structure
WiFi Commissioning Flow Diagram


API descriptions are available on the following page: X-CUBE-ST67W61 Architecture.

4.4. Build and Install

Refer to build and load chapter for details on how to build and download the software onto the device.

4.5. User setup

4.5.1. ST67W6X default configuration

The default System configuration can be modified in "ST67W6X/Target/w6x_config.h":

/** NCP power save mode : 0: NCP stays always active / 1: NCP goes in low power mode when idle */
#define W6X_POWER_SAVE_AUTO                     0

/** NCP clock mode : 1: Internal RC oscillator, 2: External passive crystal, 3: External active crystal */
#define W6X_CLOCK_MODE                          1

Note: An external clock oscillator must be used to support Bluetooth® Low Energy in low-power mode. If W6X_POWER_SAVE_AUTO is set to 1 but the clock mode is not correct, the W6X_Ble_Init() API disables low-power mode.

The default Bluetooth® Low Energy configuration can be modified in the "ST67W6X/Target/w6x_config.h" file:

/** String defining BLE hostname */
#define W6X_BLE_HOSTNAME                        "ST_WiFi"

The default Wi-Fi® API configuration can be modified in the "ST67W6X/Target/w6x_config.h" file:

/** Define the region code, supported values : [CN, JP, US, EU, 00] */
#define W6X_WIFI_COUNTRY_CODE                   "00"

/** Define if the country code will match AP's one.
  * 0: match AP's country code,
  * 1: static country code */
#define W6X_WIFI_ADAPTIVE_COUNTRY_CODE          0

The default Net API configuration can be modified in the "ST67W6X/Target/w6x_config.h" file:

/** Define the DHCP configuration : 0: NO DHCP, 1: DHCP CLIENT STA, 2:DHCP SERVER AP, 3: DHCP STA+AP */
#define W6X_NET_DHCP                            1

/** String defining Wi-Fi® hostname */
#define W6X_NET_HOSTNAME                        "ST67W61_WiFi"

/** Timeout in ticks when calling W6X_Net_Recv() */
#define W6X_NET_RECV_TIMEOUT                    10000

/** Timeout in ticks when calling W6X_Net_Send() */
#define W6X_NET_SEND_TIMEOUT                    10000

The AT driver can be configured in "ST67W6X/Target/w61_driver_config.h":

/** Maximum number of detected AP during the scan. Cannot be greater than 50 */
#define W61_WIFI_MAX_DETECTED_AP                20

/** Enable/Disable Wi-Fi® module logging */
#define WIFI_LOG_ENABLE                         1

/** Enable/Disable Network module logging */
#define NET_LOG_ENABLE                          1

/** Maximum number of detected peripheral during the scan. Cannot be greater than 50 */
#define W61_BLE_MAX_DETECTED_PERIPHERAL         10

/** Enable/Disable BLE module logging */
#define BLE_LOG_ENABLE                          1

/** Maximum SPI buffer size */
#define W61_MAX_SPI_XFER                        6000

/** Enable/Disable System module logging */
#define SYS_LOG_ENABLE                          1

/** Debugging only: Enable AT log, i.e. logs the AT commands incoming/outcoming from/to the NCP */
#define W61_AT_LOG_ENABLE                       0

Additionally, some other options can be modified in the "ST67W6X/Target" directory with different configuration files, as outlined below:

  • logging_config.h: This file provides configuration for the logging component, enabling the setting of the log level
  • shell_config.h: This file provides configuration for the Shell component.
  • w6x_config.h: This file provides configuration for the W6X APIs (used during init).
  • w61_driver_config.h: This file provides configuration for the W61 configuration module.

All available defines are provided in the template directory "Middlewares/ST/ST67W6X_Network_Driver/Conf"

4.5.2. Application configuration

The logging output mode can be modified in "Appli/App/app_config.h":

/** Select output log mode [0: printf / 1: UART / 2: ITM] */
#define LOG_OUTPUT_MODE             LOG_OUTPUT_UART

The host low-power mode can be modified in "Appli/App/app_config.h":

/** Low power configuration [0: disable / 1: sleep / 2: stop / 3: standby] */
#define LOW_POWER_MODE              LOW_POWER_DISABLE

The host debugger pins can be modified in "Appli/App/app_config.h":

/**
* Enable/Disable MCU Debugger pins (dbg serial wires)
* @note by HW serial wires are ON by default, need to put them OFF to save power
*/
#define DEBUGGER_ENABLED            1

4.6. Bluetooth® Low Energy Client solutions

One of the following two Bluetooth® Low Energy client solutions must be used to scan, connect, and interface with the embedded Bluetooth® Low Energy commissioning application.

Note:

  • Pressing USER button on the board while not connected clears the bonded device list of the platform.
  • Pressing USER button on the board while connected disconnects from the remote client.

4.6.1. ST BLE Toolbox application

In order to interface with the embedded Wi-Fi® commissioning application, the STBLEToolbox Android/iOS application has been updated.
The versions supporting the Wi-Fi® commissioning service are v1.4.3 for Android and 1.2.8 for iOS.

Launch the smartphone application and enable the scan button, if it is not already activated.
You can filter scanned devices by clicking on the SHOW FILTERS button and select ST BLE Wi-Fi to show only devices with Wi-Fi® commissioning service.

Select your device, named ST_WiFi_XX where XX represents the last BD address digit, and connect to it.

ST BLE Toolbox: Bluetooth® Low Energy scan filter
Bluetooth® Low Energy Scan filter

Once connected to the Bluetooth® Low Energy device, click on Wi-Fi Provisioning button to open the commissioning dedicated interface.

ST BLE Toolbox: Wi-Fi® commissioning interface
WiFi Commissioning interface


From this interface, you can launch a Wi-Fi® scan (1), to detect and list all available networks (2).

Once the available networks are displayed, select the one you want to connect to (2), type a password if needed (3), and click on the CONNECT button (4).

Wi-Fi® connection interface
WiFi connection interface


Once the connection request is done, the connection status is displayed in the interface.
Clicking the Ping button starts a ping test with the Wi-Fi® access point and returns the results in the interface.

Wi-Fi® status and ping
WiFi Ping status and ping

4.6.2. ST Web Bluetooth® commissioning interface

Another way to interface with the embedded Wi-Fi® commissioning application is to use the web interface developed by ST and available at the following link: ST Web Bluetooth® Interface, accessible from a computer, tablet, or smartphone.

Enable the Bluetooth® connection of the device, click on "Connect" button and select ST_WiFi_[...] device.

Connection from web Bluetooth®
Connection from Web Bluetooth®

Once connected, click on the Wi-Fi Commissioning button to open the commissioning dedicated interface.

Wi-Fi® commissioning interface
WiFi Commissioning interface


From this interface, you can launch a Wi-Fi® scan (1), to detect and list all available networks (2).

Once the available networks are displayed, select the one you want to connect to (2), type a password if needed (3) and click on Wi-Fi Connection Request button (4).

Wi-Fi® connection interface
WiFi connection interface


Once the connection request is done, the connection status is displayed in the interface.

Wi-Fi® connection status
WiFi connection status


Clicking the Ping button starts a ping test with the Wi-Fi® access point and returns the results in the interface.

Wi-Fi® ping status
WiFi Ping status

4.7. Bluetooth® Low Energy FUOTA

This section describes the Bluetooth® Low Energy-based FUOTA mechanism integrated in the ST67W611M1 Bluetooth® Low Energy Commissioning application.
It enables:

  • Updating the ST67W611M1 module firmware
  • Updating the STM32 NUCLEO-U575ZI-Q host application image (STM32 NUCLEO-U575ZI-Q only)

The Bluetooth® Low Energy FUOTA design reuses the concepts of the Wi-Fi® FOTA workflow while adapting them to a write‑stream Bluetooth® Low Energy pattern (no per‑chunk acknowledgments). For generic concepts see:

4.7.1. Main Points

  • Minimal GATT surface: one service, three characteristics (Control Point, Confirmation, Data)
  • Write Without Response streaming
  • Low ISR load: callbacks enqueue work; heavy operations deferred to a task
  • Buffering: single linear buffer with automatic flush

4.7.2. GATT Service Model

The firmware update over the air (FUOTA) profile is intended to demonstrate the multiple capabilities of the ST67W611M1 Bluetooth® Low Energy solution. It acts as:

  • GAP central & GATT server (Router service) device to be connected and controlled by a smartphone.
  • GAP peripheral & GATT client device to control end device (Bluetooth® Commissioning FUOTA Server).

The FUOTA service is a generic attribute profile (GATT) based on the low-energy profile defined by STMicroelectronics with proprietary UUIDs (128 bits) including three characteristics, described below.

The structure of the FUOTA service is described below:

Bluetooth® Low Energy FUOTA service specification
Service Characteristic Mode UUID Size
FUOTA service 0000FE20-cc7a-482a-984a-7f2ed5b3e58f
Base Address Write without response 0000FE22-8e22-4541-9d4c-21edae82ed19 5
Confirmation Indicate 0000FE23-8e22-4541-9d4c-21edae82ed19 1
Raw Data Write without response 0000FE24-8e22-4541-9d4c-21edae82ed19 240

The FUOTA service is composed of three characteristics:

FUOTA service - Base address characteristic
Byte Index 0 [1:4]
Name Action N/A
Value 0x00: STOP All Upload
0x01: START Application co-processor binary Update
0x02: START Wireless co-processor binary Update
0x06: End Of File Transfer
0x07: File Upload Finish
0x08: Cancel Upload
(Not used by application in ST67W611M1 case)

The smartphone or web Bluetooth® application uses this characteristic to indicate the action to perform. The address where to load the new application file is managed by the embedded application and not configurable from ​web Bluetooth® interface.

FUOTA service - Confirmation characteristic
Byte Index 0
Name File Upload Indication
Value 0x01: Reboot
0x02: Ready To Receive File
0x03: Error Not Free

Device (FUOTA server) used this characteristic to inform the smartphone or web Bluetooth® application about:

  • Ready To Receive File: ready to receive the new binary application.​
  • Reboot: the new file is fully received.​
  • Error not free: not ready to receive a new binary application.
FUOTA Service - Raw data characteristic
Byte Index [0..239]
Name Raw Data (LSB First)
Value File Data

The smartphone or web Bluetooth® application uses this characteristic to transfer the file.
Raw Data size is limited to 240 bytes, multiple of 16 bytes, the minimum flash writes access size.
240 bytes is the maximum size multiple of 16 bytes behind the negotiated maximum ATT MTU size 251 bytes.
Only size multiple of 16 bytes lower than 240 bytes are allowed.

4.7.3. FUOTA interfaces

To interface with the embedded Bluetooth® Low Energy FUOTA application, both the ST Web Bluetooth® solution and the ST BLE Toolbox Android/iOS application can be used.

4.7.3.1. ST Web Bluetooth® FUOTA interface

The ST Web Bluetooth® solution has been developed by ST and is available at the following link ST Web Bluetooth® Interface, accessible from a computer, tablet, or smartphone.

Enable the Bluetooth® connection of the device, click on "Connect" button and select ST_WiFi_[...] device.

Connection from web Bluetooth®
Connection from Web Bluetooth®

Once connected, click on the Firmware Update Over The Air button to open the FUOTA dedicated interface.

BLE® FUOTA interface
Wi-Fi® Commissioning interface


From this interface, select the co-processor to update (1), select the binary file to upload (2) and (3), then start the update (4).

Button descriptions
Wi-Fi® Commissioning interface


Upload progress is displayed in the web interface and a platform reboot is performed once it is completed.

4.7.3.2. ST BLE Toolbox FUOTA interface

In order to interface with the Bluetooth® Low Energy FUOTA service, the ST BLE Toolbox Android/iOS application has been updated.
The versions supporting the FUOTA service for the ST67 platform are v1.5.0 for Android and 1.2.10 for iOS.

Connect in the same way as described in the ST BLE Toolbox application chapter.
Then, click on Over The Air Update Server button to open the FUOTA dedicated interface.

ST BLE Toolbox: FUOTA interface
FUOTA interface


From this interface, select the co-processor to update (1), select the binary file to upload (2), and start the update (3).

Button descriptions
Wi-Fi® Commissioning interface


Upload progress is displayed in the web interface and a platform reboot is performed once it is completed.

4.7.4. Operation Flow

The Bluetooth® Low Energy FUOTA task is responsible for processing FUOTA events. It uses a queue to decouple the Bluetooth® Low Energy event callback from the actual processing.
This way the processing can happen in the FUOTA task context, without blocking the Bluetooth® Low Energy stack.

BLE FUOTA event is received → event is queued → FUOTA task dequeues the event → processes data.

The queue contains a structure with the event type (control or data), the data length and a pointer to the data. The FUOTA task processes the events in the order they are received.

A buffer is allocated at START and freed at FINISH or STOP/CANCEL. This buffer acts as a staging area for incoming data chunks.
Incoming data chunks are appended to this buffer until it is full; at that point, it is flushed to the appropriate API (ST67W611M1 or STM32 NUCLEO-U575ZI-Q), which writes the data to the target flash memory.
If a FINISH command is received, any remaining data in the buffer is flushed before finalizing the update.

The FINISH operation consists of applying the update by bank swapping and rebooting to the new bank. For the ST67W611M1 path, finalize operations are handled internally, including an integrity check before rebooting on the new software.

Note
To load a binary or perform debugging through any IDE after completing an application processor Update Over The Air (STM32 NUCLEO-U575ZI-Q FOTA), use STM32CubeProgrammer to set the SWAP_BANK option byte to "Not swapped".

File Upload indications (0x02: start, 0x01: reboot, 0x03: error) are sent only from the FUOTA task to acknowledge progress or raise an error.
Note that the data characteristic uses Write Without Response, so no per-chunk acknowledgment is sent.

The following tables show FUOTA service base address characteristic usage depending on the target to be updated.

4.7.4.1. ST67W611M1 Update
Step Trigger / Base address characteristic Action Performed Update Indication
(if any)
Notes
1 START ST67W611M1 update (0x02) Allocate a buffer, set ST67W611M1 update mode 0x02 Session context initialized
2 Raw data chunks stream Append to buffer; flush to module OTA API on full – Write Without Response
3 FINISH (0x07) Flush remaining buffer data; the ST67W611M1 checks integrity and swaps to the new version if it passes 0x01
Abort STOP (0x00) / CANCEL (0x08) In case of error or context reset; Free buffer; reset state – Partial image discarded


Below is the flow diagram example of Bluetooth® Low Energy FUOTA for network co-processor binary:

Example of flow diagram between STM32WBAs & ST Bluetooth® LE Toolbox smartphone application for Network co-processor FUOTA.


4.7.4.2. STM32 Update
Step Trigger / Base address characteristic Action Performed Update Indication
(if any)
Notes
1 START STM32 update (0x01) Allocate buffer; select STM32 update mode; erase target flash bank 0x02 Done in task context
2 Raw data chunks stream Append to buffer; when full write in secondary flash bank – Write Without Response
3 FINISH (0x07) Flush remaining buffer data; STM32 NUCLEO-U575ZI-Q bank swap and reboot on the new version 0x01 Schedule bank swap / reboot sequence
Abort STOP (0x00) / CANCEL (0x08) In case of error or context reset; Free buffer; reset state – Partial image discarded


Below is the flow diagram example of Bluetooth® Low Energy FUOTA for application binary :

Flow diagram between STM32WBAs & ST Bluetooth® LE Toolbox smartphone application for Application co-processor FUOTA.


4.7.5. Client binary time upload

The following tables show indicative timing when using compressed and uncompressed ST67W611M1 binaries with varying connection intervals.
These results were obtained using the ST67W611M1 Bluetooth® Low Energy Web Application.
They give a general idea of expected time to upload a binary image to the ST67W611M1 module using Bluetooth® Low Energy FUOTA.

XZ Compressed Image (806400 bytes)
Connection Interval (ms) 55 20 7.5
Avg Download Time (s) 44 18 16


RAW Image (1399872 bytes)
Connection Interval (ms) 55 20 7.5
Avg Download Time (s) 75 34 30


Note
Times are measured on the client side (Bluetooth® Low Energy Web App, Windows PC). They exclude module finalize, reboot, and post‑update housekeeping.

4.7.6. Quick Reference Sequence (Module)

BLE FUOTA event sequence diagram

4.8. Memory footprint

Module Description
[Driver] HAL/CMSIS/BSP STM32 CMSIS Cortex, HAL and LL, Board Specific Package drivers
[Project] Core Native STM32 core components
[Project] App Main part of the application
[Project] Target Configuration files for ST67W6X_Network_Driver component
[MW] ST67W6X_Network_Driver Core and API System, Wi-Fi®, Bluetooth® Low Energy and Network components
Util/Logging: Utility to process shell and trace messages onto the UART interface (can be changed by ITM)
[MW] FreeRTOS FreeRTOS kernel source
[Utility] lpm Tiny Low-Power Management
[Toolchain] Startup Int_vect, init routines, init table, CSTACK and HEAP
[Toolchain] EWARM Libraries Native compiler libraries

These values depend on the chosen toolset, and they can change in future releases.

4.8.1. ROM/Flash memory footprint

The picture below shows the sum of the read-only memory (flash) of the Wi-Fi® commissioning over Bluetooth® Low Energy application.

ST67W6X_BLE_Commissioning read-only memory footprint.

The picture below shows the middleware ST67W6X_Network_Driver read-only memory (flash) used by Wi-Fi® commissioning over the Bluetooth® Low Energy application.

ST67W6X_Network_Driver read-only memory footprint used by ST67W6X_BLE_Commissioning application.

4.8.2. Read-Write (RW) memory footprint

Information
The FreeRTOS Heap is not part of the chart below.
The dynamic memory allocation adds 200'000 bytes (value set for the TOTAL_HEAP_SIZE FreeRTOS parameter).

The ST67W6X_BLE_Commissioning project uses only 18 KB of the heap. Refer to Dynamic memory overview wiki page.

The picture below shows only the sum of the static read/write memory (static RAM) of the Wi-Fi® commissioning over the Bluetooth® Low Energy application.

ST67W6X_BLE_Commissioning Read Write memory footprint

5. References